The component manages a disk on a volatile memory (internal RAM).
This can be connected to a File System management or a USB Device Mass Storage Interface via the service Memory Control Access.
Functions | |
Ctrl_status | virtual_mem_2_ram (uint32_t addr, void *ram) |
This function transfers 1 data sector from memory to RAM sector = 512 bytes. More... | |
Ctrl_status | virtual_ram_2_mem (uint32_t addr, const void *ram) |
This function transfers 1 data sector from memory to RAM sector = 512 bytes. More... | |
Ctrl_status | virtual_read_capacity (uint32_t *uint32_t_nb_sector) |
This function returns the address of the last valid sector. More... | |
bool | virtual_removal (void) |
This function informs about the memory type. More... | |
Ctrl_status | virtual_test_unit_ready (void) |
This function tests memory state, and starts memory initialization. More... | |
bool | virtual_unload (bool unload) |
This function unloads/loads the memory. More... | |
Ctrl_status | virtual_usb_read_10 (uint32_t addr, uint16_t nb_sector) |
This function transfers the memory data to the USB MSC interface. More... | |
static Ctrl_status | virtual_usb_trans (uint32_t addr, uint16_t nb_sector, bool b_read) |
This function transfers the data between memory and USB MSC interface. More... | |
Ctrl_status | virtual_usb_write_10 (uint32_t addr, uint16_t nb_sector) |
This function transfers the USB MSC data to the memory. More... | |
bool | virtual_wr_protect (void) |
This function returns the write-protected mode. More... | |
Variables | |
static bool | b_vmem_unloaded = false |
static COMPILER_WORD_ALIGNED uint8_t | vmem_data [VMEM_NB_SECTOR *VMEM_SECTOR_SIZE] |
Ctrl_status virtual_mem_2_ram | ( | uint32_t | addr, |
void * | ram | ||
) |
This function transfers 1 data sector from memory to RAM sector = 512 bytes.
addr | Sector address to start read |
ram | Address of RAM buffer |
References CTRL_FAIL, CTRL_GOOD, Max, min, virtual_check_init(), vmem_data, VMEM_NB_SECTOR, and VMEM_SECTOR_SIZE.
Ctrl_status virtual_ram_2_mem | ( | uint32_t | addr, |
const void * | ram | ||
) |
This function transfers 1 data sector from memory to RAM sector = 512 bytes.
addr | Sector address to start write |
ram | Address of RAM buffer |
References CTRL_FAIL, CTRL_GOOD, virtual_check_init(), vmem_data, VMEM_NB_SECTOR, and VMEM_SECTOR_SIZE.
Ctrl_status virtual_read_capacity | ( | uint32_t * | uint32_t_nb_sector | ) |
This function returns the address of the last valid sector.
uint32_t_nb_sector | Pointer to number of sectors (sector=512 bytes) |
References b_vmem_unloaded, CTRL_GOOD, CTRL_NO_PRESENT, Max, virtual_check_init(), and VMEM_NB_SECTOR.
bool virtual_removal | ( | void | ) |
This function informs about the memory type.
Ctrl_status virtual_test_unit_ready | ( | void | ) |
This function tests memory state, and starts memory initialization.
References b_vmem_unloaded, CTRL_GOOD, CTRL_NO_PRESENT, and virtual_check_init().
This function unloads/loads the memory.
References b_vmem_unloaded.
Ctrl_status virtual_usb_read_10 | ( | uint32_t | addr, |
uint16_t | nb_sector | ||
) |
This function transfers the memory data to the USB MSC interface.
This function transfers the memory data (programmed in sbc_read_10) directly to the USB interface sector = 512 bytes.
addr | Sector address to start read |
nb_sector | Number of sectors to transfer (sector=512 bytes) |
References CTRL_FAIL, CTRL_GOOD, data_to_transfer, g_scsi_ep_ms_in, Is_usb_endpoint_enabled, Is_usb_in_ready, Max, min, Usb_ack_in_ready_send, Usb_reset_endpoint_fifo_access, usb_write_ep_txpacket(), virtual_check_init(), virtual_usb_trans(), vmem_data, VMEM_NB_SECTOR, and VMEM_SECTOR_SIZE.
|
static |
This function transfers the data between memory and USB MSC interface.
addr | Sector address to start read |
nb_sector | Number of sectors to transfer (sector=512 bytes) |
b_read | Memory to USB, if true |
References buffer, CTRL_FAIL, CTRL_GOOD, min, NULL, udi_msc_trans_block(), vmem_data, VMEM_NB_SECTOR, and VMEM_SECTOR_SIZE.
Referenced by virtual_usb_read_10(), and virtual_usb_write_10().
Ctrl_status virtual_usb_write_10 | ( | uint32_t | addr, |
uint16_t | nb_sector | ||
) |
This function transfers the USB MSC data to the memory.
This function transfers the USB data (programmed in sbc_write_10) directly to the memory interface sector = 512 bytes.
addr | Sector address to start write |
nb_sector | Number of sectors to transfer (sector=512 bytes) |
References CTRL_FAIL, CTRL_GOOD, data_to_transfer, g_scsi_ep_ms_out, Is_usb_endpoint_enabled, Is_usb_out_received, Usb_ack_out_received_free, usb_read_ep_rxpacket(), Usb_reset_endpoint_fifo_access, virtual_check_init(), virtual_usb_trans(), vmem_data, VMEM_NB_SECTOR, and VMEM_SECTOR_SIZE.
bool virtual_wr_protect | ( | void | ) |
This function returns the write-protected mode.
This function returns the write-protected mode Only used by memory removal with a HARDWARE-SPECIFIC write-protected detection.
Referenced by virtual_read_capacity(), virtual_test_unit_ready(), and virtual_unload().
|
static |
Referenced by virtual_mem_2_ram(), virtual_ram_2_mem(), and virtual_usb_trans().