Microchip® Advanced Software Framework

 All Data Structures Namespaces Files Functions Variables Typedefs Enumerations Enumerator Friends Macros Groups Pages
Common SW Timer

Implements the software Algorithm for Timer Handling in the Stack.

Modules

 Group_pal_common_hw_timer
 Implements a common api interface for accessing timer drivers of all architectures.
 

Data Structures

struct  timer_info_tag
 

Macros

#define ADD_TIME(a, b)   ((a) + (b))
 Adds two time values. More...
 
#define HW_TIME_MASK   (0xFFFF)
 
#define MAX_NO_OF_TIMERS   (25)
 
#define MAX_TIMEOUT   (0x7FFFFFFF)
 
#define MIN_TIMEOUT   (0x80)
 
#define NO_TIMER   (0xFF)
 
#define SUB_TIME(a, b)   ((a) - (b))
 Subtracts two time values. More...
 
#define SYS_TIME_SHIFT_MASK   (16)
 
#define TOTAL_TIMERS   TOTAL_NUMBER_OF_TIMERS
 

Typedefs

typedef enum sw_timeout_type_tag sw_timeout_type_t
 Timeout type. More...
 
typedef void(* timer_expiry_cb_t )(void *)
 
typedef struct timer_info_tag timer_info_t
 

Enumerations

enum  sw_timeout_type_tag {
  SW_TIMEOUT_RELATIVE,
  SW_TIMEOUT_ABSOLUTE
}
 Timeout type. More...
 

Functions

status_code_t sw_timer_get_id (uint8_t *timer_id)
 Returns a timer id to be used before starting a timer. More...
 
uint32_t sw_timer_get_residual_time (uint8_t timer_id)
 
uint32_t sw_timer_get_time (void)
 Gets current time. More...
 
void sw_timer_init (void)
 Initializes the Software Timer module. More...
 
bool sw_timer_is_running (uint8_t timer_id)
 Checks whether a given timer is running or not. More...
 
uint32_t sw_timer_next_timer_expiry_duration (void)
 
void sw_timer_run_residual_time (uint32_t offset)
 
void sw_timer_service (void)
 Handles Queues and Callbacks for Expired Timers. More...
 
status_code_t sw_timer_start (uint8_t timer_id, uint32_t timer_count, sw_timeout_type_t timeout_type, FUNC_PTR timer_cb, void *param_cb)
 Starts a timer. More...
 
status_code_t sw_timer_stop (uint8_t timer_id)
 Stops a running timer. More...
 

Variables

uint32_t timer_info_tag::abs_exp_timer
 
bool timer_info_tag::loaded
 
uint8_t timer_info_tag::next_timer_in_queue
 
void * timer_info_tag::param_cb
 
FUNC_PTR timer_info_tag::timer_cb
 

#define ADD_TIME (   a,
  b 
)    ((a) + (b))

Adds two time values.

Referenced by pal_add_time_us().

#define HW_TIME_MASK   (0xFFFF)
#define MAX_NO_OF_TIMERS   (25)
#define MAX_TIMEOUT   (0x7FFFFFFF)
#define MIN_TIMEOUT   (0x80)
#define NO_TIMER   (0xFF)

Referenced by sw_timer_init(), and sw_timer_service().

#define SUB_TIME (   a,
  b 
)    ((a) - (b))

Subtracts two time values.

Referenced by calculate_time_duration(), and pal_sub_time_us().

#define SYS_TIME_SHIFT_MASK   (16)
#define TOTAL_TIMERS   TOTAL_NUMBER_OF_TIMERS

Timeout type.

typedef void(* timer_expiry_cb_t)(void *)
typedef struct timer_info_tag timer_info_t

Timeout type.

Enumerator
SW_TIMEOUT_RELATIVE 

The timeout is relative to the current time.

SW_TIMEOUT_ABSOLUTE 

The timeout is an absolute value.

status_code_t sw_timer_get_id ( uint8_t *  timer_id)

Returns a timer id to be used before starting a timer.

Parameters
timer_idValue of the id returned by the function

Referenced by app_timers_init(), main(), and pal_timer_get_id().

uint32_t sw_timer_get_residual_time ( uint8_t  timer_id)
uint32_t sw_timer_get_time ( void  )

Gets current time.

This function returns the current time.

Parameters
[out]current_timeReturns current system time

Referenced by pal_get_current_time(), pal_trx_read_timestamp(), per_mode_initiator_tx_done_cb(), and start_test().

bool sw_timer_is_running ( uint8_t  timer_id)

Checks whether a given timer is running or not.

Parameters
[out]Trueif the timer is running else False

Referenced by pal_is_timer_running(), peer_req_send_task(), per_mode_initiator_rx_cb(), and stop_pkt_streaming().

uint32_t sw_timer_next_timer_expiry_duration ( void  )
void sw_timer_run_residual_time ( uint32_t  offset)
void sw_timer_service ( void  )

Handles Queues and Callbacks for Expired Timers.

References callback, cpu_irq_restore(), cpu_irq_save(), timer_info_tag::loaded, NO_TIMER, NULL, timer_info_tag::param_cb, and timer_info_tag::timer_cb.

Referenced by pal_task().

uint32_t timer_info_tag::abs_exp_timer
bool timer_info_tag::loaded

Referenced by sw_timer_service().

uint8_t timer_info_tag::next_timer_in_queue

Referenced by sw_timer_init().

void* timer_info_tag::param_cb

Referenced by sw_timer_service().

FUNC_PTR timer_info_tag::timer_cb

Referenced by sw_timer_init(), and sw_timer_service().