Microchip® Advanced Software Framework

lightprox_visualizer/data_visualizer.h File Reference

Atmel Data Visualizer definitions.

This file contains various definitions related to applications producing data streams expected by the Atmel Data Visualizer tool.

The Atmel Data Visualizer (ADV) tool is a standalone Windows application that provides a graphical display of data sent from a remote target. It is available as a separate download. For more information on downloading and installing the ADV tool, visit Atmel Data Visualizer

Copyright (c) 2014-2018 Microchip Technology Inc. and its subsidiaries.

#include <stdio.h>
#include <string.h>
#include <stdint.h>
#include <stdlib.h>

Data Structures

struct  adv_config_end_t
 Atmel Data Visualizer end-of-configuration packet. More...
 
struct  adv_config_field_t
 Atmel Data Visualizer data field configuration packet. More...
 
struct  adv_config_stream_t
 Atmel Data Visualizer data stream configuration packet. More...
 
struct  adv_data_end_t
 
struct  adv_data_field_t
 
struct  adv_data_start_t
 Atmel Data Visualizer data packet components. More...
 

Macros

#define ADV_PKT_CONFIG_END   0x02
 
#define ADV_PKT_CONFIG_FIELD   0x04
 
#define ADV_PKT_CONFIG_START   0x01
 
#define ADV_PKT_CONFIG_STREAM   0x03
 
#define ADV_PKT_DATA   0x05
 
#define ADV_PKT_END   0x06
 
#define ADV_PKT_HEADER_1   0xFF
 
#define ADV_PKT_HEADER_2   0x5A
 
#define FIELD_FORMAT_FLOAT   3
 
#define FIELD_FORMAT_SIGNED   1
 
#define FIELD_FORMAT_UNSIGNED   2
 
#define FIELD_NAME_LEN   11
 
#define FIELD_UNIT_LEN   20
 
#define STREAM_NAME_LEN   25
 

Functions

void adv_data_send_1 (uint8_t stream_num, uint32_t timestamp, int32_t value)
 Send Atmel Data Visualizer data packet with 1 data field. More...
 
void adv_data_send_3 (uint8_t stream_num, uint32_t timestamp, int32_t value0, int32_t value1, int32_t value2)
 Send Atmel Data Visualizer data packet w/ 3 data fields. More...
 
 COMPILER_PACK_RESET () void adv_write_buf(uint8_t *buf
 Write Atmel Data Visualizer data buffer via USB or serial port. More...
 
 COMPILER_PACK_SET (1) typedef struct
 Atmel Data Visualizer start-of-configuration packet. More...
 

Variables

 adv_config_start_t
 
int num_bytes
 

#define ADV_PKT_CONFIG_END   0x02
#define ADV_PKT_CONFIG_FIELD   0x04
#define ADV_PKT_CONFIG_START   0x01
#define ADV_PKT_CONFIG_STREAM   0x03
#define ADV_PKT_DATA   0x05
#define ADV_PKT_END   0x06
#define ADV_PKT_HEADER_1   0xFF
#define ADV_PKT_HEADER_2   0x5A
#define FIELD_FORMAT_FLOAT   3
#define FIELD_FORMAT_SIGNED   1
#define FIELD_FORMAT_UNSIGNED   2
#define FIELD_NAME_LEN   11
#define FIELD_UNIT_LEN   20
#define STREAM_NAME_LEN   25

void adv_data_send_1 ( uint8_t  stream_num,
uint32_t  timestamp,
int32_t  value 
)

Send Atmel Data Visualizer data packet with 1 data field.

This routine constructs a data visualizer data packet with one data value field and then transmits it. All multi-byte transmitted values use little endian byte order.

Parameters
stream_numThe ID number of the visualizer data stream
timestampA 32-bit timestamp value, in microseconds
valueThe data value to include in the transmitted packet
Returns
Nothing.

Send Atmel Data Visualizer data packet with 1 data field.

This routine constructs a data visualizer data packet with one data value field and then transmits it. All multi-byte transmitted values use little endian byte order.

Parameters
stream_numThe ID number of the visualizer data stream
timestampA 32-bit timestamp value, in microseconds
valueThe data value to include in the transmitted packet

References ADV_PKT_DATA, ADV_PKT_END, ADV_PKT_HEADER_1, ADV_PKT_HEADER_2, cpu_to_le16, cpu_to_le32, end, and start.

Referenced by main().

void adv_data_send_3 ( uint8_t  stream_num,
uint32_t  timestamp,
int32_t  value0,
int32_t  value1,
int32_t  value2 
)

Send Atmel Data Visualizer data packet w/ 3 data fields.

This routine constructs a data visualizer data packet with three data value fields and then transmits it. All multi-byte transmitted values use little endian byte order.

Parameters
stream_numThe ID number of the visualizer data stream
timestampA 32-bit timestamp value, in microseconds
value0Data field 0 value
value1Data field 1 value
value2Data field 2 value
Returns
Nothing.

Send Atmel Data Visualizer data packet w/ 3 data fields.

This routine constructs a data visualizer data packet with three data value fields and then transmits it. All multi-byte transmitted values use little endian byte order.

Parameters
stream_numThe ID number of the visualizer data stream
timestampA 32-bit timestamp value, in microseconds
value0Data field 0 value
value1Data field 1 value
value2Data field 2 value

References ADV_PKT_DATA, ADV_PKT_END, ADV_PKT_HEADER_1, ADV_PKT_HEADER_2, cpu_to_le16, cpu_to_le32, end, and start.

Referenced by main().

COMPILER_PACK_RESET ( )

Write Atmel Data Visualizer data buffer via USB or serial port.

This application uses a serial or USB connection to transmit sensor data. This routine takes the specified input buffer and writes each byte to the appropriate output device.

Parameters
bufferThe address of a buffer containing the data to transmit
num_bytesThe number of bytes to transmit
Returns
Nothing.
COMPILER_PACK_SET ( )

Atmel Data Visualizer start-of-configuration packet.

References length.

adv_config_start_t
int num_bytes