Microchip® Advanced Software Framework

mmi_task.h File Reference

Functions

void mmi_task (void)
 Entry point of the MMI task management. More...
 
void mmi_task_init (uint32_t fcpu, uint32_t fpba)
 This function initializes the hardware/software resources required for the MMI task. More...
 

void mmi_task_init ( uint32_t  fcpu,
uint32_t  fpba 
)

This function initializes the hardware/software resources required for the MMI task.

References BLACK, et024006_DrawFilledRect(), ET024006_HEIGHT, et024006_Init(), ET024006_WIDTH, gpio_set_gpio_pin(), mmi_state, and MMI_TOP_MENU_START.

Referenced by main().