Macros | |
#define | _NF_C_ |
Functions | |
bool | nf_check_status (void) |
Check the status of the selected device. More... | |
U8 | nf_check_type (U8 nb_dev) |
Tests the Nand Flash configuration. More... | |
void | nf_copy_back_init (U32 page_addr) |
Prepare a copy-back session. More... | |
void | nf_erase_block (U32 page_addr, U8 force_erase) |
Erases a block. More... | |
U8 | nf_get_freq (void) |
returns the frequency supported by the selected NF. More... | |
void | nf_init (U32 hsb_f_hz) |
Initializes the Nand Flash Controller and low level driver. More... | |
void | nf_mark_bad_block (U32 page_addr) |
Mark a block as 'invalid' by clearing it entirely. More... | |
void | nf_open_page_read (U32 page_addr, U16 byte_addr) |
Opens a page for read. More... | |
void | nf_open_page_write (U32 page_addr, U16 byte_addr) |
Opens a page for write. More... | |
void | nf_protect (void) |
Protect all the flashes. More... | |
U32 | nf_read_id (U8 read_id_cmd, U8 nf_num) |
Read the ID of the Nand-Flash. More... | |
void | nf_reset_nands (U8 nb_dev) |
Reset all the NF devices. More... | |
void | nf_unprotect (void) |
unprotect all the flashes More... | |
void | nf_wait_busy (void) |
Tests the true busy. More... | |
U8 | nfc_detect (void) |
Read the ID of the Nand-Flash and update the global variable. More... | |
static bool | nfc_nf_is_ready (void) |
Check the status Ready/Busy of the Nand Flash. More... | |
void | nfc_read_spare_byte (U8 _MEM_TYPE_SLOW_ *p_byte, U8 n_byte, U32 page_addr) |
Reads the number spare bytes specified and stores them in a array. More... | |
#define _NF_C_ |
U8 nfc_detect | ( | void | ) |
Read the ID of the Nand-Flash and update the global variable.
References St_nf_conf::cache_program, St_nf_conf::ce_low, St_nf_id::conf, St_nf_conf::copy_back_cont, St_nf_conf::copy_back_discont, St_nf_conf::dfc_nfc_clock, g_cache_program, g_ce_low, g_clock_dfc_nfc, g_copy_back_cont, g_copy_back_discont, g_dev_id, g_dev_maker, g_n_blocks, g_n_row_cycles, g_n_zones, g_shift_block_page, g_shift_page_byte, MSB0, MSB1, St_nf_link_id_block::nb_zones, nf_force_CE, nf_init(), nf_list_conf, nf_list_id, nf_list_link_id_block, NF_MAX_DEVICES, nf_read_id(), NF_READ_ID_CMD, nf_reset_nands(), and nfc_nf_is_ready().
|
static |
Check the status Ready/Busy of the Nand Flash.
Referenced by nfc_detect().
void nfc_read_spare_byte | ( | U8 _MEM_TYPE_SLOW_ * | p_byte, |
U8 | n_byte, | ||
U32 | page_addr | ||
) |
Reads the number spare bytes specified and stores them in a array.
p_byte | pointer on the array in which are stored the spare bytes. |
n_byte | number of spare bytes to read. |
page_addr | absolute page address of the block. |
nf_init()
should have been called before. The NF device should have been selected before with nf_select( id )
. References i, nf_open_page_read(), nf_rd_data(), and NF_SPARE_POS.