#include "lwip/opt.h"
#include "lwip/mem.h"
#include "lwip/raw.h"
#include "lwip/icmp.h"
#include "lwip/netif.h"
#include "lwip/sys.h"
#include "lwip/sockets.h"
#include "lwip/inet.h"
#include "lwip/inet_chksum.h"
#include "lwip/tcp.h"
#include "lwip/udp.h"
#include <net/ttcp.h>
#include <ports/avr32/timer.h>
#include <util/util.h>
#include <net/lwip_setup.h>
#include "getopt.h"
#include <wl/cmd_wl.h>
Data Structures | |
struct | ttcp |
Macros | |
#define | TTCP_MODE_RECEIVE 1 |
#define | TTCP_MODE_TRANSMIT 0 |
Typedefs | |
typedef void( | ttcp_done_cb_t )(void *opaque, int result) |
Functions | |
cmd_state_t | cmd_ttcp (int argc, char *argv[], void *ctx) |
static err_t | tcp_accept_cb (void *arg, struct tcp_pcb *newpcb, err_t err) |
Only used in TCP mode. More... | |
static void | tcp_conn_err_cb (void *arg, err_t err) |
Only used in TCP mode. More... | |
static err_t | tcp_connect_cb (void *arg, struct tcp_pcb *tpcb, err_t err) |
Only used in TCP mode. More... | |
static err_t | tcp_recv_cb (void *arg, struct tcp_pcb *pcb, struct pbuf *p, err_t err) |
Only used in TCP mode. More... | |
static void | tcp_send_data (struct ttcp *ttcp) |
Only used in TCP mode. More... | |
static int | tcp_start (struct ttcp *ttcp) |
Start TCP transfer. More... | |
static void | tcp_timeout_cb (void *ctx) |
Only used in TCP mode. More... | |
static void | ttcp_destroy (struct ttcp *ttcp) |
Clean up and free the ttcp structure. More... | |
static void | ttcp_done (struct ttcp *ttcp, int result) |
Invoked when transfer is done or aborted (non-zero result). More... | |
static void | ttcp_print_stats (struct ttcp *ttcp) |
Calculate bitrate based on number of bytes transmitted and elapsed time. More... | |
int | ttcp_start (struct ip_addr addr, uint16_t port, void *opaque, ttcp_done_cb_t *done_cb, int mode, uint16_t nbuf, uint16_t buflen, int udp, int verbose) |
Start a new ttcp transfer. More... | |
static void | udp_recv_cb (void *arg, struct udp_pcb *upcb, struct pbuf *p, struct ip_addr *addr, u16_t port) |
Only used in UDP mode. More... | |
static int | udp_send_bytes (struct ttcp *ttcp, uint32_t len) |
static void | udp_send_data (struct ttcp *ttcp) |
Only used in UDP mode. More... | |
static int | udp_start (struct ttcp *ttcp) |
Start UDP transfer. More... | |
static void | udp_timeout_cb (void *ctx) |
Only used in UDP mode. More... | |
Variables | |
char | usage [] |
#define TTCP_MODE_RECEIVE 1 |
Referenced by cmd_ttcp(), and ttcp_start().
#define TTCP_MODE_TRANSMIT 0 |
Referenced by cmd_ttcp(), tcp_start(), ttcp_print_stats(), ttcp_start(), and udp_start().
typedef void( ttcp_done_cb_t)(void *opaque, int result) |
cmd_state_t cmd_ttcp | ( | int | argc, |
char * | argv[], | ||
void * | ctx | ||
) |
References ttcp::buflen, c, CMD_DONE, ctx, getopt(), mode, ttcp::nbuf, net_cfg::netif, netif_is_up, NULL, optarg, optind, ttcp::port, printk(), str2ip(), TTCP_MODE_RECEIVE, TTCP_MODE_TRANSMIT, ttcp_start(), ttcp::udp, and ttcp::verbose.
Referenced by wl_init_complete_cb().
Only used in TCP mode.
References arg, ERR_OK, printk(), ttcp::start_time, tcp_conn_err_cb(), tcp_recv_cb(), timer_get_ms(), and ttcp::tpcb.
Referenced by tcp_start().
|
static |
Only used in TCP mode.
References arg, NULL, printk(), ttcp::tpcb, and ttcp_done().
Referenced by tcp_accept_cb(), and tcp_start().
Only used in TCP mode.
References arg, ERR_OK, printk(), ttcp::start_time, tcp_send_data(), and timer_get_ms().
Referenced by tcp_start().
Only used in TCP mode.
References arg, ERR_OK, NULL, pbuf_free(), ttcp::print_cnt, printk(), ttcp::recved, pbuf::tot_len, ttcp_done(), and ttcp::verbose.
Referenced by tcp_accept_cb(), and tcp_start().
|
static |
Only used in TCP mode.
Will transmit a maximum of pbuf->tot_len bytes. Called upon connect and when there's space available in the TCP send window
References ttcp::buflen, ERR_MEM, ERR_OK, ttcp::left, ttcp::payload, printk(), tcp_timeout_cb(), ttcp::tid, TIMEOUT_ONESHOT, timer_sched_timeout_cb(), and ttcp::tpcb.
Referenced by tcp_connect_cb(), and tcp_timeout_cb().
|
static |
Start TCP transfer.
References ttcp::addr, ttcp::buflen, ERR_OK, ttcp::lpcb, ttcp::mode, NULL, ttcp::payload, ttcp::port, printk(), tcp_accept_cb(), tcp_conn_err_cb(), tcp_connect_cb(), tcp_recv_cb(), ttcp::tpcb, and TTCP_MODE_TRANSMIT.
Referenced by ttcp_start().
|
static |
Only used in TCP mode.
Scheduled by tcp_send_data(). tcp_sent() is not used for performance reasons.
References ctx, ttcp::left, ttcp::print_cnt, printk(), tcp_send_data(), ttcp::tid, TIMEOUT_ONESHOT, timer_sched_timeout_cb(), ttcp::tpcb, ttcp_done(), and ttcp::verbose.
Referenced by tcp_send_data().
|
static |
Clean up and free the ttcp structure.
References ttcp::lpcb, NULL, ttcp::payload, ttcp::tid, timer_cancel_timeout(), ttcp::tpcb, and ttcp::upcb.
Referenced by ttcp_done(), and ttcp_start().
|
static |
Invoked when transfer is done or aborted (non-zero result).
References ttcp::done_cb, ttcp::opaque, ttcp_destroy(), and ttcp_print_stats().
Referenced by tcp_conn_err_cb(), tcp_recv_cb(), tcp_timeout_cb(), udp_recv_cb(), and udp_send_data().
|
static |
Calculate bitrate based on number of bytes transmitted and elapsed time.
References ttcp::buflen, ttcp::mode, ttcp::nbuf, printk(), ttcp::recved, ttcp::start_time, timer_get_ms(), TTCP_MODE_TRANSMIT, ttcp::udp, and ttcp::verbose.
Referenced by ttcp_done().
int ttcp_start | ( | struct ip_addr | addr, |
uint16_t | port, | ||
void * | opaque, | ||
ttcp_done_cb_t * | done_cb, | ||
int | mode, | ||
uint16_t | nbuf, | ||
uint16_t | buflen, | ||
int | udp, | ||
int | verbose | ||
) |
Start a new ttcp transfer.
It should be possible to call this function multiple times in order to get multiple ttcp streams. done_cb() will be invoked upon completion.
References ttcp::addr, ttcp::buflen, ttcp::done_cb, ttcp::left, ttcp::mode, mode, ttcp::nbuf, NULL, ttcp::opaque, ttcp::port, printk(), status, tcp_start(), ttcp_destroy(), TTCP_MODE_RECEIVE, TTCP_MODE_TRANSMIT, ttcp::udp, udp_start(), and ttcp::verbose.
Referenced by cmd_ttcp().
|
static |
Only used in UDP mode.
Will finalize the ttcp process when an end marker is seen.
References arg, out, pbuf_free(), ttcp::print_cnt, printk(), ttcp::recved, ttcp::start_time, timer_get_ms(), pbuf::tot_len, ttcp_done(), ttcp::udp_started, and ttcp::verbose.
Referenced by udp_start().
|
static |
References ERR_OK, NULL, pbuf_alloc(), pbuf_free(), PBUF_RAM, PBUF_TRANSPORT, printk(), and ttcp::upcb.
Referenced by udp_send_data().
|
static |
Only used in UDP mode.
First call will send the start marker. When all ttcp data has been sent, a number of end markers will be sent. After end marker transmission, this function will complete the ttcp process.
References ttcp::buflen, ttcp::left, ttcp::start_time, ttcp::tid, TIMEOUT_ONESHOT, timer_get_ms(), timer_sched_timeout_cb(), ttcp_done(), ttcp::udp_end_marker_left, udp_send_bytes(), ttcp::udp_started, and udp_timeout_cb().
Referenced by udp_start(), and udp_timeout_cb().
|
static |
Start UDP transfer.
References ttcp::addr, ERR_OK, ttcp::mode, NULL, ttcp::port, printk(), TTCP_MODE_TRANSMIT, ttcp::udp_end_marker_left, udp_recv_cb(), udp_send_data(), and ttcp::upcb.
Referenced by ttcp_start().
|
static |
Only used in UDP mode.
Scheduled after data has been sent in udp_send_data() if we have more data to send.
References ctx, and udp_send_data().
Referenced by udp_send_data().
char usage[] |