UC3 USART in SPI mode driver functions.
Copyright (c) 2014-2018 Microchip Technology Inc. and its subsidiaries.
Functions | |
void | usart_spi_deselect_device (volatile avr32_usart_t *p_usart, struct usart_spi_device *device) |
De-select the given device on the SPI bus. More... | |
void | usart_spi_init (volatile avr32_usart_t *p_usart) |
Enable the USART system clock in SPI master mode. More... | |
uint32_t | usart_spi_is_rx_full (volatile avr32_usart_t *p_usart) |
Check if both receive buffers are full. More... | |
uint32_t | usart_spi_is_rx_ready (volatile avr32_usart_t *p_usart) |
Check whether the USART in SPI master mode contains a received character. More... | |
uint32_t | usart_spi_is_tx_empty (volatile avr32_usart_t *p_usart) |
Check whether there are data in Transmit Holding Register or Transmit Shift Register in SPI master mode. More... | |
uint32_t | usart_spi_is_tx_ready (volatile avr32_usart_t *p_usart) |
Check if the USART Transmit Holding Register is empty or not in SPI mode. More... | |
uint32_t | usart_spi_read_packet (volatile avr32_usart_t *p_usart, uint8_t *data, size_t len) |
Receive a sequence of bytes from a USART in SPI mode device. More... | |
void | usart_spi_read_single (volatile avr32_usart_t *p_usart, uint8_t *data) |
Receive one byte from an SPI device using USART in SPI mode. More... | |
void | usart_spi_select_device (volatile avr32_usart_t *p_usart, struct usart_spi_device *device) |
Select the given device on the SPI bus. More... | |
void | usart_spi_setup_device (volatile avr32_usart_t *p_usart, struct usart_spi_device *device, spi_flags_t flags, unsigned long baud_rate, board_spi_select_id_t sel_id) |
Set up a USART in SPI master mode device. More... | |
uint32_t | usart_spi_write_packet (volatile avr32_usart_t *p_usart, const uint8_t *data, size_t len) |
Send a sequence of bytes to an SPI device using USART in SPI mode. More... | |
void | usart_spi_write_single (volatile avr32_usart_t *p_usart, uint8_t data) |
Write one byte to an SPI device using USART in SPI mode. More... | |
void usart_spi_deselect_device | ( | volatile avr32_usart_t * | p_usart, |
struct usart_spi_device * | device | ||
) |
De-select the given device on the SPI bus.
p_usart | Base address of the USART instance. |
device | SPI device. |
References UNUSED().
Referenced by at25dfx_spi_deselect_device().
void usart_spi_init | ( | volatile avr32_usart_t * | p_usart | ) |
Enable the USART system clock in SPI master mode.
p_usart | Pointer to Base address of the USART instance. |
References sysclk_enable_pba_module(), SYSCLK_USART0, SYSCLK_USART1, SYSCLK_USART2, and SYSCLK_USART3.
Referenced by at25dfx_spi_init(), at45dbx_spi_init(), and ili9341_interface_init().
uint32_t usart_spi_is_rx_full | ( | volatile avr32_usart_t * | p_usart | ) |
Check if both receive buffers are full.
p_usart | Base address of the USART instance. |
1 | Receive buffers are full. |
0 | Receive buffers are not full. |
uint32_t usart_spi_is_rx_ready | ( | volatile avr32_usart_t * | p_usart | ) |
Check whether the USART in SPI master mode contains a received character.
p_usart | Base address of the USART instance. |
1 | Some data have been received. |
0 | No data has been received. |
uint32_t usart_spi_is_tx_empty | ( | volatile avr32_usart_t * | p_usart | ) |
Check whether there are data in Transmit Holding Register or Transmit Shift Register in SPI master mode.
p_usart | Base address of the USART instance. |
1 | The two registers are empty. |
0 | One of the two registers contains data. |
References usart_tx_empty().
Referenced by ili9341_wait_for_send_done().
uint32_t usart_spi_is_tx_ready | ( | volatile avr32_usart_t * | p_usart | ) |
Check if the USART Transmit Holding Register is empty or not in SPI mode.
p_usart | Base address of the USART instance. |
1 | There is no data in the Transmit Holding Register. |
0 | There are data in the Transmit Holding Register. |
References usart_tx_ready().
uint32_t usart_spi_read_packet | ( | volatile avr32_usart_t * | p_usart, |
uint8_t * | data, | ||
size_t | len | ||
) |
Receive a sequence of bytes from a USART in SPI mode device.
All bytes sent out on usart bus are sent as value 0.
p_usart | Base address of the usart instance. |
data | Data buffer to put read data. |
len | Length of data. |
References CONFIG_USART_SPI_DUMMY, i, usart_getchar(), usart_putchar(), and val.
Referenced by at25dfx_spi_read_byte(), and at25dfx_spi_read_packet().
void usart_spi_read_single | ( | volatile avr32_usart_t * | p_usart, |
uint8_t * | data | ||
) |
Receive one byte from an SPI device using USART in SPI mode.
p_usart | Base address of the USART instance. |
data | Pointer to the data byte where to store the received data. |
References CONFIG_USART_SPI_DUMMY, usart_getchar(), and usart_putchar().
Referenced by ili9341_read_byte().
void usart_spi_select_device | ( | volatile avr32_usart_t * | p_usart, |
struct usart_spi_device * | device | ||
) |
Select the given device on the SPI bus.
p_usart | Base address of the USART instance. |
device | SPI device. |
References UNUSED().
Referenced by at25dfx_spi_select_device().
void usart_spi_setup_device | ( | volatile avr32_usart_t * | p_usart, |
struct usart_spi_device * | device, | ||
spi_flags_t | flags, | ||
unsigned long | baud_rate, | ||
board_spi_select_id_t | sel_id | ||
) |
Set up a USART in SPI master mode device.
The returned device descriptor structure must be passed to the driver whenever that device should be used as current slave device.
p_usart | Base address of the USART instance. |
device | Pointer to usart device struct that should be initialized. |
flags | USART configuration flags. Common flags for all implementations are the usart modes, which should be SPI_MODE_0, SPI_MODE_1, SPI_MODE_2, SPI_MODE_3. |
baud_rate | Baud rate for communication with slave device in Hz. |
sel_id | Board specific select id. |
References opt, sysclk_get_cpu_hz(), UNUSED(), and USART_NORMAL_CHMODE.
Referenced by at25dfx_spi_init(), and ili9341_interface_init().
uint32_t usart_spi_write_packet | ( | volatile avr32_usart_t * | p_usart, |
const uint8_t * | data, | ||
size_t | len | ||
) |
Send a sequence of bytes to an SPI device using USART in SPI mode.
Received bytes on the USART in SPI mode are discarded.
p_usart | Base address of the USART instance. |
data | Data buffer to write. |
len | Length of data. |
References i, usart_getchar(), and usart_putchar().
Referenced by at25dfx_spi_write_byte(), and at25dfx_spi_write_packet().
void usart_spi_write_single | ( | volatile avr32_usart_t * | p_usart, |
uint8_t | data | ||
) |
Write one byte to an SPI device using USART in SPI mode.
p_usart | Base address of the USART instance. |
data | The data to be sent out. |
References usart_putchar().
Referenced by ili9341_send_byte().