#include "conf_audio_mixer.h"
#include "conf_audio_player.h"
#include "conf_usb.h"
#include "audio_mixer.h"
Data Structures | |
struct | usb_stream_context_t |
Macros | |
#define | PPM(value, ppm) ( ((int)( (long long)value*(ppm)/1000000) ) ) |
Compute the PPM of a number. More... | |
#define | PPM_ADD(value, ppm) ( ((int)(value + (long long)value*(ppm)/1000000)) ) |
Add x PPM to a value. More... | |
#define | PPM_SUB(value, ppm) ( ((int)(value - (long long)value*(ppm)/1000000)) ) |
Remove x PPM to a value. More... | |
#define | USB_STREAM_REAL_BUFFER_SIZE (USB_STREAM_BUFFER_SIZE) |
Real size of the buffer, i.e. taking into account the possible data 'expansion'. More... | |
Functions | |
void | adc_sample_sent_cb (void) |
void | adc_underflow_cb (void) |
void | dac_sample_sent_cb (void) |
This callback function is called when the DAC interrupt has sent the buffer 'n-1' and switches to buffer 'n'. More... | |
void | dac_underflow_cb (void) |
This callback function is called when the PWM DAC interrupt does not have any more audio samples (i.e. More... | |
void | player_init (void) |
void | player_shutdown (void) |
static __always_inline void | usb_stream_fifo_get (void **pp_buffer, uint16_t *p_size) |
This function gets from the audio stream FIFO the next buffer to read. More... | |
static __always_inline int8_t * | usb_stream_fifo_get_buffer (uint8_t index) |
This function returns the pointer on a buffer according to its index. More... | |
static __always_inline int | usb_stream_fifo_get_free_room (void) |
This function returns the number of free buffers in the USB stream FIFO. More... | |
static __always_inline int | usb_stream_fifo_get_used_room (void) |
This function returns the number of used buffers in the USB stream FIFO. More... | |
static __always_inline void | usb_stream_fifo_pull (void) |
This function increases the read index of the FIFO. More... | |
static __always_inline void | usb_stream_fifo_push (uint16_t size) |
This function put into the audio stream FIFO a new buffer and increases the write index of the FIFO. More... | |
uint32_t | usb_stream_get_buffer_level (void) |
This function returns the number of full buffers. More... | |
uint16_t | usb_stream_get_counter (void) |
This function returns the internal audio counter. More... | |
uint16_t | usb_stream_get_stream_status (void) |
This function returns the audio status. More... | |
void | usb_stream_init (uint32_t sample_rate_hz, uint8_t num_channels, uint8_t bits_per_sample, bool swap_channels) |
This function initializes the USB Stream driver. More... | |
int | usb_stream_input (usb_stream_side_t side, uint8_t pipe_in, uint32_t *pFifoCount) |
This function takes the stream coming from the selected USB pipe and sends it to the DAC driver. More... | |
bool | usb_stream_new_sample_rate (uint32_t sample_rate) |
Sync the sample rate of the audio output stream with the USB stream. More... | |
int32_t | usb_stream_ppm_get (void) |
This function returns the PPM differences between the input audio stream frequency and the DAC output frequency. More... | |
void | usb_stream_resync (void) |
This function ensures that no underflow/underflow will never occur by adjusting the SSC/ABDAC frequencies. More... | |
Variables | |
usb_stream_context_t * | usb_stream_context |
#define PPM | ( | value, | |
ppm | |||
) | ( ((int)( (long long)value*(ppm)/1000000) ) ) |
Compute the PPM of a number.
#define PPM_ADD | ( | value, | |
ppm | |||
) | ( ((int)(value + (long long)value*(ppm)/1000000)) ) |
Add x PPM to a value.
#define PPM_SUB | ( | value, | |
ppm | |||
) | ( ((int)(value - (long long)value*(ppm)/1000000)) ) |
Remove x PPM to a value.
#define USB_STREAM_REAL_BUFFER_SIZE (USB_STREAM_BUFFER_SIZE) |
Real size of the buffer, i.e. taking into account the possible data 'expansion'.
Referenced by usb_stream_input().
enum usb_stream_side_t |
void adc_sample_sent_cb | ( | void | ) |
void adc_underflow_cb | ( | void | ) |
References b_microphone_started.
void dac_sample_sent_cb | ( | void | ) |
This callback function is called when the DAC interrupt has sent the buffer 'n-1' and switches to buffer 'n'.
The aim of this function is thus to prepare the buffer 'n+1'; so that there is always a pending buffer for the interrupt.
References audio_mixer_dacs_output_direct(), usb_stream_context_t::bits_per_sample, buffer, usb_stream_context_t::channel_count, usb_stream_context_t::status, usb_stream_context_t::synchronized, USB_STREAM_ERROR_NOT_SYNCHRONIZED, USB_STREAM_ERROR_UNDERFLOW, usb_stream_fifo_get(), usb_stream_fifo_get_used_room(), and usb_stream_fifo_pull().
void dac_underflow_cb | ( | void | ) |
This callback function is called when the PWM DAC interrupt does not have any more audio samples (i.e.
"famine").
References usb_stream_context_t::status, usb_stream_context_t::synchronized, USB_STREAM_ERROR_NOT_SYNCHRONIZED, and USB_STREAM_ERROR_UNDERFLOW.
void player_init | ( | void | ) |
References i, j, USB_STREAM_ERROR_NONE, and USB_STREAM_ERROR_UNSUPPORTED.
Referenced by device_audio_task_init().
void player_shutdown | ( | void | ) |
References audio_mixer_dacs_flush_direct(), i, j, NULL, and usb_stream_close().
|
static |
This function gets from the audio stream FIFO the next buffer to read.
Note that it does not increase the read index of the FIFO.
pp_buffer | (return parameter) Pointer to the buffer address to update. |
p_size | (return parameter) Pointer to the size of the buffer. |
References usb_stream_context_t::audio_buffer, usb_stream_context_t::audio_buffer_size, usb_stream_context_t::rd_id, and USB_STREAM_BUFFER_NUMBER.
Referenced by dac_sample_sent_cb(), and usb_stream_input().
|
static |
This function returns the pointer on a buffer according to its index.
index | Index of the buffer |
pointer
on buffer References usb_stream_context_t::audio_buffer, and USB_STREAM_BUFFER_NUMBER.
Referenced by usb_stream_input().
|
static |
This function returns the number of free buffers in the USB stream FIFO.
number
of free buffers. References USB_STREAM_BUFFER_NUMBER, and usb_stream_fifo_get_used_room().
|
static |
This function returns the number of used buffers in the USB stream FIFO.
number
of used buffers. References audio_mixer_dacs_output_direct(), NULL, usb_stream_context_t::rd_id, USB_STREAM_BUFFER_NUMBER, and usb_stream_context_t::wr_id.
Referenced by dac_sample_sent_cb(), usb_stream_fifo_get_free_room(), usb_stream_get_buffer_level(), usb_stream_input(), and usb_stream_resync().
|
static |
This function increases the read index of the FIFO.
References usb_stream_context_t::rd_id, and USB_STREAM_BUFFER_NUMBER.
Referenced by dac_sample_sent_cb(), and usb_stream_input().
|
static |
This function put into the audio stream FIFO a new buffer and increases the write index of the FIFO.
size | Size of the buffer. |
References usb_stream_context_t::audio_buffer_size, USB_STREAM_BUFFER_NUMBER, and usb_stream_context_t::wr_id.
Referenced by usb_stream_input().
uint32_t usb_stream_get_buffer_level | ( | void | ) |
This function returns the number of full buffers.
References usb_stream_count_nb_buffer(), and usb_stream_fifo_get_used_room().
uint16_t usb_stream_get_counter | ( | void | ) |
This function returns the internal audio counter.
References usb_stream_cnt.
uint16_t usb_stream_get_stream_status | ( | void | ) |
This function returns the audio status.
References usb_stream_context_t::status.
void usb_stream_init | ( | uint32_t | sample_rate_hz, |
uint8_t | num_channels, | ||
uint8_t | bits_per_sample, | ||
bool | swap_channels | ||
) |
This function initializes the USB Stream driver.
References usb_stream_context_t::audio_buffer_size, audio_mixer_dacs_setup_direct(), bits_per_sample, usb_stream_context_t::bits_per_sample, BROKEN_STREAM_TIMER, usb_stream_context_t::channel_count, dsp16_resampling_options_t::coefficients_generation, cpu_ms_2_cy(), cpu_set_timeout(), cpu_stop_timeout(), dsp16_resampling_get_output_max_buffer_size(), dsp16_resampling_setup(), dsp16_resampling_options_t::dynamic, FCPU_HZ, i, max, num_channels, usb_stream_context_t::rd_id, usb_stream_context_t::sample_rate, sample_rate_hz, usb_stream_context_t::status, swap_channels, usb_stream_context_t::synchronized, USB_STREAM_BUFFER_NUMBER, usb_stream_close(), USB_STREAM_ERROR_NONE, USB_STREAM_ERROR_UNSUPPORTED, usb_stream_resync_b_acting, usb_stream_resync_frequency, and usb_stream_context_t::wr_id.
Referenced by audio_speaker_set_sample_freq(), device_audio_task_init(), and usb_stream_new_sample_rate().
int usb_stream_input | ( | usb_stream_side_t | side, |
uint8_t | pipe_in, | ||
uint32_t * | pFifoCount | ||
) |
This function takes the stream coming from the selected USB pipe and sends it to the DAC driver.
Moreover, it ensures that both input and output stream keep synchronized by adding or deleting samples.
side | USB_STREAM_HOST for USB host, USB_STREAM_DEVICE for device. |
pipe_in | Number of the addressed pipe |
pFifoCount | (return parameter) NULL or pointer to the number of used buffers at this time |
Moreover, it ensures that both input and output stream keep synchronized by adding or deleting samples.
side | USB_STREAM_HOST for USB host, USB_STREAM_DEVICE for device. |
pipe_in | Number of the addressed pipe/endpoint |
pFifoCount | (return parameter) NULL or pointer to the number of used buffers at this time |
References _32_BITS_RATIO, abs, audio_mixer_dacs_output_direct(), usb_stream_context_t::bits_per_sample, BROKEN_STREAM_TIMER, buffer, usb_stream_context_t::channel_count, cpu_is_timeout(), cpu_is_timer_stopped(), cpu_ms_2_cy(), cpu_set_timeout(), cpu_stop_timeout(), cpu_us_2_cy(), CS2200_FREF, cs2200_freq_clk_out(), FCPU_HZ, for(), Host_byte_count, host_read_p_rxpacket(), Host_reset_pipe_fifo_access, i, Min, NULL, PPM, UnionPtr::s16ptr, UnionPtr::s32ptr, UnionPtr::s8ptr, usb_stream_context_t::sample_rate, usb_stream_context_t::status, swap16, swap32, usb_stream_context_t::synchronized, TIMER_USB_RESYNC_CORRECTION, TIMER_USB_STREAM_MONITOR, Usb_byte_count, usb_read_ep_rxpacket(), Usb_reset_endpoint_fifo_access, USB_STREAM_BUFFER_NUMBER, usb_stream_cnt, usb_stream_count_nb_buffer(), USB_STREAM_DEVICE, USB_STREAM_ERROR_BROKEN_STREAM, USB_STREAM_ERROR_NO_DATA, USB_STREAM_ERROR_NONE, USB_STREAM_ERROR_NOT_SYNCHRONIZED, USB_STREAM_ERROR_OVERFLOW, usb_stream_fifo_get(), usb_stream_fifo_get_buffer(), usb_stream_fifo_get_used_room(), usb_stream_fifo_pull(), usb_stream_fifo_push(), usb_stream_fill_input_buffers(), USB_STREAM_HOST, USB_STREAM_REAL_BUFFER_SIZE, usb_stream_real_sample_freq, usb_stream_resync(), usb_stream_resync_b_acting, usb_stream_resync_freq_ofst, usb_stream_resync_frequency, usb_stream_resync_last_room, usb_stream_resync_ppm, usb_stream_resync_ppm_ofst, USB_STREAM_RESYNC_PPM_STEPS, usb_stream_resync_step, and usb_stream_context_t::wr_id.
Referenced by device_audio_task().
bool usb_stream_new_sample_rate | ( | uint32_t | sample_rate | ) |
Sync the sample rate of the audio output stream with the USB stream.
false | The new sample rate already matches the current settings. |
true | The output sample rate was changed. |
References audio_mixer_dacs_flush_direct(), and usb_stream_init().
int32_t usb_stream_ppm_get | ( | void | ) |
This function returns the PPM differences between the input audio stream frequency and the DAC output frequency.
Note that this information should only be considered as an indication, for debug or visual effect for example.
References usb_stream_resync_ppm, and usb_stream_resync_ppm_ofst.
Referenced by mmi_activity_display().
void usb_stream_resync | ( | void | ) |
This function ensures that no underflow/underflow will never occur by adjusting the SSC/ABDAC frequencies.
This function ensures that no underflow/underflow will never occur by adjusting the SSC/ABDAC frequencies.
This will ensures that no underflow/underflow will never occur by inserting/removing samples.
References _32_BITS_RATIO, abs, cpu_is_timeout(), cpu_ms_2_cy(), cpu_set_timeout(), CS2200_FREF, cs2200_freq_clk_adjust(), FCPU_HZ, PPM_ADD, usb_stream_context_t::sample_rate, usb_stream_context_t::synchronized, TIMER_USB_RESYNC_CORRECTION, TIMER_USB_STREAM_MONITOR, USB_STREAM_BUFFER_NUMBER, usb_stream_fifo_get_used_room(), usb_stream_real_sample_freq, usb_stream_resync_b_acting, usb_stream_resync_freq_ofst, usb_stream_resync_last_room, usb_stream_resync_ppm, usb_stream_resync_ppm_ofst, USB_STREAM_RESYNC_PPM_STEPS, usb_stream_resync_step, and usb_stream_task().
Referenced by device_audio_task(), and usb_stream_input().
usb_stream_context_t* usb_stream_context |