See Quick start guide for Calendar service.
This is the common API for a calendar service. It provides functionality to convert UNIX timestamps to dates and back. It also provides functionality for calculating the difference between dates and converting timestamps to dates with different time zones and back.
Modules | |
Quick Start Guide(s) | |
In this section you can find a list of all Quick Start guides related to the Calendar service. | |
Data Structures | |
struct | calendar_date |
Calendar structure to hold a date. More... | |
Functions | |
void | calendar_add_second_to_date (struct calendar_date *date) |
Increments a date with one second. More... | |
uint32_t | calendar_date_to_timestamp (struct calendar_date *date) |
Convert a date to a UNIX timestamp. More... | |
uint32_t | calendar_date_to_timestamp_tz (struct calendar_date *date, int8_t hour, uint8_t min) |
This function converts a date in a given time zone to a UNIX timestamp. More... | |
bool | calendar_is_date_valid (struct calendar_date *date) |
Check if a date is valid. More... | |
void | calendar_time_between_dates (struct calendar_date *date_end, struct calendar_date *date_start, struct calendar_date *date_out) |
This function calculates the time difference between to dates. More... | |
void | calendar_timestamp_to_date (uint32_t timestamp, struct calendar_date *date_out) |
Convert a UNIX timestamp to a date. More... | |
void | calendar_timestamp_to_date_tz (uint32_t timestamp, int8_t hour, uint8_t min, struct calendar_date *date_out) |
Convert a UNIX timestamp to a date in a given time zone. More... | |
void calendar_add_second_to_date | ( | struct calendar_date * | date | ) |
Increments a date with one second.
This function will add one second to specified date. If second is 59, it will increment minute.
date | The date to add a second to |
References Assert, calendar_add_minute_to_date(), calendar_is_date_valid(), and calendar_date::second.
uint32_t calendar_date_to_timestamp | ( | struct calendar_date * | date | ) |
Convert a date to a UNIX timestamp.
date | Date |
0 | if date is not valid |
References calendar_is_date_valid(), calendar_leapyear(), calendar_yearsize(), calendar_date::date, EPOCH_YEAR, calendar_date::hour, calendar_date::minute, month, calendar_date::month, calendar_date::second, SECS_PER_DAY, SECS_PER_HOUR, SECS_PER_MINUTE, while(), and calendar_date::year.
Referenced by calendar_date_to_timestamp_tz(), and calendar_time_between_dates().
uint32_t calendar_date_to_timestamp_tz | ( | struct calendar_date * | date, |
int8_t | hour, | ||
uint8_t | min | ||
) |
This function converts a date in a given time zone to a UNIX timestamp.
date | Date |
hour | Hour offset from UTC (UTC-12 to UTC+14) |
min | Minute offset from UTC (0, 15, 30, 45) |
0 | if date is not valid |
References calendar_date_to_timestamp(), SECS_PER_HOUR, and SECS_PER_MINUTE.
bool calendar_is_date_valid | ( | struct calendar_date * | date | ) |
Check if a date is valid.
Checks that number of seconds, minutes and hours is a valid value. Checks that number of days does not exceed number of days in current month. Checks that number of months is a valid value, and checks that year is between 1970 (epoch year) and 2106 (overflow year).
*date | the date to check if valid |
References calendar_leapyear(), calendar_date::date, EPOCH_YEAR, calendar_date::hour, calendar_date::minute, month, calendar_date::month, calendar_date::second, and calendar_date::year.
Referenced by calendar_add_second_to_date(), and calendar_date_to_timestamp().
void calendar_time_between_dates | ( | struct calendar_date * | date_end, |
struct calendar_date * | date_start, | ||
struct calendar_date * | date_out | ||
) |
This function calculates the time difference between to dates.
The time difference is provided as number of years, months, days, hours, minutes and seconds between the dates. If end date is before start date, the dates are switched.
date_end | The end date |
date_start | The start date |
date_out | The time between the dates |
References calendar_date_to_timestamp(), calendar_leapyear(), calendar_date::date, calendar_date::hour, calendar_date::minute, month, calendar_date::month, calendar_date::second, temp, and calendar_date::year.
void calendar_timestamp_to_date | ( | uint32_t | timestamp, |
struct calendar_date * | date_out | ||
) |
Convert a UNIX timestamp to a date.
Finds the corresponding date and time for a UNIX timestamp.
timestamp | UNIX timestamp |
date_out | Date to store result |
References calendar_leapyear(), calendar_yearsize(), calendar_date::date, calendar_date::dayofweek, EPOCH_YEAR, calendar_date::hour, calendar_date::minute, month, calendar_date::month, calendar_date::second, SECS_PER_DAY, SECS_PER_HOUR, SECS_PER_MINUTE, and calendar_date::year.
Referenced by calendar_timestamp_to_date_tz().
void calendar_timestamp_to_date_tz | ( | uint32_t | timestamp, |
int8_t | hour, | ||
uint8_t | min, | ||
struct calendar_date * | date_out | ||
) |
Convert a UNIX timestamp to a date in a given time zone.
The provided UNIX timestamp is converted to the corresponding time in the provided time zone.
timestamp | UNIX timestamp |
hour | Hour offset from UTC (UTC-12 to UTC+14) |
min | Minute offset from UTC (0, 15, 30, 45) |
date_out | Date to store result |
References calendar_timestamp_to_date(), SECS_PER_HOUR, and SECS_PER_MINUTE.