See Quick start guide for First-In-First-Out Buffer (FIFO).
These functions manages FIFOs thanks to simple a API. The FIFO can be 100% full thanks to a double-index range implementation. For example, a FIFO of 4 elements can be implemented: the FIFO can really hold up to 4 elements. This is particularly well suited for any kind of application needing a lot of small FIFO. The maximum fifo size is 128 items (uint8, uint16 or uint32). Note that the driver, thanks to its conception, does not use interrupt protection.
Modules | |
Quick Start Guide(s) | |
In this section you can find a list of all Quick Start guides related to the First-In-First-Out Buffer (FIFO). | |
Data Structures | |
struct | fifo_desc |
FIFO descriptor used by FIFO driver. More... | |
Typedefs | |
typedef struct fifo_desc | fifo_desc_t |
Enumerations | |
enum | { FIFO_OK = 0, FIFO_ERROR_OVERFLOW, FIFO_ERROR_UNDERFLOW, FIFO_ERROR } |
Error codes used by FIFO driver. More... | |
Functions | |
static void | fifo_flush (fifo_desc_t *fifo_desc) |
Flushes a software FIFO. More... | |
static uint8_t | fifo_get_free_size (fifo_desc_t *fifo_desc) |
Returns the remaining free spaces of the FIFO (in number of elements). More... | |
static uint8_t | fifo_get_used_size (fifo_desc_t *fifo_desc) |
Returns the number of elements in the FIFO. More... | |
int | fifo_init (fifo_desc_t *fifo_desc, void *buffer, uint8_t size) |
Initializes a new software FIFO for a certain 'size'. More... | |
static bool | fifo_is_empty (fifo_desc_t *fifo_desc) |
Tests if a FIFO is empty. More... | |
static bool | fifo_is_full (fifo_desc_t *fifo_desc) |
Tests if a FIFO is full. More... | |
static uint16_t | fifo_peek_uint16 (fifo_desc_t *fifo_desc) |
Gets a 16-bits element from the FIFO but does not remove it from the FIFO. More... | |
static uint32_t | fifo_peek_uint32 (fifo_desc_t *fifo_desc) |
Gets a 32-bits element from the FIFO but does not remove it from the FIFO. More... | |
static uint8_t | fifo_peek_uint8 (fifo_desc_t *fifo_desc) |
Gets a 8-bits element from the FIFO but does not remove it from the FIFO. More... | |
static int | fifo_pull_uint16 (fifo_desc_t *fifo_desc, uint16_t *item) |
Gets a 16-bits element from the FIFO and checks for a possible underflow. More... | |
static uint16_t | fifo_pull_uint16_nocheck (fifo_desc_t *fifo_desc) |
Gets a 16-bits element from the FIFO. More... | |
static int | fifo_pull_uint32 (fifo_desc_t *fifo_desc, uint32_t *item) |
Gets a 32-bits element from the FIFO and checks for a possible underflow. More... | |
static uint32_t | fifo_pull_uint32_nocheck (fifo_desc_t *fifo_desc) |
Gets a 32-bits element from the FIFO. More... | |
static int | fifo_pull_uint8 (fifo_desc_t *fifo_desc, uint8_t *item) |
Gets a 8-bits element from the FIFO and checks for a possible underflow. More... | |
static uint8_t | fifo_pull_uint8_nocheck (fifo_desc_t *fifo_desc) |
Gets a 8-bits element from the FIFO. More... | |
static int | fifo_push_uint16 (fifo_desc_t *fifo_desc, uint32_t item) |
Puts a new 16-bits element into the FIFO and checks for a possible overflow. More... | |
static void | fifo_push_uint16_nocheck (fifo_desc_t *fifo_desc, uint32_t item) |
Puts a new 16-bits element into the FIFO. More... | |
static int | fifo_push_uint32 (fifo_desc_t *fifo_desc, uint32_t item) |
Puts a new 32-bits element into the FIFO and checks for a possible overflow. More... | |
static void | fifo_push_uint32_nocheck (fifo_desc_t *fifo_desc, uint32_t item) |
Puts a new 32-bits element into the FIFO. More... | |
static int | fifo_push_uint8 (fifo_desc_t *fifo_desc, uint32_t item) |
Puts a new 8-bits element into the FIFO and checks for a possible overflow. More... | |
static void | fifo_push_uint8_nocheck (fifo_desc_t *fifo_desc, uint32_t item) |
Puts a new 8-bits element into the FIFO. More... | |
typedef struct fifo_desc fifo_desc_t |
anonymous enum |
|
inlinestatic |
Flushes a software FIFO.
fifo_desc | The FIFO descriptor. |
References fifo_desc::read_index, and fifo_desc::write_index.
|
inlinestatic |
Returns the remaining free spaces of the FIFO (in number of elements).
fifo_desc | The FIFO descriptor. |
References fifo_get_used_size(), and fifo_desc::size.
|
inlinestatic |
Returns the number of elements in the FIFO.
fifo_desc | The FIFO descriptor. |
References fifo_desc::mask, fifo_desc::read_index, and fifo_desc::write_index.
Referenced by device_cdc_task(), fifo_get_free_size(), fifo_is_full(), and fill_tx_buffer().
int fifo_init | ( | fifo_desc_t * | fifo_desc, |
void * | buffer, | ||
uint8_t | size | ||
) |
Initializes a new software FIFO for a certain 'size'.
fifo_desc | Pointer on the FIFO descriptor. |
buffer | Pointer on the FIFO buffer. |
size | Size of the buffer (unit is in number of 'elements'). It must be a 2-power and <= to 128. |
FIFO_OK | when no error occurred. |
FIFO_ERROR | when the size is not a 2-power. |
References Assert, fifo_desc::buffer, buffer, FIFO_OK, fifo_desc::mask, fifo_desc::read_index, fifo_desc::size, fifo_desc::u8ptr, and fifo_desc::write_index.
Referenced by device_cdc_task_init(), and device_generic_hid_task_init().
|
inlinestatic |
Tests if a FIFO is empty.
fifo_desc | The FIFO descriptor. |
true | when the FIFO is empty. |
false | when the FIFO is not empty. |
References fifo_desc::read_index, and fifo_desc::write_index.
Referenced by fifo_pull_uint16(), fifo_pull_uint32(), and fifo_pull_uint8().
|
inlinestatic |
Tests if a FIFO is full.
fifo_desc | The FIFO descriptor. |
true | when the FIFO is full. |
false | when the FIFO is not full. |
References fifo_get_used_size(), and fifo_desc::size.
Referenced by fifo_push_uint16(), fifo_push_uint32(), and fifo_push_uint8().
|
inlinestatic |
Gets a 16-bits element from the FIFO but does not remove it from the FIFO.
fifo_desc | The FIFO descriptor. |
item | extracted element. |
References fifo_desc::buffer, fifo_desc::mask, fifo_desc::read_index, and fifo_desc::u16ptr.
|
inlinestatic |
Gets a 32-bits element from the FIFO but does not remove it from the FIFO.
fifo_desc | The FIFO descriptor. |
item | extracted element. |
References fifo_desc::buffer, fifo_desc::mask, fifo_desc::read_index, and fifo_desc::u32ptr.
|
inlinestatic |
Gets a 8-bits element from the FIFO but does not remove it from the FIFO.
fifo_desc | The FIFO descriptor. |
item | extracted element. |
References fifo_desc::buffer, fifo_desc::mask, fifo_desc::read_index, and fifo_desc::u8ptr.
|
inlinestatic |
Gets a 16-bits element from the FIFO and checks for a possible underflow.
fifo_desc | The FIFO descriptor. |
item | extracted element. |
FIFO_OK | when no error occurred. |
FIFO_ERROR_UNDERFLOW | when the FIFO was empty. |
References barrier, fifo_desc::buffer, FIFO_ERROR_UNDERFLOW, fifo_is_empty(), FIFO_OK, fifo_desc::mask, fifo_desc::read_index, and fifo_desc::u16ptr.
|
inlinestatic |
Gets a 16-bits element from the FIFO.
fifo_desc | The FIFO descriptor. |
References barrier, fifo_desc::buffer, item, fifo_desc::mask, fifo_desc::read_index, and fifo_desc::u16ptr.
|
inlinestatic |
Gets a 32-bits element from the FIFO and checks for a possible underflow.
fifo_desc | The FIFO descriptor. |
item | extracted element. |
FIFO_OK | when no error occurred. |
FIFO_ERROR_UNDERFLOW | when the FIFO was empty. |
References barrier, fifo_desc::buffer, FIFO_ERROR_UNDERFLOW, fifo_is_empty(), FIFO_OK, fifo_desc::mask, fifo_desc::read_index, and fifo_desc::u32ptr.
|
inlinestatic |
Gets a 32-bits element from the FIFO.
fifo_desc | The FIFO descriptor. |
References barrier, fifo_desc::buffer, item, fifo_desc::mask, fifo_desc::read_index, and fifo_desc::u32ptr.
|
inlinestatic |
Gets a 8-bits element from the FIFO and checks for a possible underflow.
fifo_desc | The FIFO descriptor. |
item | extracted element. |
FIFO_OK | when no error occurred. |
FIFO_ERROR_UNDERFLOW | when the FIFO was empty. |
References barrier, fifo_desc::buffer, FIFO_ERROR_UNDERFLOW, fifo_is_empty(), FIFO_OK, fifo_desc::mask, fifo_desc::read_index, and fifo_desc::u8ptr.
Referenced by device_cdc_task(), and fill_tx_buffer().
|
inlinestatic |
Gets a 8-bits element from the FIFO.
fifo_desc | The FIFO descriptor. |
References barrier, fifo_desc::buffer, item, fifo_desc::mask, fifo_desc::read_index, and fifo_desc::u8ptr.
|
inlinestatic |
Puts a new 16-bits element into the FIFO and checks for a possible overflow.
fifo_desc | The FIFO descriptor. |
item | extracted element. |
FIFO_OK | when no error occurred. |
FIFO_ERROR_UNDERFLOW | when the FIFO was empty. |
References barrier, fifo_desc::buffer, FIFO_ERROR_OVERFLOW, fifo_is_full(), FIFO_OK, fifo_desc::mask, fifo_desc::u16ptr, and fifo_desc::write_index.
|
inlinestatic |
Puts a new 16-bits element into the FIFO.
fifo_desc | The FIFO descriptor. |
item | extracted element. |
References barrier, fifo_desc::buffer, fifo_desc::mask, fifo_desc::u16ptr, and fifo_desc::write_index.
|
inlinestatic |
Puts a new 32-bits element into the FIFO and checks for a possible overflow.
fifo_desc | The FIFO descriptor. |
item | extracted element. |
FIFO_OK | when no error occurred. |
FIFO_ERROR_UNDERFLOW | when the FIFO was empty. |
References barrier, fifo_desc::buffer, FIFO_ERROR_OVERFLOW, fifo_is_full(), FIFO_OK, fifo_desc::mask, fifo_desc::u32ptr, and fifo_desc::write_index.
|
inlinestatic |
Puts a new 32-bits element into the FIFO.
fifo_desc | The FIFO descriptor. |
item | extracted element. |
References barrier, fifo_desc::buffer, fifo_desc::mask, fifo_desc::u32ptr, and fifo_desc::write_index.
|
inlinestatic |
Puts a new 8-bits element into the FIFO and checks for a possible overflow.
fifo_desc | The FIFO descriptor. |
item | extracted element. |
FIFO_OK | when no error occurred. |
FIFO_ERROR_UNDERFLOW | when the FIFO was empty. |
References barrier, fifo_desc::buffer, FIFO_ERROR_OVERFLOW, fifo_is_full(), FIFO_OK, fifo_desc::mask, fifo_desc::u8ptr, and fifo_desc::write_index.
Referenced by int_handler_usart().
|
inlinestatic |
Puts a new 8-bits element into the FIFO.
fifo_desc | The FIFO descriptor. |
item | extracted element. |
References barrier, fifo_desc::buffer, fifo_desc::mask, fifo_desc::u8ptr, and fifo_desc::write_index.