Microchip® Advanced Software Framework

 All Data Structures Namespaces Files Functions Variables Typedefs Enumerations Enumerator Friends Macros Groups Pages
SDT028ATFT display using ILI9341 display controller

This is hardware specific configuration that configures the graphical service for use with the ILI9341 display controller and the SDT028ATFT display.

All the drawing functionality in this configuration is provided by the Generic Implementation of Graphics Primitives driver. This configuration includes information about the panel size, data type used for coordinates and color and functionality to convert RGB color to the color format native to the display.

Macros

#define GFX_COLOR(r, g, b)   ILI9341_COLOR(r, g, b)
 
#define gfx_color(r, g, b)   gfx_ili9341_color(r, g, b)
 ILI9341 display driver specific function, see gfx_ili9341_color. More...
 
#define GFX_COLOR_INVALID   GFX_COLOR(5, 5, 5)
 It is not possible to define a color that is outside the color spectrum for the ILI9341 driver, hence use a dark color as an invalid color. More...
 
#define GFX_COLOR_TRANSPARENT   GFX_COLOR(240, 0, 240)
 It is not possible to define a color that is outside the color spectrum for the ILI9341 driver, hence use a very uncommon strong magenta color as transparency mask color. More...
 
#define gfx_copy_pixels_from_screen(pixels, count)   ili9341_copy_pixels_from_screen(pixels, count)
 ILI9341 display driver specific function, see ili9341_copy_pixels_from_screen. More...
 
#define gfx_copy_pixels_to_screen(pixels, count)   ili9341_copy_pixels_to_screen(pixels, count)
 ILI9341 display driver specific function, see ili9341_copy_pixels_to_screen. More...
 
#define gfx_copy_progmem_pixels_to_screen(pixels, count)   ili9341_copy_progmem_pixels_to_screen(pixels, count)
 ILI9341 display driver specific function available for ATmega and ATXmega devices, see ili9341_copy_progmem_pixels_to_screen. More...
 
#define gfx_draw_bitmap(bmp, x, y)   gfx_generic_draw_bitmap(bmp, x, y)
 ILI9341 display driver uses generic gfx implementation for this function. More...
 
#define gfx_draw_bitmap_tiled(bmp, x1, y1, x2, y2, tile_origin_x, tile_origin_y)
 ILI9341 display driver uses generic gfx implementation for this function. More...
 
#define gfx_draw_circle(x, y, radius, color, octant_mask)   gfx_generic_draw_circle(x, y, radius, color, octant_mask)
 ILI9341 display driver uses generic gfx implementation for this function. More...
 
#define gfx_draw_filled_circle(x, y, radius, color, quadrant_mask)
 ILI9341 display driver uses generic gfx implementation for this function. More...
 
#define gfx_draw_filled_rect(x, y, width, height, color)   gfx_generic_draw_filled_rect(x, y, width, height, color)
 ILI9341 display driver uses generic gfx implementation for this function. More...
 
#define gfx_draw_horizontal_line(x, y, length, color)   gfx_generic_draw_horizontal_line(x, y, length, color)
 ILI9341 display driver uses generic gfx implementation for this function. More...
 
#define gfx_draw_line(x1, y1, x2, y2, color)   gfx_generic_draw_line(x1, y1, x2, y2, color)
 ILI9341 display driver uses generic gfx implementation for this function. More...
 
#define gfx_draw_line_pixel(x, y, color)
 ILI9341 display driver specific function, see gfx_ili9341_draw_line_pixel. More...
 
#define gfx_draw_pixel(x, y, color)   gfx_ili9341_draw_pixel(x, y, color)
 ILI9341 display driver specific function, see gfx_ili9341_draw_pixel. More...
 
#define gfx_draw_rect(x, y, width, height, color)   gfx_generic_draw_rect(x, y, width, height, color)
 ILI9341 display driver uses generic gfx implementation for this function. More...
 
#define gfx_draw_vertical_line(x, y, length, color)   gfx_generic_draw_vertical_line(x, y, length, color)
 ILI9341 display driver uses generic gfx implementation for this function. More...
 
#define gfx_duplicate_pixel(color, count)   ili9341_duplicate_pixel(color, count)
 ILI9341 display driver specific function, see ili9341_duplicate_pixel. More...
 
#define gfx_get_pixel(x, y)   gfx_ili9341_get_pixel(x, y)
 ILI9341 display driver specific function, see gfx_ili9341_get_pixel. More...
 
#define gfx_get_pixmap(pixmap, map_width, map_x, map_y, x, y, width, height)
 ILI9341 display driver uses generic gfx implementation for this function. More...
 
#define gfx_init()   gfx_ili9341_init()
 ILI9341 display driver specific function, see gfx_ili9341_init. More...
 
#define gfx_put_bitmap(bmp, map_x, map_y, x, y, width, height)   gfx_generic_put_bitmap(bmp, map_x, map_y, x, y, width, height)
 ILI9341 display driver uses generic gfx implementation for this function. More...
 
#define gfx_put_pixmap(pixmap, map_width, map_x, map_y, x, y, width, height)
 ILI9341 display driver uses generic gfx implementation for this function. More...
 
#define gfx_set_bottom_right_limit(x, y)   ili9341_set_bottom_right_limit(x, y)
 ILI9341 display driver specific function, see ili9341_set_bottom_right_limit. More...
 
#define gfx_set_ext_handler(ext_draw_handler)   gfx_generic_set_ext_handler(ext_draw_handler)
 ILI9341 display driver uses generic gfx implementation for this function. More...
 
#define gfx_set_limits(x1, y1, x2, y2)   ili9341_set_limits(x1, y1, x2, y2)
 ILI9341 display driver specific function, see ili9341_set_limits. More...
 
#define gfx_set_orientation(flags)   gfx_ili9341_set_orientation(flags)
 ILI9341 display driver specific function, see gfx_ili9341_set_orientation. More...
 
#define gfx_set_top_left_limit(x, y)   ili9341_set_top_left_limit(x, y)
 ILI9341 display driver specific function, see ili9341_set_top_left_limit. More...
 
#define gfx_sync()   gfx_generic_sync()
 ILI9341 display driver uses generic gfx implementation for this function. More...
 

Functions

gfx_color_t gfx_ili9341_color (uint8_t r, uint8_t g, uint8_t b)
 Generate native color value from R/G/B values. More...
 
void gfx_ili9341_draw_line_pixel (gfx_coord_t x, gfx_coord_t y, gfx_color_t color)
 Draw a single pixel on the screen. More...
 
void gfx_ili9341_draw_pixel (gfx_coord_t x, gfx_coord_t y, gfx_color_t color)
 Draw a single pixel on the screen. More...
 
gfx_color_t gfx_ili9341_get_pixel (gfx_coord_t x, gfx_coord_t y)
 Get the color of a pixel on the display. More...
 
void gfx_ili9341_init (void)
 Initialize the ili9341 display controller. More...
 
void gfx_ili9341_set_orientation (uint8_t flags)
 Set display orientation. More...
 

Driver-specific Definitions

typedef ili9341_color_t gfx_color_t
 Data type for color values native to the display. More...
 
typedef ili9341_coord_t gfx_coord_t
 Data type representing a coordinate on the screen. More...
 

#define GFX_COLOR (   r,
  g,
  b 
)    ILI9341_COLOR(r, g, b)
#define gfx_color (   r,
  g,
  b 
)    gfx_ili9341_color(r, g, b)

ILI9341 display driver specific function, see gfx_ili9341_color.

#define GFX_COLOR_INVALID   GFX_COLOR(5, 5, 5)

It is not possible to define a color that is outside the color spectrum for the ILI9341 driver, hence use a dark color as an invalid color.

Referenced by gfx_et024006dhu_get_pixel(), and gfx_ili9341_get_pixel().

#define GFX_COLOR_TRANSPARENT   GFX_COLOR(240, 0, 240)

It is not possible to define a color that is outside the color spectrum for the ILI9341 driver, hence use a very uncommon strong magenta color as transparency mask color.

Referenced by gfx_draw_char(), wtk_button_handler(), wtk_check_box_handler(), wtk_frame_handler(), wtk_label_handler(), and wtk_radio_button_handler().

#define gfx_copy_pixels_from_screen (   pixels,
  count 
)    ili9341_copy_pixels_from_screen(pixels, count)

ILI9341 display driver specific function, see ili9341_copy_pixels_from_screen.

#define gfx_copy_pixels_to_screen (   pixels,
  count 
)    ili9341_copy_pixels_to_screen(pixels, count)

ILI9341 display driver specific function, see ili9341_copy_pixels_to_screen.

#define gfx_copy_progmem_pixels_to_screen (   pixels,
  count 
)    ili9341_copy_progmem_pixels_to_screen(pixels, count)

ILI9341 display driver specific function available for ATmega and ATXmega devices, see ili9341_copy_progmem_pixels_to_screen.

#define gfx_draw_bitmap (   bmp,
  x,
  y 
)    gfx_generic_draw_bitmap(bmp, x, y)

ILI9341 display driver uses generic gfx implementation for this function.

See gfx_generic_draw_bitmap

#define gfx_draw_bitmap_tiled (   bmp,
  x1,
  y1,
  x2,
  y2,
  tile_origin_x,
  tile_origin_y 
)
Value:
gfx_generic_draw_bitmap_tiled(bmp, x1, y1, x2, y2,\
tile_origin_x, tile_origin_y)
void gfx_generic_draw_bitmap_tiled(const struct gfx_bitmap *bmp, gfx_coord_t x1, gfx_coord_t y1, gfx_coord_t x2, gfx_coord_t y2, gfx_coord_t tile_origin_x, gfx_coord_t tile_origin_y)
Definition: gfx_generic.c:546

ILI9341 display driver uses generic gfx implementation for this function.

See gfx_generic_draw_bitmap_tiled

#define gfx_draw_circle (   x,
  y,
  radius,
  color,
  octant_mask 
)    gfx_generic_draw_circle(x, y, radius, color, octant_mask)

ILI9341 display driver uses generic gfx implementation for this function.

See gfx_generic_draw_circle

Referenced by wtk_radio_button_handler().

#define gfx_draw_filled_circle (   x,
  y,
  radius,
  color,
  quadrant_mask 
)
Value:
quadrant_mask)
A_ALIGNED dsp32_t y[SIZE+DEN_SIZE]
The output buffer.
Definition: dsp32_iirpart/iirpart_example.c:139
A_ALIGNED dsp32_t x[SIZE+NUM_SIZE]
The input signal.
Definition: dsp32_iirpart/iirpart_example.c:142
void gfx_generic_draw_filled_circle(gfx_coord_t x, gfx_coord_t y, gfx_coord_t radius, gfx_color_t color, uint8_t quadrant_mask)
Definition: gfx_generic.c:296

ILI9341 display driver uses generic gfx implementation for this function.

See gfx_generic_draw_filled_circle

Referenced by wtk_continue_drag(), wtk_frame_handler(), wtk_radio_button_handler(), and wtk_start_drag().

#define gfx_draw_horizontal_line (   x,
  y,
  length,
  color 
)    gfx_generic_draw_horizontal_line(x, y, length, color)

ILI9341 display driver uses generic gfx implementation for this function.

See gfx_generic_draw_horizontal_line

Referenced by gfx_generic_draw_rect().

#define gfx_draw_line (   x1,
  y1,
  x2,
  y2,
  color 
)    gfx_generic_draw_line(x1, y1, x2, y2, color)

ILI9341 display driver uses generic gfx implementation for this function.

See gfx_generic_draw_line

Referenced by wtk_plot_draw(), and wtk_plot_grid_draw().

#define gfx_draw_line_pixel (   x,
  y,
  color 
)
Value:
color)
A_ALIGNED dsp32_t y[SIZE+DEN_SIZE]
The output buffer.
Definition: dsp32_iirpart/iirpart_example.c:139
void gfx_ili9341_draw_line_pixel(gfx_coord_t x, gfx_coord_t y, gfx_color_t color)
Draw a single pixel on the screen.
Definition: gfx_ili9341_sdt028atft.c:110
A_ALIGNED dsp32_t x[SIZE+NUM_SIZE]
The input signal.
Definition: dsp32_iirpart/iirpart_example.c:142

ILI9341 display driver specific function, see gfx_ili9341_draw_line_pixel.

#define gfx_draw_pixel (   x,
  y,
  color 
)    gfx_ili9341_draw_pixel(x, y, color)

ILI9341 display driver specific function, see gfx_ili9341_draw_pixel.

#define gfx_draw_rect (   x,
  y,
  width,
  height,
  color 
)    gfx_generic_draw_rect(x, y, width, height, color)

ILI9341 display driver uses generic gfx implementation for this function.

See gfx_generic_draw_rect

Referenced by wtk_button_handler(), wtk_check_box_handler(), wtk_icon_button_handler(), wtk_plot_handler(), wtk_progress_bar_handler(), and wtk_slider_handler().

#define gfx_draw_vertical_line (   x,
  y,
  length,
  color 
)    gfx_generic_draw_vertical_line(x, y, length, color)

ILI9341 display driver uses generic gfx implementation for this function.

See gfx_generic_draw_vertical_line

Referenced by gfx_generic_draw_filled_circle(), and gfx_generic_draw_rect().

#define gfx_duplicate_pixel (   color,
  count 
)    ili9341_duplicate_pixel(color, count)

ILI9341 display driver specific function, see ili9341_duplicate_pixel.

#define gfx_get_pixel (   x,
  y 
)    gfx_ili9341_get_pixel(x, y)

ILI9341 display driver specific function, see gfx_ili9341_get_pixel.

#define gfx_get_pixmap (   pixmap,
  map_width,
  map_x,
  map_y,
  x,
  y,
  width,
  height 
)
Value:
gfx_generic_get_pixmap(pixmap, map_width, map_x, map_y, x, y,\
width, height)
JDIMENSION width
Definition: jquant2.c:926
A_ALIGNED dsp32_t y[SIZE+DEN_SIZE]
The output buffer.
Definition: dsp32_iirpart/iirpart_example.c:139
void gfx_generic_get_pixmap(gfx_color_t *pixmap, gfx_coord_t map_width, gfx_coord_t map_x, gfx_coord_t map_y, gfx_coord_t x, gfx_coord_t y, gfx_coord_t width, gfx_coord_t height)
Definition: gfx_generic.c:358
A_ALIGNED dsp32_t x[SIZE+NUM_SIZE]
The input signal.
Definition: dsp32_iirpart/iirpart_example.c:142

ILI9341 display driver uses generic gfx implementation for this function.

See gfx_generic_get_pixmap

Referenced by wtk_continue_drag(), and wtk_start_drag().

#define gfx_init ( )    gfx_ili9341_init()

ILI9341 display driver specific function, see gfx_ili9341_init.

#define gfx_put_bitmap (   bmp,
  map_x,
  map_y,
  x,
  y,
  width,
  height 
)    gfx_generic_put_bitmap(bmp, map_x, map_y, x, y, width, height)

ILI9341 display driver uses generic gfx implementation for this function.

See gfx_generic_put_bitmap

#define gfx_put_pixmap (   pixmap,
  map_width,
  map_x,
  map_y,
  x,
  y,
  width,
  height 
)
Value:
gfx_generic_put_pixmap(pixmap, map_width, map_x, map_y, x, y,\
width, height)
JDIMENSION width
Definition: jquant2.c:926
A_ALIGNED dsp32_t y[SIZE+DEN_SIZE]
The output buffer.
Definition: dsp32_iirpart/iirpart_example.c:139
void gfx_generic_put_pixmap(const gfx_color_t *pixmap, gfx_coord_t map_width, gfx_coord_t map_x, gfx_coord_t map_y, gfx_coord_t x, gfx_coord_t y, gfx_coord_t width, gfx_coord_t height)
Definition: gfx_generic.c:452
A_ALIGNED dsp32_t x[SIZE+NUM_SIZE]
The input signal.
Definition: dsp32_iirpart/iirpart_example.c:142

ILI9341 display driver uses generic gfx implementation for this function.

See gfx_generic_put_pixmap

Referenced by wtk_continue_drag(), and wtk_stop_drag().

#define gfx_set_bottom_right_limit (   x,
  y 
)    ili9341_set_bottom_right_limit(x, y)

ILI9341 display driver specific function, see ili9341_set_bottom_right_limit.

#define gfx_set_ext_handler (   ext_draw_handler)    gfx_generic_set_ext_handler(ext_draw_handler)

ILI9341 display driver uses generic gfx implementation for this function.

See gfx_generic_set_ext_handler

#define gfx_set_limits (   x1,
  y1,
  x2,
  y2 
)    ili9341_set_limits(x1, y1, x2, y2)

ILI9341 display driver specific function, see ili9341_set_limits.

#define gfx_set_orientation (   flags)    gfx_ili9341_set_orientation(flags)

ILI9341 display driver specific function, see gfx_ili9341_set_orientation.

#define gfx_set_top_left_limit (   x,
  y 
)    ili9341_set_top_left_limit(x, y)

ILI9341 display driver specific function, see ili9341_set_top_left_limit.

#define gfx_sync (   void)    gfx_generic_sync()

ILI9341 display driver uses generic gfx implementation for this function.

See gfx_generic_sync

Data type for color values native to the display.

Data type representing a coordinate on the screen.

gfx_color_t gfx_ili9341_color ( uint8_t  r,
uint8_t  g,
uint8_t  b 
)

Generate native color value from R/G/B values.

Converts 8-bit R/G/B values to a color value native to the display.

The macro GFX_COLOR does the same, only allows the preprocessor to handle the calculations.

Parameters
r8-bit red value.
g8-bit green value.
b8-bit blue value.
Returns
Color value in display native format.

References GFX_COLOR.

void gfx_ili9341_draw_line_pixel ( gfx_coord_t  x,
gfx_coord_t  y,
gfx_color_t  color 
)

Draw a single pixel on the screen.

This function draws a single pixel on screen only setting top limit which makes it more suitable for line drawing. If outside the clipping region, nothing is drawn.

Parameters
xX coordinate of the pixel to be drawn.
yY coordinate of the pixel to be drawn.
colorColor value of the pixel in display native format.

References gfx_max_x, gfx_max_y, gfx_min_x, gfx_min_y, gfx_set_top_left_limit(), and ili9341_write_gram().

void gfx_ili9341_draw_pixel ( gfx_coord_t  x,
gfx_coord_t  y,
gfx_color_t  color 
)

Draw a single pixel on the screen.

Draw a single pixel on screen setting top and bottom limits. If outside the clipping region, nothing is drawn.

Parameters
xX coordinate of the pixel to be drawn.
yY coordinate of the pixel to be drawn.
colorColor value of the pixel in display native format.

References gfx_max_x, gfx_max_y, gfx_min_x, gfx_min_y, gfx_set_limits(), and ili9341_write_gram().

gfx_color_t gfx_ili9341_get_pixel ( gfx_coord_t  x,
gfx_coord_t  y 
)

Get the color of a pixel on the display.

Parameters
xX coordinate of the pixel to be sampled.
yY coordinate of the pixel to be sampled.
Returns
Color value of the pixel at (x, y) in display native format, or GFX_COLOR_INVALID if outside the clipping region.

References gfx_bitmap::color, GFX_COLOR_INVALID, gfx_max_x, gfx_max_y, gfx_min_x, gfx_min_y, gfx_set_limits(), and ili9341_read_gram().

void gfx_ili9341_init ( void  )

Initialize the ili9341 display controller.

This function will be called when calling gfx_init. It will draw a black background to the display and enable the display backlight if available.

References GFX_COLOR_BLACK, gfx_draw_filled_rect, gfx_height, gfx_set_clipping(), gfx_width, ili9341_backlight_on(), ILI9341_DEFAULT_HEIGHT, ILI9341_DEFAULT_WIDTH, and ili9341_init().

void gfx_ili9341_set_orientation ( uint8_t  flags)