Device Class (PHDC)
Common APIs used by high level application to use this USB class.
Modules | |
Related Project(s) | |
In this section you can find all the projects related to the USB Device Interface (UDI) for Personal Healthcare. | |
Interface with USB Device Core (UDC) | |
Structures and functions required by UDC. | |
Implementation of UDI PHDC | |
Class internal implementation. | |
USB interface descriptors | |
The following structures provide predefined USB interface descriptors. | |
Data Structures | |
struct | udi_phdc_metadata_t |
Functions | |
bool | udi_phdc_senddata (udi_phdc_metadata_t *metadata, void(*callback)(uint16_t)) |
Send metadata to USB host. More... | |
void | udi_phdc_senddata_abort (void) |
Abort of send metadata to USB host. More... | |
bool | udi_phdc_waitdata (udi_phdc_metadata_t *metadata, void(*callback)(bool, uint16_t)) |
Wait metadata from USB host. More... | |
bool udi_phdc_senddata | ( | udi_phdc_metadata_t * | metadata, |
void(*)(uint16_t) | callback | ||
) |
Send metadata to USB host.
metadata | Information about metadata to send |
callback | Function to call at the end of transfer. |
1
if function was successfully done, otherwise 0
. References callback, cpu_irq_restore(), cpu_irq_save(), metadata, udi_phdc_metadata_t::qos, udi_phdc_in_trans, udi_phdc_preample_feature, udi_phdc_send_metadata(), udi_phdc_send_preamplemsg(), and USB_PHDC_QOS_LOW_GOOD.
void udi_phdc_senddata_abort | ( | void | ) |
Abort of send metadata to USB host.
References UDI_PHDC_EP_BULK_IN, UDI_PHDC_EP_INTERRUPT_IN, udi_phdc_in_trans, and USB_PHDC_QOS_LOW_GOOD.
bool udi_phdc_waitdata | ( | udi_phdc_metadata_t * | metadata, |
void(*)(bool, uint16_t) | callback | ||
) |
Wait metadata from USB host.
metadata | Information about expected metadata |
callback | Function to call at the end of transfer. |
1
if function was successfully done, otherwise 0
. References callback, cpu_irq_restore(), cpu_irq_save(), metadata, UDI_PHDC_EP_SIZE_BULK_OUT, udi_phdc_out_trans, udi_phdc_preample_feature, udi_phdc_wait_metadata(), and udi_phdc_wait_preamplemsg().
usb_phdc_classfnct_desc_t udi_phdc_desc_t::classfnct |
usb_ep_desc_t udi_phdc_desc_t::ep_bulk_in |
usb_ep_desc_t udi_phdc_desc_t::ep_bulk_out |
usb_ep_desc_t udi_phdc_desc_t::ep_int_in |
udi_phdc_fnctext_desc_t udi_phdc_desc_t::fnctext |
usb_phdc_fnctext_desc_t udi_phdc_fnctext_desc_t::header |
usb_iface_desc_t udi_phdc_desc_t::iface |
uint8_t* udi_phdc_metadata_t::metadata |
uint16_t udi_phdc_metadata_t::metadata_size |
Referenced by udi_phdc_send_metadata().
uint8_t udi_phdc_metadata_t::opaque_size |
uint8_t* udi_phdc_metadata_t::opaquedata |
uint8_t udi_phdc_metadata_t::qos |
Referenced by udi_phdc_senddata().
usb_phdc_qos_desc_t udi_phdc_desc_t::qos_bulk_in |
usb_phdc_qos_desc_t udi_phdc_desc_t::qos_bulk_out |
usb_phdc_qos_desc_t udi_phdc_desc_t::qos_int_in |
le16_t udi_phdc_fnctext_desc_t::wDevSpecializations[sizeof(tmp_wDevSpecializations)/2] |