Class internal implementation.
Data Structures | |
struct | uhi_vendor_dev_t |
Macros | |
#define | UHI_VENDOR_TIMEOUT 20000 |
Timeout on Vendor transfer. More... | |
Structure to store information about USB Device Vendor | |
static uhi_vendor_dev_t | uhi_vendor_dev |
Functions required by UHC | |
uhc_enum_status_t | uhi_vendor_install (uhc_device_t *dev) |
void | uhi_vendor_enable (uhc_device_t *dev) |
void | uhi_vendor_uninstall (uhc_device_t *dev) |
#define UHI_VENDOR_TIMEOUT 20000 |
Timeout on Vendor transfer.
Referenced by uhi_vendor_bulk_in_run(), uhi_vendor_bulk_out_run(), uhi_vendor_int_in_run(), uhi_vendor_int_out_run(), uhi_vendor_iso_in_run(), and uhi_vendor_iso_out_run().
bool uhi_vendor_bulk_in_run | ( | uint8_t * | buf, |
iram_size_t | buf_size, | ||
uhd_callback_trans_t | callback | ||
) |
Start a transfer on bulk IN.
When the transfer is finished or aborted (stall, reset, ...), the callback is called. The callback returns the transfer status and eventually the number of byte transfered.
buf | Buffer on Internal RAM to send or fill. It must be align, then use COMPILER_WORD_ALIGNED. |
buf_size | Buffer size to send or fill |
callback | NULL or function to call at the end of transfer |
1
if function was successfully done, otherwise 0
. References uhc_device_t::address, uhi_vendor_dev_t::dev, uhi_vendor_dev_t::ep_bulk_in, uhd_ep_run(), uhi_vendor_bulk_is_available(), and UHI_VENDOR_TIMEOUT.
bool uhi_vendor_bulk_is_available | ( | void | ) |
Check if a transfer on BULK is possible.
1
if possible, otherwise 0
. References uhi_vendor_dev_t::dev, uhi_vendor_dev_t::ep_bulk_in, uhi_vendor_dev_t::ep_bulk_out, and NULL.
Referenced by uhi_vendor_bulk_in_run(), and uhi_vendor_bulk_out_run().
bool uhi_vendor_bulk_out_run | ( | uint8_t * | buf, |
iram_size_t | buf_size, | ||
uhd_callback_trans_t | callback | ||
) |
Start a transfer on bulk OUT.
When the transfer is finished or aborted (stall, reset, ...), the callback is called. The callback returns the transfer status and eventually the number of byte transfered.
buf | Buffer on Internal RAM to send or fill. It must be align, then use COMPILER_WORD_ALIGNED. |
buf_size | Buffer size to send or fill |
callback | NULL or function to call at the end of transfer |
1
if function was successfully done, otherwise 0
. References uhc_device_t::address, uhi_vendor_dev_t::dev, uhi_vendor_dev_t::ep_bulk_out, uhd_ep_run(), uhi_vendor_bulk_is_available(), and UHI_VENDOR_TIMEOUT.
bool uhi_vendor_control_in_run | ( | uint8_t * | buf, |
iram_size_t | buf_size, | ||
uhd_callback_setup_end_t | callback | ||
) |
Start a transfer on control IN.
When the transfer is finished or aborted (stall, reset, ...), the callback is called. The callback returns the transfer status and eventually the number of byte transfered.
buf | Buffer on Internal RAM to send or fill. It must be align, then use COMPILER_WORD_ALIGNED. |
buf_size | Buffer size to send or fill |
callback | NULL or function to call at the end of transfer |
1
if function was successfully done, otherwise 0
. References uhc_device_t::address, usb_setup_req_t::bmRequestType, usb_setup_req_t::bRequest, uhi_vendor_dev_t::dev, NULL, uhd_setup_request(), USB_REQ_DIR_IN, USB_REQ_RECIP_INTERFACE, USB_REQ_TYPE_VENDOR, usb_setup_req_t::wIndex, usb_setup_req_t::wLength, and usb_setup_req_t::wValue.
bool uhi_vendor_control_out_run | ( | uint8_t * | buf, |
iram_size_t | buf_size, | ||
uhd_callback_setup_end_t | callback | ||
) |
Start a transfer on control OUT.
When the transfer is finished or aborted (stall, reset, ...), the callback is called. The callback returns the transfer status and eventually the number of byte transfered.
buf | Buffer on Internal RAM to send or fill. It must be align, then use COMPILER_WORD_ALIGNED. |
buf_size | Buffer size to send or fill |
callback | NULL or function to call at the end of transfer |
1
if function was successfully done, otherwise 0
. References uhc_device_t::address, usb_setup_req_t::bmRequestType, usb_setup_req_t::bRequest, uhi_vendor_dev_t::dev, NULL, uhd_setup_request(), USB_REQ_RECIP_INTERFACE, USB_REQ_TYPE_VENDOR, usb_setup_req_t::wIndex, usb_setup_req_t::wLength, and usb_setup_req_t::wValue.
void uhi_vendor_enable | ( | uhc_device_t * | dev | ) |
References uhc_device_t::address, uhi_vendor_dev_t::bInterfaceNumber, usb_setup_req_t::bmRequestType, usb_setup_req_t::bRequest, uhi_vendor_dev_t::dev, NULL, uhd_setup_request(), USB_REQ_RECIP_INTERFACE, USB_REQ_SET_INTERFACE, usb_setup_req_t::wIndex, usb_setup_req_t::wLength, and usb_setup_req_t::wValue.
uhc_enum_status_t uhi_vendor_install | ( | uhc_device_t * | dev | ) |
References uhc_device_t::address, Assert, usb_iface_desc_t::bAlternateSetting, usb_iface_desc_t::bDescriptorType, usb_iface_desc_t::bInterfaceClass, uhi_vendor_dev_t::bInterfaceNumber, usb_iface_desc_t::bInterfaceNumber, usb_iface_desc_t::bInterfaceProtocol, usb_iface_desc_t::bInterfaceSubClass, usb_iface_desc_t::bLength, uhc_device_t::conf_desc, uhi_vendor_dev_t::dev, uhc_device_t::dev_desc, uhi_vendor_dev_t::ep_bulk_in, uhi_vendor_dev_t::ep_bulk_out, uhi_vendor_dev_t::ep_int_in, uhi_vendor_dev_t::ep_int_out, uhi_vendor_dev_t::ep_iso_in, uhi_vendor_dev_t::ep_iso_out, i, usb_dev_desc_t::idProduct, usb_dev_desc_t::idVendor, le16_to_cpu, NULL, uhc_device_t::speed, UHC_ENUM_HARDWARE_LIMIT, UHC_ENUM_SOFTWARE_LIMIT, UHC_ENUM_SUCCESS, UHC_ENUM_UNSUPPORTED, uhd_ep_alloc(), USB_DT_ENDPOINT, USB_DT_INTERFACE, USB_EP_DIR_IN, USB_EP_TYPE_BULK, USB_EP_TYPE_INTERRUPT, USB_EP_TYPE_ISOCHRONOUS, USB_EP_TYPE_MASK, VENDOR_CLASS, VENDOR_PROTOCOL, VENDOR_SUBCLASS, and usb_conf_desc_t::wTotalLength.
bool uhi_vendor_int_in_run | ( | uint8_t * | buf, |
iram_size_t | buf_size, | ||
uhd_callback_trans_t | callback | ||
) |
Start a transfer on interrupt IN.
When the transfer is finished or aborted (stall, reset, ...), the callback is called. The callback returns the transfer status and eventually the number of byte transfered.
buf | Buffer on Internal RAM to send or fill. It must be align, then use COMPILER_WORD_ALIGNED. |
buf_size | Buffer size to send or fill |
callback | NULL or function to call at the end of transfer |
1
if function was successfully done, otherwise 0
. References uhc_device_t::address, uhi_vendor_dev_t::dev, uhi_vendor_dev_t::ep_int_in, uhd_ep_run(), uhi_vendor_int_is_available(), and UHI_VENDOR_TIMEOUT.
bool uhi_vendor_int_is_available | ( | void | ) |
Check if a transfer on INTERRUPT is possible.
1
if possible, otherwise 0
. References uhi_vendor_dev_t::dev, uhi_vendor_dev_t::ep_int_in, uhi_vendor_dev_t::ep_int_out, and NULL.
Referenced by uhi_vendor_int_in_run(), and uhi_vendor_int_out_run().
bool uhi_vendor_int_out_run | ( | uint8_t * | buf, |
iram_size_t | buf_size, | ||
uhd_callback_trans_t | callback | ||
) |
Start a transfer on interrupt OUT.
When the transfer is finished or aborted (stall, reset, ...), the callback is called. The callback returns the transfer status and eventually the number of byte transfered.
buf | Buffer on Internal RAM to send or fill. It must be align, then use COMPILER_WORD_ALIGNED. |
buf_size | Buffer size to send or fill |
callback | NULL or function to call at the end of transfer |
1
if function was successfully done, otherwise 0
. References uhc_device_t::address, uhi_vendor_dev_t::dev, uhi_vendor_dev_t::ep_int_out, uhd_ep_run(), uhi_vendor_int_is_available(), and UHI_VENDOR_TIMEOUT.
bool uhi_vendor_iso_in_run | ( | uint8_t * | buf, |
iram_size_t | buf_size, | ||
uhd_callback_trans_t | callback | ||
) |
Start a transfer on ISO IN.
When the transfer is finished or aborted (stall, reset, ...), the callback is called. The callback returns the transfer status and eventually the number of byte transfered.
buf | Buffer on Internal RAM to send or fill. It must be align, then use COMPILER_WORD_ALIGNED. |
buf_size | Buffer size to send or fill |
callback | NULL or function to call at the end of transfer |
1
if function was successfully done, otherwise 0
. References uhc_device_t::address, uhi_vendor_dev_t::dev, uhi_vendor_dev_t::ep_iso_in, uhd_ep_run(), uhi_vendor_iso_is_available(), and UHI_VENDOR_TIMEOUT.
bool uhi_vendor_iso_is_available | ( | void | ) |
Check if a transfer on ISO is possible.
1
if possible, otherwise 0
. References uhi_vendor_dev_t::dev, uhi_vendor_dev_t::ep_iso_in, uhi_vendor_dev_t::ep_iso_out, and NULL.
Referenced by uhi_vendor_iso_in_run(), and uhi_vendor_iso_out_run().
bool uhi_vendor_iso_out_run | ( | uint8_t * | buf, |
iram_size_t | buf_size, | ||
uhd_callback_trans_t | callback | ||
) |
Start a transfer on ISO OUT.
When the transfer is finished or aborted (stall, reset, ...), the callback is called. The callback returns the transfer status and eventually the number of byte transfered.
buf | Buffer on Internal RAM to send or fill. It must be align, then use COMPILER_WORD_ALIGNED. |
buf_size | Buffer size to send or fill |
callback | NULL or function to call at the end of transfer |
1
if function was successfully done, otherwise 0
. References uhc_device_t::address, uhi_vendor_dev_t::dev, uhi_vendor_dev_t::ep_iso_out, uhd_ep_run(), uhi_vendor_iso_is_available(), and UHI_VENDOR_TIMEOUT.
void uhi_vendor_uninstall | ( | uhc_device_t * | dev | ) |
References uhi_vendor_dev_t::dev, and NULL.
|
static |