#include "lwip/netif.h"
#include "lwip/err.h"
Functions | |
err_t | wlif_init (struct netif *netif) |
Should be called at the beginning of the program to set up the network interface. More... | |
void | wlif_poll (struct netif *netif) |
Should be called at the beginning of the program to set up the network interface.
It calls the function low_level_init() to do the actual setup of the hardware.
This function should be passed as a parameter to netif_add().
netif | the lwip network interface structure for this ethernetif |
void wlif_poll | ( | struct netif * | netif | ) |