Microchip® Advanced Software Framework

msc/device/unit_tests/unit_tests.h File Reference

Declaration of main function used by MSC unit test.

Copyright (c) 2014-2018 Microchip Technology Inc. and its subsidiaries.

Functions

void main_msc_disable (void)
 Called by MSC interface Callback running when USB Host disable MSC interface. More...
 
bool main_msc_enable (void)
 Called by MSC interface Callback running when USB Host enable MSC interface. More...
 
void main_msc_read_finish (void)
 Allows to check that a memory read access works. More...
 
void main_resume_action (void)
 Called by UDD when the USB line exit of suspend state. More...
 
void main_sof_action (void)
 Called when a start of frame is received on USB line. More...
 
void main_suspend_action (void)
 Enters the application in low power mode Callback called when USB host sets USB line in suspend state. More...
 
void main_vbus_action (bool b_high)
 Called when Vbus line state change. More...
 
void memories_initialization (void)
 Initialize the memories used by examples. More...
 

void main_msc_disable ( void  )

Called by MSC interface Callback running when USB Host disable MSC interface.

bool main_msc_enable ( void  )

Called by MSC interface Callback running when USB Host enable MSC interface.

Return values
trueif MSC startup is ok
void main_msc_read_finish ( void  )

Allows to check that a memory read access works.

References main_b_msc_read.

void main_resume_action ( void  )

Called by UDD when the USB line exit of suspend state.

Turn on a led to notify active mode Called when the USB line is resumed from the suspend state.

void main_sof_action ( void  )

Called when a start of frame is received on USB line.

Manages the leds behaviors Called when a start of frame is received on USB line each 1ms.

void main_suspend_action ( void  )

Enters the application in low power mode Callback called when USB host sets USB line in suspend state.

void main_vbus_action ( bool  b_high)

Called when Vbus line state change.

void memories_initialization ( void  )

Initialize the memories used by examples.