Atmel Software Framework Common Sensor API.
The sensor device service provides high-level interfaces and binary driver libraries for sensor devices on systems built around UC3, XMEGA, and SAM microcontrollers.
Copyright (c) 2014-2018 Microchip Technology Inc. and its subsidiaries.
#include "sensor.h"
Macros | |
#define | SENSOR_DRV_CALL(sns, fn,...) |
Driver Call Wrapper. More... | |
Functions | |
void | default_event_handler (volatile sensor_event_data_t *data, volatile void *arg) |
Default sensor event callback handler. More... | |
static bool | sensor_band_index (const sensor_caps_t *caps, int16_t band, int *index) |
Get a bandwidth table index associated with a bandwidth value. More... | |
static bool | sensor_range_index (const sensor_caps_t *caps, int16_t range, int *index) |
Get a range table index associated with a range value. More... | |
static bool | sensor_driver_unimpl (sensor_t *sensor) |
Unimplemented driver function handler. More... | |
bool | sensor_attach (sensor_t *sensor, sensor_type_t type, int num, void *aux) |
Attach a specified sensor descriptor to a sensor device. More... | |
bool | sensor_device_enum (sensor_type_t type, sensor_enum_callback func, void *arg) |
Enumerate sensor devices. More... | |
bool | sensor_device_id (sensor_t *sensor, uint32_t *id, uint8_t *ver) |
Get sensor hardware device ID. More... | |
bool | sensor_read (sensor_t *sensor, sensor_read_t type, sensor_data_t *data) |
Read sensor data. More... | |
bool | sensor_enum_bandwidth (sensor_t *sensor, const sensor_band_t **table, size_t *count) |
Enumerate sensor bandwidth settings. More... | |
bool | sensor_enum_range (sensor_t *sensor, const sensor_range_t **table, size_t *count) |
Enumerate sensor range settings. More... | |
bool | sensor_add_event (sensor_t *sensor, sensor_event_t sensor_event, sensor_event_callback handler, volatile void *arg, bool enable) |
Install a sensor event handler. More... | |
bool | sensor_calibrate (sensor_t *sensor, sensor_calibration_t caltype, int code, void *caldata) |
Calibrate a sensor device. More... | |
bool | sensor_sleep (sensor_t *sensor, int arg) |
Set a sensor device to low-power or standby mode. More... | |
bool | sensor_reset (sensor_t *sensor, int arg) |
Initiate a sensor device software reset. More... | |
bool | sensor_set_state (sensor_t *sensor, sensor_state_t mode) |
Set a sensor mode. More... | |
bool | sensor_get_state (sensor_t *sensor, sensor_state_t *mode) |
Get a sensor mode. More... | |
bool | sensor_set_threshold (sensor_t *sensor, sensor_threshold_t type, int16_t value) |
Set a sensor operational threshold. More... | |
bool | sensor_get_threshold (sensor_t *sensor, sensor_threshold_t type, int16_t *value) |
Get a sensor operational threshold. More... | |
bool | sensor_ioctl (sensor_t *sensor, sensor_command_t cmd, void *arg) |
Execute a sensor device control function. More... | |
bool | sensor_set_tap (sensor_t *sensor, sensor_tap_params_t *params) |
Set tap event parameters. More... | |
bool | sensor_selftest (sensor_t *sensor, int *test_code, void *arg) |
Activate a sensor self-test function. More... | |
const char * | sensor_api_version (void) |
Atmel Software Framework Common Sensor API version. More... | |
#define SENSOR_DRV_CALL | ( | sns, | |
fn, | |||
... | |||
) |
Driver Call Wrapper.
Referenced by sensor_add_event(), sensor_calibrate(), sensor_get_threshold(), sensor_ioctl(), sensor_read(), sensor_selftest(), sensor_set_state(), sensor_set_tap(), and sensor_set_threshold().
|
inlinestatic |
Get a bandwidth table index associated with a bandwidth value.
This utility routine, provided for internal API and driver functions, fetches the driver bandwidth table index associated with a specified bandwidth value. The table index returned in index
is undefined in the event of a false
return value.
caps | Specifies an initialized driver capabilities descriptor. |
band | A bandwidth value (Hz). |
index | The driver range table index is returned to this location. |
References sensor_caps_t::band_count, sensor_caps_t::band_table, sensor_map_t::bandwidth_Hz, and i.
Referenced by sensor_ioctl().
|
inlinestatic |
Get a range table index associated with a range value.
This utility routine, provided for internal API and driver functions, fetches the driver range table index associated with a device-specific range value. The table index returned in index
is undefined in the event of a false
return value.
caps | Specifies an initialized driver capabilities descriptor. |
range | A device-specific operational range value. |
index | The driver range table index is returned to this location. |
References i, sensor_caps_t::range_count, sensor_caps_t::range_table, and sensor_map_t::range_units.
Referenced by sensor_ioctl().