#include "conf_usb.h"
#include "compiler.h"
#include "usb_drv.h"
#include "usb_task.h"
#include "usb_descriptors.h"
#include "usb_standard_request.h"
#include "usb_device_task.h"
Functions | |
void | usb_device_task (void) |
Entry point of the USB device management. More... | |
void | usb_device_task_init (void) |
This function initializes the USB device controller. More... | |
void | usb_start_device (void) |
This function starts the USB device controller. More... | |
Variables | |
volatile bool | usb_connected |
Public : (bool) usb_connected usb_connected is set to true when VBus has been detected usb_connected is set to false otherwise. More... | |
volatile bool usb_connected |
Public : (bool) usb_connected usb_connected is set to true when VBus has been detected usb_connected is set to false otherwise.
Public: bool usb_connected usb_connected is set to true when VBus has been detected usb_connected is set to false otherwise Used with USB_DEVICE_FEATURE == true only.
Referenced by ai_hid_class_get_device_status(), usb_device_task(), usb_device_task_init(), usb_general_interrupt(), and usb_start_device().