Common Sensor Service Light and Proximity Sensor Example.
Copyright (c) 2012-2018 Microchip Technology Inc. and its subsidiaries.
Macros | |
#define | ACTIVITY_LED (LED1) /* Which LED to blink to show activity */ |
#define | LIGHT_SAMPLE_RATE (10) /* Light sensor sample rate (Hz) */ |
#define | PRINT_BANNER |
#define | PROX_CURRENT_mA (50) /* Current for proximity sensor LEDs (mA) */ |
#define | PROX_SAMPLE_RATE (10) /* Proximity sensor sample rate (Hz) */ |
#define | PROX_THRESHOLD (100) /* Manual prox sensor threshold for "near" */ |
#define | SCALED_DATA |
#define | SET_PROX_CURRENT (true) /* If true, manually set proximity current */ |
#define | SET_PROX_THRESHOLD |
Functions | |
int | main (void) |
Light & proximity sensor demo application entry. More... | |
Variables | |
static const char *const | prox_labels [4] |
Strings to display based on proximity values. More... | |
#define LIGHT_SAMPLE_RATE (10) /* Light sensor sample rate (Hz) */ |
Referenced by main().
#define PRINT_BANNER |
Referenced by main().
#define PROX_CURRENT_mA (50) /* Current for proximity sensor LEDs (mA) */ |
Referenced by main().
#define PROX_SAMPLE_RATE (10) /* Proximity sensor sample rate (Hz) */ |
Referenced by main().
#define PROX_THRESHOLD (100) /* Manual prox sensor threshold for "near" */ |
Referenced by main().
#define SCALED_DATA |
Referenced by main().
#define SET_PROX_THRESHOLD |
int main | ( | void | ) |
Light & proximity sensor demo application entry.
After initializing the Xplained platform and sensor boards, this application attaches descriptors to the ambient light and proximity sensor devices on an Xplained inertial sensor board. The sensor data, which is formatted and printed via printf() after being read, can be viewed with a serial terminal application on a machine attached to the USB interface on the Xplained board.
References ACTIVITY_LED, sensor_device_t::caps, delay_ms, sensor_desc::drv, sensor_desc::err, LED_Toggle, sensor_data_t::light, LIGHT_SAMPLE_RATE, sensor_caps_t::name, PRINT_BANNER, PROX_CURRENT_mA, prox_labels, PROX_SAMPLE_RATE, PROX_THRESHOLD, sensor_data_t::proximity, sensor_data_t::scaled, SCALED_DATA, sensor_attach(), SENSOR_CHANNEL_ALL, sensor_device_id(), sensor_get_bandwidth(), sensor_get_light(), sensor_get_proximity(), sensor_get_range(), sensor_platform_init(), sensor_set_channel(), sensor_set_current(), sensor_set_sample_rate(), sensor_set_threshold(), SENSOR_THRESHOLD_NEAR_PROXIMITY, SENSOR_TYPE_LIGHT, and SENSOR_TYPE_PROXIMITY.
|
static |
Strings to display based on proximity values.
Referenced by main().