XMEGA-A1 Xplained demo application.
Copyright (c) 2010-2018 Microchip Technology Inc. and its subsidiaries.
#include <board.h>
#include <compiler.h>
#include <gpio.h>
#include <nvm.h>
#include <sysclk.h>
#include <tc.h>
#include <conf_example.h>
#include "sound.h"
#include <util/delay.h>
Macros | |
#define | F_CPU sysclk_get_cpu_hz() |
#define | SEQUENCE_BUFFER_MAX_LENGTH 255 |
Maximum length of buffer for button press sequence. More... | |
#define | SEQUENCE_HEADER_LENGTH 2 |
Length of header for saving button presses to EEPROM. More... | |
Enumerations | |
enum | game_mode { GAME_RECORD_MODE, GAME_PLAY_MODE } |
Enumeration of game modes. More... | |
enum | sound_mode { SOUND_SAMPLES, SOUND_SINEWAVE } |
Enumeration of sound playback modes. More... | |
Functions | |
int | main (void) |
Main function. More... | |
void | timeout_callback (void) |
Timer/counter overflow interrupt callback function. More... | |
Internal application functions | |
static void | start_debounce_timer (void) |
Set up and start timer for debouncing of the push buttons. More... | |
static void | init_save_timer (void) |
Set up timer for measuring inactivity before saving. More... | |
static void | start_save_timer (void) |
Start timer for measuring inactivity before saving. More... | |
static void | play_game (uint8_t buttons, enum sound_mode soundmode, enum game_mode *gamemode) |
Compares button presses with stored game data. More... | |
static void | record_buttons (uint8_t buttons, enum sound_mode soundmode) |
Record button presses and play sound. More... | |
static void | save_gamedata (void) |
Save current game data to EEPROM. More... | |
static void | load_gamedata (void) |
Load game data from EEPROM. More... | |
Variables | |
static volatile uint8_t | save_timeout |
Counter for timeout-period before saving button sequence. More... | |
uint8_t | sequence_buffer [SEQUENCE_BUFFER_MAX_LENGTH] |
Buffer to contain the button press sequence. More... | |
uint8_t | sequence_buffer_length |
Length of currently recorded button sequence in buffer. More... | |
#define F_CPU sysclk_get_cpu_hz() |
#define SEQUENCE_BUFFER_MAX_LENGTH 255 |
Maximum length of buffer for button press sequence.
Referenced by load_gamedata(), main(), and save_gamedata().
#define SEQUENCE_HEADER_LENGTH 2 |
Length of header for saving button presses to EEPROM.
Referenced by main(), play_game(), and record_buttons().
enum game_mode |
enum sound_mode |
|
static |
Set up timer for measuring inactivity before saving.
The timer/counter is set up in normal, up-counting mode with a period of approximately 1.6 seconds.
References PMIC_LVL_LOW, sysclk_get_per_hz(), tc_enable(), tc_set_overflow_interrupt_callback(), tc_set_overflow_interrupt_level(), tc_write_period(), timeout_callback(), and TIMEOUT_TIMER_MODULE.
Referenced by main().
|
static |
Load game data from EEPROM.
References nvm_eeprom_read_byte(), sequence_buffer, and SEQUENCE_BUFFER_MAX_LENGTH.
Referenced by main().
int main | ( | void | ) |
Main function.
Initializes the board, checks the jumper configuration and sets up the game accordingly before the main loop is entered. The main loop is where the state of the board buttons is read out and passed on to the game functions record_buttons or play_game, depending on the state of the game.
References board_init(), cpu_irq_enable, GAME_PLAY_MODE, GAME_RECORD_MODE, GAMEMODE_GROUND_PIN, GAMEMODE_SENSE_PIN, get_board_button_mask(), gpio_configure_pin, gpio_pin_is_low, init_save_timer(), IOPORT_DIR_INPUT, IOPORT_DIR_OUTPUT, IOPORT_INIT_LOW, IOPORT_PULL_UP, load_gamedata(), play_game(), pmic_enable_level(), PMIC_LVL_LOW, record_buttons(), save_gamedata(), save_timeout, sequence_buffer, sequence_buffer_length, SEQUENCE_BUFFER_MAX_LENGTH, SEQUENCE_HEADER_LENGTH, sound_init(), SOUND_SAMPLES, SOUND_SINEWAVE, SOUNDMODE_GROUND_PIN, SOUNDMODE_SENSE_PIN, start_debounce_timer(), start_save_timer(), sysclk_init(), and write_board_led_mask().
|
static |
Compares button presses with stored game data.
Uses a timer to debounce buttons. The method used requires the function to be called often, but not necessarily regularly.
buttons | Mask with pressed buttons. |
soundmode | Indicates whether to play a sound sample or sinewave. |
gamemode | Game mode pointer – the mode is changed if the game is won. |
References DEBOUNCE_TIMER_MODULE, GAME_RECORD_MODE, save_timeout, sequence_buffer, sequence_buffer_length, SEQUENCE_HEADER_LENGTH, sound_is_playing(), sound_play_note(), sound_play_sample(), SOUND_SAMPLES, SOUND_SINEWAVE, sound_stop_timer(), start_save_timer(), tc_clear_overflow(), tc_is_overflow(), and write_board_led_mask().
Referenced by main().
|
static |
Record button presses and play sound.
buttons | Mask with pressed buttons. |
soundmode | Indicates whether to play a sound sample or sinewave. |
References DEBOUNCE_TIMER_MODULE, sequence_buffer, sequence_buffer_length, SEQUENCE_HEADER_LENGTH, sound_play_note(), sound_play_sample(), SOUND_SAMPLES, SOUND_SINEWAVE, tc_clear_overflow(), and tc_is_overflow().
Referenced by main().
|
static |
Save current game data to EEPROM.
References nvm_eeprom_atomic_write_page(), nvm_eeprom_flush_buffer(), nvm_eeprom_load_page_to_buffer(), sequence_buffer, sequence_buffer_length, and SEQUENCE_BUFFER_MAX_LENGTH.
Referenced by main().
|
static |
Set up and start timer for debouncing of the push buttons.
The timer/counter is set up in normal, up-counting mode with a period of approximately 10 ms.
References DEBOUNCE_TIMER_MODULE, tc_enable(), tc_get_resolution(), tc_set_resolution(), tc_set_wgm(), TC_WG_NORMAL, and tc_write_period().
Referenced by main().
|
static |
Start timer for measuring inactivity before saving.
The timer/counter should be initialized with init_save_timer before this function is called.
References tc_write_clock_source(), and TIMEOUT_TIMER_MODULE.
Referenced by main(), and play_game().
void timeout_callback | ( | void | ) |
Timer/counter overflow interrupt callback function.
This updates the variable for the save timeout and stops its timer/counter once timeout has occurred.
References save_timeout, tc_write_clock_source(), and TIMEOUT_TIMER_MODULE.
Referenced by init_save_timer().
|
static |
Counter for timeout-period before saving button sequence.
Referenced by main(), play_game(), and timeout_callback().
uint8_t sequence_buffer[SEQUENCE_BUFFER_MAX_LENGTH] |
Buffer to contain the button press sequence.
Referenced by load_gamedata(), main(), play_game(), record_buttons(), and save_gamedata().
uint8_t sequence_buffer_length |
Length of currently recorded button sequence in buffer.
Referenced by main(), play_game(), record_buttons(), and save_gamedata().