This is the unit test application for the Advanced Encryption Standard (AES). It consists of test cases for the following functionality:
All AVR XMEGA devices can be used. This example has been tested with the following setup:
See the documentation for the individual unit test functions here for detailed descriptions of the tests.
This example depends directly on the following modules:
This software was written for the GNU GCC and IAR for AVR. Other compilers may or may not work.
For further information, visit Microchip.