Macros | |
#define | COMMON_SENSOR_PLATFORM |
< Validate board support for the common sensor service. More... | |
#define | LED_COUNT 8 |
Number of LEDs. More... | |
GPIO Connections of LEDs | |
#define | LED0_GPIO IOPORT_CREATE_PIN(PORTE, 0) |
#define | LED1_GPIO IOPORT_CREATE_PIN(PORTE, 1) |
#define | LED2_GPIO IOPORT_CREATE_PIN(PORTE, 2) |
#define | LED3_GPIO IOPORT_CREATE_PIN(PORTE, 3) |
#define | LED4_GPIO IOPORT_CREATE_PIN(PORTE, 4) |
#define | LED5_GPIO IOPORT_CREATE_PIN(PORTE, 5) |
#define | LED6_GPIO IOPORT_CREATE_PIN(PORTE, 6) |
#define | LED7_GPIO IOPORT_CREATE_PIN(PORTE, 7) |
#define | LED0 LED0_GPIO |
#define | LED1 LED1_GPIO |
#define | LED2 LED2_GPIO |
#define | LED3 LED3_GPIO |
#define | LED4 LED4_GPIO |
#define | LED5 LED5_GPIO |
#define | LED6 LED6_GPIO |
#define | LED7 LED7_GPIO |
GPIO Connections of Push Buttons | |
#define | GPIO_PUSH_BUTTON_0 IOPORT_CREATE_PIN(PORTD, 0) |
#define | GPIO_PUSH_BUTTON_1 IOPORT_CREATE_PIN(PORTD, 1) |
#define | GPIO_PUSH_BUTTON_2 IOPORT_CREATE_PIN(PORTD, 2) |
#define | GPIO_PUSH_BUTTON_3 IOPORT_CREATE_PIN(PORTD, 3) |
#define | GPIO_PUSH_BUTTON_4 IOPORT_CREATE_PIN(PORTD, 4) |
#define | GPIO_PUSH_BUTTON_5 IOPORT_CREATE_PIN(PORTD, 5) |
#define | GPIO_PUSH_BUTTON_6 IOPORT_CREATE_PIN(PORTR, 0) |
#define | GPIO_PUSH_BUTTON_7 IOPORT_CREATE_PIN(PORTR, 1) |
ADC Connection of the Light Sensor | |
#define | LIGHT_SENSOR_ADC_MODULE ADCB |
#define | LIGHT_SENSOR_ADC_INPUT ADCCH_POS_PIN1 |
#define | LIGHT_SENSOR_SIGNAL_PIN IOPORT_CREATE_PIN(PORTB, 1) |
ADC Connection of the Temperature Sensor | |
#define | TEMPERATURE_SENSOR_ADC_MODULE ADCB |
#define | TEMPERATURE_SENSOR_ADC_INPUT ADCCH_POS_PIN0 |
#define | TEMPERATURE_SENSOR_SIGNAL_PIN IOPORT_CREATE_PIN(PORTB, 0) |
#define | TEMPERATURE_SENSOR_ENABLE_PIN IOPORT_CREATE_PIN(PORTB, 3) |
#define | TEMPERATURE_SENSOR_ENABLE_LEVEL false |
DAC connection and control of the Speaker | |
#define | SPEAKER_DAC_MODULE DACB |
#define | SPEAKER_DAC_CHANNEL DAC_CH0 |
#define | SPEAKER_SIGNAL_PIN IOPORT_CREATE_PIN(PORTB, 2) |
#define | SPEAKER_ENABLE_PIN IOPORT_CREATE_PIN(PORTQ, 3) |
#define | SPEAKER_ENABLE_LEVEL true |
SPI Connections of the AT45DBX Data Flash Memory | |
#define | AT45DBX_SPI &USARTC0 |
#define | AT45DBX_CS IOPORT_CREATE_PIN(PORTQ,3) |
#define | AT45DBX_MASTER_SCK IOPORT_CREATE_PIN(PORTC,7) |
#define | AT45DBX_MASTER_MOSI IOPORT_CREATE_PIN(PORTC,5) |
#define | AT45DBX_MASTER_MISO IOPORT_CREATE_PIN(PORTC,6) |
#define | AT45DBX_SPI_CLK_MASK SYSCLK_PORT_C |
MXT143E Xplained top module | |
#define | MXT143E_XPLAINED_TWI &TWIF |
#define | MXT143E_XPLAINED_USART_SPI &USARTF1 |
#define | MXT143E_XPLAINED_CS IOPORT_CREATE_PIN(PORTF, 4) |
#define | MXT143E_XPLAINED_SCK IOPORT_CREATE_PIN(PORTF, 7) |
#define | MXT143E_XPLAINED_MOSI IOPORT_CREATE_PIN(PORTF, 5) |
#define | MXT143E_XPLAINED_MISO IOPORT_CREATE_PIN(PORTF, 6) |
#define | MXT143E_XPLAINED_CHG IOPORT_CREATE_PIN(PORTF, 2) |
#define | MXT143E_XPLAINED_DC IOPORT_CREATE_PIN(PORTF, 3) |
#define | MXT143E_XPLAINED_BACKLIGHT IOPORT_CREATE_PIN(PORTA, 4) |
#define | MXT143E_XPLAINED_LCD_RESET IOPORT_CREATE_PIN(PORTA, 6) |
External oscillator | |
#define | BOARD_XOSC_HZ 8000000 |
#define | BOARD_XOSC_TYPE XOSC_TYPE_XTAL |
#define | BOARD_XOSC_STARTUP_US 2000 |
#define AT45DBX_CS IOPORT_CREATE_PIN(PORTQ,3) |
Referenced by board_init().
#define AT45DBX_MASTER_MISO IOPORT_CREATE_PIN(PORTC,6) |
Referenced by board_init().
#define AT45DBX_MASTER_MOSI IOPORT_CREATE_PIN(PORTC,5) |
Referenced by board_init().
#define AT45DBX_MASTER_SCK IOPORT_CREATE_PIN(PORTC,7) |
Referenced by board_init().
#define AT45DBX_SPI &USARTC0 |
#define AT45DBX_SPI_CLK_MASK SYSCLK_PORT_C |
#define BOARD_XOSC_HZ 8000000 |
Referenced by osc_get_rate(), and sysclk_get_main_hz().
#define BOARD_XOSC_STARTUP_US 2000 |
#define BOARD_XOSC_TYPE XOSC_TYPE_XTAL |
Referenced by osc_enable_external().
#define COMMON_SENSOR_PLATFORM |
< Validate board support for the common sensor service.
#define GPIO_PUSH_BUTTON_0 IOPORT_CREATE_PIN(PORTD, 0) |
Referenced by board_init().
#define GPIO_PUSH_BUTTON_1 IOPORT_CREATE_PIN(PORTD, 1) |
Referenced by board_init().
#define GPIO_PUSH_BUTTON_2 IOPORT_CREATE_PIN(PORTD, 2) |
Referenced by board_init().
#define GPIO_PUSH_BUTTON_3 IOPORT_CREATE_PIN(PORTD, 3) |
Referenced by board_init().
#define GPIO_PUSH_BUTTON_4 IOPORT_CREATE_PIN(PORTD, 4) |
Referenced by board_init().
#define GPIO_PUSH_BUTTON_5 IOPORT_CREATE_PIN(PORTD, 5) |
Referenced by board_init().
#define GPIO_PUSH_BUTTON_6 IOPORT_CREATE_PIN(PORTR, 0) |
Referenced by board_init().
#define GPIO_PUSH_BUTTON_7 IOPORT_CREATE_PIN(PORTR, 1) |
Referenced by board_init().
#define LED0 LED0_GPIO |
Referenced by example_dma_transfer_done(), and main().
#define LED0_GPIO IOPORT_CREATE_PIN(PORTE, 0) |
Referenced by board_init().
#define LED1 LED1_GPIO |
Referenced by example_dma_transfer_done().
#define LED1_GPIO IOPORT_CREATE_PIN(PORTE, 1) |
Referenced by board_init().
#define LED2 LED2_GPIO |
#define LED2_GPIO IOPORT_CREATE_PIN(PORTE, 2) |
Referenced by board_init().
#define LED3 LED3_GPIO |
#define LED3_GPIO IOPORT_CREATE_PIN(PORTE, 3) |
Referenced by board_init().
#define LED4 LED4_GPIO |
#define LED4_GPIO IOPORT_CREATE_PIN(PORTE, 4) |
Referenced by board_init().
#define LED5 LED5_GPIO |
#define LED5_GPIO IOPORT_CREATE_PIN(PORTE, 5) |
Referenced by board_init().
#define LED6 LED6_GPIO |
#define LED6_GPIO IOPORT_CREATE_PIN(PORTE, 6) |
Referenced by board_init().
#define LED7 LED7_GPIO |
#define LED7_GPIO IOPORT_CREATE_PIN(PORTE, 7) |
Referenced by board_init().
#define LED_COUNT 8 |
Number of LEDs.
#define LIGHT_SENSOR_ADC_INPUT ADCCH_POS_PIN1 |
#define LIGHT_SENSOR_ADC_MODULE ADCB |
#define LIGHT_SENSOR_SIGNAL_PIN IOPORT_CREATE_PIN(PORTB, 1) |
Referenced by board_init().
#define MXT143E_XPLAINED_BACKLIGHT IOPORT_CREATE_PIN(PORTA, 4) |
Referenced by board_init().
#define MXT143E_XPLAINED_CHG IOPORT_CREATE_PIN(PORTF, 2) |
Referenced by board_init().
#define MXT143E_XPLAINED_CS IOPORT_CREATE_PIN(PORTF, 4) |
Referenced by board_init().
#define MXT143E_XPLAINED_DC IOPORT_CREATE_PIN(PORTF, 3) |
Referenced by board_init().
#define MXT143E_XPLAINED_LCD_RESET IOPORT_CREATE_PIN(PORTA, 6) |
Referenced by board_init().
#define MXT143E_XPLAINED_MISO IOPORT_CREATE_PIN(PORTF, 6) |
Referenced by board_init().
#define MXT143E_XPLAINED_MOSI IOPORT_CREATE_PIN(PORTF, 5) |
Referenced by board_init().
#define MXT143E_XPLAINED_SCK IOPORT_CREATE_PIN(PORTF, 7) |
Referenced by board_init().
#define MXT143E_XPLAINED_TWI &TWIF |
#define MXT143E_XPLAINED_USART_SPI &USARTF1 |
#define SPEAKER_DAC_CHANNEL DAC_CH0 |
#define SPEAKER_DAC_MODULE DACB |
#define SPEAKER_ENABLE_LEVEL true |
Referenced by board_init().
#define SPEAKER_ENABLE_PIN IOPORT_CREATE_PIN(PORTQ, 3) |
Referenced by board_init().
#define SPEAKER_SIGNAL_PIN IOPORT_CREATE_PIN(PORTB, 2) |
Referenced by board_init().
#define TEMPERATURE_SENSOR_ADC_INPUT ADCCH_POS_PIN0 |
#define TEMPERATURE_SENSOR_ADC_MODULE ADCB |
#define TEMPERATURE_SENSOR_ENABLE_LEVEL false |
Referenced by board_init().
#define TEMPERATURE_SENSOR_ENABLE_PIN IOPORT_CREATE_PIN(PORTB, 3) |
Referenced by board_init().
#define TEMPERATURE_SENSOR_SIGNAL_PIN IOPORT_CREATE_PIN(PORTB, 0) |
Referenced by board_init().