Microchip® Advanced Software Framework

 All Data Structures Files Functions Variables Typedefs Enumerations Enumerator Macros Groups Pages
External Bus Interface (EBI)

See Quick Start Guide for the XMEGA EBI Driver .

This is a driver for configuring, enabling, disabling and use of the on-chip external bus interface (EBI).

Dependencies

The external bus interface depends on the following modules:

Quick Start Guide

See Quick Start Guide for the XMEGA EBI Driver

Modules

 EBI port/pin configuration
 This is a driver for configuring the external bus interface port.
 
 Common EBI test functions
 This module contains common functions for testing of External Bus Interface (EBI) and the setup of external RAM devices.
 

Data Structures

struct  ebi_cs_config
 External bus interface chip select configuration. More...
 
struct  ebi_sdram_config
 External bus interface SDRAM configuration. More...
 

Macros

#define EBI_SDRAM_CS   3
 Chip select on the EBI that can be configured for SDRAM operation. More...
 

External Bus Interface management

void ebi_cs_write_config (const uint8_t cs, const struct ebi_cs_config *config)
 Write EBI chip select configuration to hardware. More...
 
void ebi_cs_read_config (const uint8_t cs, struct ebi_cs_config *config)
 Read EBI chip select configuration from hardware. More...
 
void ebi_sdram_write_config (const struct ebi_sdram_config *config)
 Write EBI SDRAM configuration to hardware. More...
 
void ebi_sdram_read_config (struct ebi_sdram_config *config)
 Read EBI SDRAM configuration from hardware. More...
 
void ebi_enable_cs (const uint8_t cs, const struct ebi_cs_config *config)
 Enable an EBI chip select. More...
 
void ebi_disable_cs (const uint8_t cs)
 Disable an EBI chip select. More...
 
static bool ebi_sdram_is_ready (void)
 Check if SDRAM is ready for access. More...
 

External Bus Interface Chip Select configuration helper functions

static void ebi_cs_set_mode (struct ebi_cs_config *config, EBI_CS_MODE_t mode)
 Set chip select mode. More...
 
static void ebi_cs_set_address_size (struct ebi_cs_config *config, EBI_CS_ASPACE_t size)
 Set chip select address size. More...
 
static void ebi_cs_set_sram_wait_states (struct ebi_cs_config *config, EBI_CS_SRWS_t cycles)
 Set chip select SRAM wait states. More...
 
static void ebi_cs_set_base_address (struct ebi_cs_config *config, uint32_t address)
 Set chip select base address. More...
 

External Bus Interface SDRAM configuration helper functions

static void ebi_sdram_set_mode (struct ebi_cs_config *config, EBI_CS_SDMODE_t mode)
 Set SDRAM mode. More...
 
static void ebi_sdram_set_cas_latency (struct ebi_sdram_config *config, const uint8_t cas)
 Set SDRAM CAS latency. More...
 
static void ebi_sdram_set_row_bits (struct ebi_sdram_config *config, const uint8_t bits)
 Set number of SDRAM row bits. More...
 
static void ebi_sdram_set_col_bits (struct ebi_sdram_config *config, const uint8_t bits)
 Set number of SDRAM column bits. More...
 
static void ebi_sdram_set_refresh_period (struct ebi_sdram_config *config, const uint16_t period)
 Set SDRAM refresh period. More...
 
static void ebi_sdram_set_initialization_delay (struct ebi_sdram_config *config, const uint16_t delay)
 Set SDRAM initialization delay. More...
 
static void ebi_sdram_set_mode_delay (struct ebi_sdram_config *config, const EBI_MRDLY_t delay)
 Set SDRAM mode delay. More...
 
static void ebi_sdram_set_row_cycle_delay (struct ebi_sdram_config *config, const EBI_ROWCYCDLY_t delay)
 Set SDRAM row cycle delay. More...
 
static void ebi_sdram_set_row_to_precharge_delay (struct ebi_sdram_config *config, const EBI_RPDLY_t delay)
 Set SDRAM row to pre-charge delay. More...
 
static void ebi_sdram_set_write_recovery_delay (struct ebi_sdram_config *config, const EBI_WRDLY_t delay)
 Set SDRAM write recovery delay. More...
 
static void ebi_sdram_set_self_refresh_to_active_delay (struct ebi_sdram_config *config, const EBI_ESRDLY_t delay)
 Set SDRAM exit self refresh to active delay. More...
 
static void ebi_sdram_set_row_to_col_delay (struct ebi_sdram_config *config, const EBI_ROWCOLDLY_t delay)
 Set SDRAM row to column delay. More...
 

External Bus Interface SDRAM power management

static void ebi_sdram_enable_self_refresh (void)
 Enable SDRAM self refresh mode. More...
 
static void ebi_sdram_disable_self_refresh (void)
 Disable SDRAM self refresh mode. More...
 

#define EBI_SDRAM_CS   3

Chip select on the EBI that can be configured for SDRAM operation.

Referenced by ebi_sdram_init().

void ebi_cs_read_config ( const uint8_t  cs,
struct ebi_cs_config config 
)

Read EBI chip select configuration from hardware.

This function will read the EBI chip select hardware configuration and put it into the ebi_cs_config argument.

Parameters
csChip select number to read configuration from
configPointer to an ebi_cs_config variable

References ebi_cs_config::base_address, cpu_irq_restore(), cpu_irq_save(), ebi_cs_config::ctrla, ebi_cs_config::ctrlb, ebi_get_cs_addr_from_cs_num(), sysclk_disable_module(), SYSCLK_EBI, sysclk_enable_module(), sysclk_module_is_enabled(), and SYSCLK_PORT_GEN.

static void ebi_cs_set_address_size ( struct ebi_cs_config config,
EBI_CS_ASPACE_t  size 
)
inlinestatic

Set chip select address size.

This function helps the caller setting the chip select address size. The different sizes are provided by an EBI_CS_ASPACE_t type from the toolchain header files.

Parameters
configPointer to an ebi_cs_config variable
sizeChip select address size given by an EBI_CS_ASPACE_t type

References ebi_cs_config::ctrla, and EBI_CS_ASPACE_gm.

Referenced by ebi_sdram_init().

static void ebi_cs_set_base_address ( struct ebi_cs_config config,
uint32_t  address 
)
inlinestatic

Set chip select base address.

This function helps the caller setting the chip select base address, e.g., the lowest address space enabled by the chip select.

Parameters
configPointer to an ebi_cs_config variable
addressThe chip select base address

References ebi_cs_config::base_address.

Referenced by ebi_sdram_init().

static void ebi_cs_set_mode ( struct ebi_cs_config config,
EBI_CS_MODE_t  mode 
)
inlinestatic

Set chip select mode.

This function helps the caller setting the chip select mode. The different modes are provided by an EBI_CS_MODE_t type from the toolchain header files.

Parameters
configPointer to an ebi_cs_config variable
modeChip select mode given by an EBI_CS_MODE_t type

References ebi_cs_config::ctrla.

Referenced by ebi_sdram_init().

static void ebi_cs_set_sram_wait_states ( struct ebi_cs_config config,
EBI_CS_SRWS_t  cycles 
)
inlinestatic

Set chip select SRAM wait states.

This function helps the caller setting the chip select SRAM wait states. The different SRAM wait states (cycles) are provided by an EBI_CS_SRWS_t type from the toolchain header files.

Parameters
configPointer to an ebi_cs_config variable
cyclesChip select SRAM wait states given by an EBI_CS_SRWS_t type

References ebi_cs_config::ctrlb.

void ebi_cs_write_config ( const uint8_t  cs,
const struct ebi_cs_config config 
)

Write EBI chip select configuration to hardware.

This function will write an ebi_cs_config struct to the selected chip select hardware.

Parameters
csChip select number to write configuration for
configPointer to an ebi_cs_config variable

References ebi_cs_config::base_address, cpu_irq_restore(), cpu_irq_save(), ebi_cs_config::ctrla, ebi_cs_config::ctrlb, ebi_get_cs_addr_from_cs_num(), sysclk_disable_module(), SYSCLK_EBI, sysclk_enable_module(), sysclk_module_is_enabled(), and SYSCLK_PORT_GEN.

Referenced by ebi_sdram_init().

void ebi_disable_cs ( const uint8_t  cs)
void ebi_enable_cs ( const uint8_t  cs,
const struct ebi_cs_config config 
)

Enable an EBI chip select.

Parameters
csChip select number to enable
configPointer to an ebi_cs_config variable

References cpu_irq_restore(), cpu_irq_save(), ebi_cs_config::ctrla, ebi_enabled_chip_selects, ebi_get_cs_addr_from_cs_num(), SLEEPMGR_IDLE, sleepmgr_lock_mode(), SYSCLK_EBI, sysclk_enable_module(), and SYSCLK_PORT_GEN.

Referenced by ebi_sdram_init().

static void ebi_sdram_disable_self_refresh ( void  )
inlinestatic

Disable SDRAM self refresh mode.

This function makes the EBI hardware send a command to the SDRAM to leave self refresh mode.

References cpu_irq_restore(), cpu_irq_save(), SLEEPMGR_IDLE, and sleepmgr_lock_mode().

static void ebi_sdram_enable_self_refresh ( void  )
inlinestatic

Enable SDRAM self refresh mode.

This function makes the EBI hardware send a command to the SDRAM to enter self refresh mode.

References cpu_irq_restore(), cpu_irq_save(), SLEEPMGR_IDLE, and sleepmgr_unlock_mode().

static bool ebi_sdram_is_ready ( void  )
inlinestatic

Check if SDRAM is ready for access.

This function must be checked after the SDRAM chip select has been enabled. It will return true when the SDRAM is initialized.

Return values
truewhen SDRAM is ready, false otherwise

Referenced by ebi_sdram_init().

void ebi_sdram_read_config ( struct ebi_sdram_config config)

Read EBI SDRAM configuration from hardware.

This function will read the SDRAM EBI hardware configuration and put it into the ebi_cs_config argument.

Note
SDRAM is by design limited to chip select 3.
Parameters
configPointer to an ebi_sdram_config variable

References cpu_irq_restore(), cpu_irq_save(), ebi_sdram_config::init_delay, ebi_sdram_config::refresh_period, ebi_sdram_config::sdramctrla, ebi_sdram_config::sdramctrlb, ebi_sdram_config::sdramctrlc, sysclk_disable_module(), SYSCLK_EBI, sysclk_enable_module(), sysclk_module_is_enabled(), and SYSCLK_PORT_GEN.

static void ebi_sdram_set_cas_latency ( struct ebi_sdram_config config,
const uint8_t  cas 
)
inlinestatic

Set SDRAM CAS latency.

This function helps the caller setting the SDRAM CAS latency.

Parameters
configPointer to an ebi_sdram_config variable
casSDRAM CAS latency, 2 or 3

References Assert, and ebi_sdram_config::sdramctrla.

Referenced by ebi_sdram_init().

static void ebi_sdram_set_col_bits ( struct ebi_sdram_config config,
const uint8_t  bits 
)
inlinestatic

Set number of SDRAM column bits.

This function helps the caller setting the number of SDRAM column bits.

Parameters
configPointer to an ebi_sdram_config variable
bitsNumber of column bits, 8 to 11

References Assert, and ebi_sdram_config::sdramctrla.

Referenced by ebi_sdram_init().

static void ebi_sdram_set_initialization_delay ( struct ebi_sdram_config config,
const uint16_t  delay 
)
inlinestatic

Set SDRAM initialization delay.

This function helps the caller setting the SDRAM initialization delay as a number of peripheral 2x clock cycles (CLKper2).

Parameters
configPointer to an ebi_sdram_config variable
delaySDREAM initialization delay, number of CLKper2 cycles

References ebi_sdram_config::init_delay.

Referenced by ebi_sdram_init().

static void ebi_sdram_set_mode ( struct ebi_cs_config config,
EBI_CS_SDMODE_t  mode 
)
inlinestatic

Set SDRAM mode.

This function helps the caller setting the SDRAM mode. The different modes are provided by an EBI_CS_SDMODE_t type from the toolchain header files.

Note
This function needs a pointer to an ebi_cs_config struct, not an ebi_sdram_config struct as the other SDRAM configuration helper function does.
Parameters
configPointer to an ebi_cs_config variable
modeSDRAM mode given by an EBI_CS_SDMODE_t type

References ebi_cs_config::ctrlb.

Referenced by ebi_sdram_init().

static void ebi_sdram_set_mode_delay ( struct ebi_sdram_config config,
const EBI_MRDLY_t  delay 
)
inlinestatic

Set SDRAM mode delay.

This function helps the caller setting the SDRAM mode delay as a number of peripheral 2x clock cycles (CLKper2). The different modes are provided by an EBI_MRDLY_t type from the toolchain header files.

Parameters
configPointer to an ebi_sdram_config variable
delaySDRAM mode delay given by an EBI_MRDLY_t type

References ebi_sdram_config::sdramctrlb.

Referenced by ebi_sdram_init().

static void ebi_sdram_set_refresh_period ( struct ebi_sdram_config config,
const uint16_t  period 
)
inlinestatic

Set SDRAM refresh period.

This function helps the caller setting the SDRAM refresh period as a number of peripheral 2x clock cycles (CLKper2).

Parameters
configPointer to an ebi_sdram_config variable
periodSDREAM refresh period, number of CLKper2 cycles

References ebi_sdram_config::refresh_period.

Referenced by ebi_sdram_init().

static void ebi_sdram_set_row_bits ( struct ebi_sdram_config config,
const uint8_t  bits 
)
inlinestatic

Set number of SDRAM row bits.

This function helps the caller setting the number of SDRAM row bits.

Parameters
configPointer to an ebi_sdram_config variable
bitsNumber of row bits, 11 or 12

References Assert, and ebi_sdram_config::sdramctrla.

Referenced by ebi_sdram_init().

static void ebi_sdram_set_row_cycle_delay ( struct ebi_sdram_config config,
const EBI_ROWCYCDLY_t  delay 
)
inlinestatic

Set SDRAM row cycle delay.

This function helps the caller setting the SDRAM row cycle delay as a number of peripheral clock 2x cycles (CLKper2). The different delays are provided by an EBI_ROWCYCDLY_t type from the toolchain header files.

Parameters
configPointer to an ebi_sdram_config variable
delaySDRAM row cycle delay given by an EBI_ROWCYCDLY_t type

References ebi_sdram_config::sdramctrlb.

Referenced by ebi_sdram_init().

static void ebi_sdram_set_row_to_col_delay ( struct ebi_sdram_config config,
const EBI_ROWCOLDLY_t  delay 
)
inlinestatic

Set SDRAM row to column delay.

This function helps the caller setting the SDRAM row to column delay as a number of peripheral clock 2x cycles (CLKper2). The different delays are provided by an EBI_ROWCOLDLY_t type from the toolchain header files.

Parameters
configPointer to an ebi_sdram_config variable
delaySDRAM row to column delay given by an EBI_ROWCOLDLY_t type

References ebi_sdram_config::sdramctrlc.

Referenced by ebi_sdram_init().

static void ebi_sdram_set_row_to_precharge_delay ( struct ebi_sdram_config config,
const EBI_RPDLY_t  delay 
)
inlinestatic

Set SDRAM row to pre-charge delay.

This function helps the caller setting the SDRAM row to pre-charge delay as a number of peripheral clock 2x cycles (CLKper2). The different delays are provided by an EBI_RPDLY_t type from the toolchain header files.

Parameters
configPointer to an ebi_sdram_config variable
delaySDRAM row to pre-charge delay given by an EBI_ROWCYCDLY_t type

References ebi_sdram_config::sdramctrlb.

Referenced by ebi_sdram_init().

static void ebi_sdram_set_self_refresh_to_active_delay ( struct ebi_sdram_config config,
const EBI_ESRDLY_t  delay 
)
inlinestatic

Set SDRAM exit self refresh to active delay.

This function helps the caller setting the SDRAM exit self refresh to active delay as a number of peripheral clock 2x cycles (CLKper2). The different delays are provided by an EBI_ESRDLY_t type from the toolchain header files.

Parameters
configPointer to an ebi_sdram_config variable
delaySDRAM exit self refresh to active delay given by an EBI_ESRDLY_t type

References ebi_sdram_config::sdramctrlc.

Referenced by ebi_sdram_init().

static void ebi_sdram_set_write_recovery_delay ( struct ebi_sdram_config config,
const EBI_WRDLY_t  delay 
)
inlinestatic

Set SDRAM write recovery delay.

This function helps the caller setting the SDRAM write recovery delay as a number of peripheral clock 2x cycles (CLKper2). The different delays are provided by an EBI_WRDLY_t type from the toolchain header files.

Parameters
configPointer to an ebi_sdram_config variable
delaySDRAM write recovery delay given by an EBI_WRDLY_t type

References ebi_sdram_config::sdramctrlc.

Referenced by ebi_sdram_init().

void ebi_sdram_write_config ( const struct ebi_sdram_config config)

Write EBI SDRAM configuration to hardware.

This function will write an ebi_sdram_config struct to the SDRAM part of the EBI hardware.

Note
SDRAM is by design limited to chip select 3.
Parameters
configPointer to an ebi_sdram_config variable

References cpu_irq_restore(), cpu_irq_save(), ebi_sdram_config::init_delay, ebi_sdram_config::refresh_period, ebi_sdram_config::sdramctrla, ebi_sdram_config::sdramctrlb, ebi_sdram_config::sdramctrlc, sysclk_disable_module(), SYSCLK_EBI, sysclk_enable_module(), sysclk_module_is_enabled(), and SYSCLK_PORT_GEN.

Referenced by ebi_sdram_init().