Example configuration.
Copyright (c) 2014-2018 Microchip Technology Inc. and its subsidiaries.
Macros | |
#define | LED_PIN_0 LED0_GPIO |
#define | LED_PIN_1 LED1_GPIO |
#define | LED_PIN_2 LED2_GPIO |
#define | LED_PIN_3 LED3_GPIO |
#define | LED_PIN_4 LED4_GPIO |
#define | LED_PIN_5 LED5_GPIO |
#define | LED_PIN_6 LED6_GPIO |
#define | LED_PIN_7 LED7_GPIO |
#define LED_PIN_2 LED2_GPIO |
#define LED_PIN_4 LED4_GPIO |
#define LED_PIN_5 LED5_GPIO |
#define LED_PIN_6 LED6_GPIO |
#define LED_PIN_7 LED7_GPIO |
Referenced by main().