This example shows how to use and tests the NVM EEPROM handling of the NVM driver.
All AVR XMEGA devices can be used. This example have been tested with the following setup:
For the A3BU Xplained, the tests are printed on the display, where successful tests are marked with OK below the test number, and failed test are marked with ERR.
This example depends on the following modules:
This software was written for the GNU GCC and IAR for AVR. Other compilers may or may not work.
For further information, visit Microchip.