Functions for handling internal EEPROM memory.
The internal EEPROM can be used to store data that will persist after power is removed. This can typically be used to store calibration data, application state, encryption keys or other data that need to be preserved when power is removed.
The functions in this module uses IO register access to manipulate the EEPROM.
Macros | |
#define | EEPROM_PAGE_SIZE 32 |
Typedefs | |
typedef uint16_t | eeprom_addr_t |
Data type for holding eeprom memory addresses. More... | |
Functions | |
static void | eeprom_disable_mapping (void) |
Disable EEPROM mapping into data space. More... | |
static void | eeprom_enable_mapping (void) |
Enable EEPROM mapping into data space. More... | |
void | nvm_eeprom_atomic_write_page (uint8_t page_addr) |
Erase and write bytes from page buffer into EEPROM. More... | |
void | nvm_eeprom_erase_all (void) |
Erase entire EEPROM memory. More... | |
void | nvm_eeprom_erase_and_write_buffer (eeprom_addr_t address, const void *buf, uint16_t len) |
Write buffer within the eeprom. More... | |
void | nvm_eeprom_erase_bytes_in_all_pages (void) |
Erase bytes from all EEPROM pages. More... | |
void | nvm_eeprom_erase_bytes_in_page (uint8_t page_addr) |
Erase bytes from EEPROM page. More... | |
void | nvm_eeprom_erase_page (uint8_t page_addr) |
Erase EEPROM page. More... | |
void | nvm_eeprom_fill_buffer_with_value (uint8_t value) |
Fill temporary EEPROM page buffer with value. More... | |
void | nvm_eeprom_flush_buffer (void) |
Flush temporary EEPROM page buffer. More... | |
void | nvm_eeprom_load_byte_to_buffer (uint8_t byte_addr, uint8_t value) |
Load single byte into temporary page buffer. More... | |
void | nvm_eeprom_load_page_to_buffer (const uint8_t *values) |
Load entire page into temporary EEPROM page buffer. More... | |
void | nvm_eeprom_read_buffer (eeprom_addr_t address, void *buf, uint16_t len) |
Read buffer within the eeprom. More... | |
uint8_t | nvm_eeprom_read_byte (eeprom_addr_t addr) |
Read one byte from EEPROM using mapped access. More... | |
void | nvm_eeprom_split_write_page (uint8_t page_addr) |
Write (without erasing) EEPROM page. More... | |
void | nvm_eeprom_write_byte (eeprom_addr_t address, uint8_t value) |
Write one byte to EEPROM using IO mapping. More... | |
#define EEPROM_PAGE_SIZE 32 |
typedef uint16_t eeprom_addr_t |
Data type for holding eeprom memory addresses.
|
inlinestatic |
Disable EEPROM mapping into data space.
This macro disables mapping of EEPROM into data space. IO mapped access is now enabled.
Referenced by nvm_eeprom_load_byte_to_buffer(), nvm_eeprom_read_buffer(), and nvm_eeprom_read_byte().
|
inlinestatic |
Enable EEPROM mapping into data space.
This macro enables mapping of EEPROM into data space. EEPROM starts at EEPROM_START in data memory. Read access can be done similar to ordinary SRAM access.
Referenced by nvm_eeprom_load_byte_to_buffer(), nvm_eeprom_read_buffer(), and nvm_eeprom_read_byte().
void nvm_eeprom_atomic_write_page | ( | uint8_t | page_addr | ) |
Erase and write bytes from page buffer into EEPROM.
This function writes the contents of an already loaded EEPROM page buffer into EEPROM memory.
As this is an atomic write, the page in EEPROM will be erased automatically before writing. Note that only the page buffer locations that have been loaded will be used when writing to EEPROM. Page buffer locations that have not been loaded will be left untouched in EEPROM.
page_addr | EEPROM Page address, between 0 and EEPROM_SIZE/EEPROM_PAGE_SIZE |
References Assert, EEPROM_PAGE_SIZE, nvm_issue_command(), and nvm_wait_until_ready().
Referenced by nvm_eeprom_erase_and_write_buffer().
void nvm_eeprom_erase_all | ( | void | ) |
Erase entire EEPROM memory.
This function erases the entire EEPROM memory block to 0xFF.
References nvm_eeprom_erase_bytes_in_all_pages(), and nvm_eeprom_fill_buffer_with_value().
void nvm_eeprom_erase_and_write_buffer | ( | eeprom_addr_t | address, |
const void * | buf, | ||
uint16_t | len | ||
) |
Write buffer within the eeprom.
address | the address to where to write |
buf | pointer to the data |
len | the number of bytes to write |
References EEPROM_PAGE_SIZE, nvm_eeprom_atomic_write_page(), nvm_eeprom_load_page_to_buffer(), and nvm_eeprom_write_byte().
void nvm_eeprom_erase_bytes_in_all_pages | ( | void | ) |
Erase bytes from all EEPROM pages.
This function erases bytes from all EEPROM pages, so that every location written to in the page buffer reads 0xFF.
References nvm_issue_command(), and nvm_wait_until_ready().
Referenced by nvm_eeprom_erase_all().
void nvm_eeprom_erase_bytes_in_page | ( | uint8_t | page_addr | ) |
Erase bytes from EEPROM page.
This function erases bytes from one EEPROM page, so that every location written to in the page buffer reads 0xFF.
page_addr | EEPROM Page address, between 0 and EEPROM_SIZE/EEPROM_PAGE_SIZE |
References Assert, EEPROM_PAGE_SIZE, nvm_issue_command(), and nvm_wait_until_ready().
Referenced by nvm_eeprom_erase_page().
void nvm_eeprom_erase_page | ( | uint8_t | page_addr | ) |
Erase EEPROM page.
This function erases one EEPROM page, so that every location reads 0xFF.
page_addr | EEPROM Page address, between 0 and EEPROM_SIZE/EEPROM_PAGE_SIZE |
References nvm_eeprom_erase_bytes_in_page(), and nvm_eeprom_fill_buffer_with_value().
void nvm_eeprom_fill_buffer_with_value | ( | uint8_t | value | ) |
Fill temporary EEPROM page buffer with value.
This fills the the EEPROM page buffers with a given value. If memory mapped EEPROM is enabled, this function will not work.
value | Value to copy to the page buffer. |
References EEPROM_PAGE_SIZE, nvm_eeprom_flush_buffer(), nvm_eeprom_load_byte_to_buffer(), and nvm_wait_until_ready().
Referenced by nvm_eeprom_erase_all(), and nvm_eeprom_erase_page().
void nvm_eeprom_flush_buffer | ( | void | ) |
Flush temporary EEPROM page buffer.
This function flushes the EEPROM page buffers. This function will cancel any ongoing EEPROM page buffer loading operations, if any. This function also works for memory mapped EEPROM access.
References nvm_exec(), and nvm_wait_until_ready().
Referenced by nvm_eeprom_fill_buffer_with_value(), and nvm_eeprom_write_byte().
void nvm_eeprom_load_byte_to_buffer | ( | uint8_t | byte_addr, |
uint8_t | value | ||
) |
Load single byte into temporary page buffer.
This function loads one byte into the temporary EEPROM page buffers. If memory mapped EEPROM is enabled, this function will not work. Make sure that the buffer is flushed before starting to load bytes. Also, if multiple bytes are loaded into the same location, they will be ANDed together, thus 0x55 and 0xAA will result in 0x00 in the buffer.
byte_addr | EEPROM Byte address, between 0 and EEPROM_PAGE_SIZE. |
value | Byte value to write to buffer. |
References eeprom_disable_mapping(), eeprom_enable_mapping(), and nvm_wait_until_ready().
Referenced by nvm_eeprom_fill_buffer_with_value(), nvm_eeprom_load_page_to_buffer(), and nvm_eeprom_write_byte().
void nvm_eeprom_load_page_to_buffer | ( | const uint8_t * | values | ) |
Load entire page into temporary EEPROM page buffer.
This function loads an entire EEPROM page from an SRAM buffer to the EEPROM page buffers. If memory mapped EEPROM is enabled, this function will not work. Make sure that the buffer is flushed before starting to load bytes.
values | Pointer to SRAM buffer containing an entire page. |
References EEPROM_PAGE_SIZE, nvm_eeprom_load_byte_to_buffer(), and nvm_wait_until_ready().
Referenced by nvm_eeprom_erase_and_write_buffer().
void nvm_eeprom_read_buffer | ( | eeprom_addr_t | address, |
void * | buf, | ||
uint16_t | len | ||
) |
Read buffer within the eeprom.
address | the address to where to read |
buf | pointer to the data |
len | the number of bytes to read |
References eeprom_disable_mapping(), eeprom_enable_mapping(), and nvm_wait_until_ready().
uint8_t nvm_eeprom_read_byte | ( | eeprom_addr_t | addr | ) |
Read one byte from EEPROM using mapped access.
This function reads one byte from EEPROM using mapped access.
addr | EEPROM address, between 0 and EEPROM_SIZE |
References Assert, eeprom_disable_mapping(), eeprom_enable_mapping(), and nvm_wait_until_ready().
void nvm_eeprom_split_write_page | ( | uint8_t | page_addr | ) |
Write (without erasing) EEPROM page.
This function writes the contents of an already loaded EEPROM page buffer into EEPROM memory.
As this is a split write, the page in EEPROM will not be erased before writing.
page_addr | EEPROM Page address, between 0 and EEPROM_SIZE/EEPROM_PAGE_SIZE |
References Assert, EEPROM_PAGE_SIZE, nvm_issue_command(), and nvm_wait_until_ready().
void nvm_eeprom_write_byte | ( | eeprom_addr_t | address, |
uint8_t | value | ||
) |
Write one byte to EEPROM using IO mapping.
This function writes one byte to EEPROM using IO-mapped access. This function will cancel all ongoing EEPROM page buffer loading operations, if any.
address | EEPROM address (max EEPROM_SIZE) |
value | Byte value to write to EEPROM. |
References Assert, nvm_eeprom_flush_buffer(), nvm_eeprom_load_byte_to_buffer(), nvm_exec(), and nvm_wait_until_ready().
Referenced by nvm_eeprom_erase_and_write_buffer().