This is a low-level driver implementation for the AVR XMEGA sleep controller.
See Quick Start Guide for the XMEGA Sleep Driver
Macros | |
#define | sleep_enter() __sleep() |
Macro for issuing the sleep instruction. More... | |
Functions | |
static void | sleep_disable (void) |
Disable sleep. More... | |
static void | sleep_enable (void) |
Enable sleep. More... | |
static void | sleep_set_mode (enum SLEEP_SMODE_enum mode) |
Set new sleep mode. More... | |
#define sleep_enter | ( | ) | __sleep() |
Macro for issuing the sleep instruction.
Referenced by sleepmgr_sleep().
|
inlinestatic |
Disable sleep.
Referenced by sleepmgr_sleep().
|
inlinestatic |
Enable sleep.
Referenced by sleepmgr_sleep().
|
inlinestatic |
Set new sleep mode.
mode | Sleep mode, from the device IO header file. |
Referenced by sleepmgr_sleep().