In this section you can find all the projects related to the CRC module driver.
Example1 for CRC driver on XMEGA-A3BU Xplained | |
An example application using both CRC-16 and CRC-32 using the I/O interface. | |
Example2 for CRC driver on XMEGA-A3BU Xplained | |
An example application performing CRC on FLASH memory. | |
Example3 for CRC driver on XMEGA-A3BU Xplained | |
An example application performing CRC on a DMA transaction. |
Unit test for XMega CRC module driver | |
Test all function of XMega CRC driver. |