#include "conf_audio_player.h"
#include "compiler.h"
#include "board.h"
#include "usb_ids.h"
#include "twim.h"
#include "pdca.h"
Macros | |
#define | CPU_RESET_CALLBACK() |
Reset callback - called just before the CPU reset takes in place. More... | |
#define | DEVICE_ADDRESS 0x05 |
The address that will be assigned to the connected device. More... | |
#define | HOST_AUTO_CFG_ENDPOINT ENABLE |
Try to configure the host pipe according to the device descriptors received. More... | |
#define | HOST_CONTINUOUS_SOF_INTERRUPT DISABLE |
Host Start-of-Frame interrupt always enabled. More... | |
#define | Host_device_class_not_supported_action() |
#define | Host_device_connection_action() |
#define | Host_device_error_action() |
#define | Host_device_not_supported_action() |
#define | Host_device_supported_action() |
#define | HOST_ERROR_RESTART DISABLE |
When host error state detected, go to detached state. More... | |
#define | Host_hwup_action() |
#define | Host_sof_action() |
#define | HOST_STRICT_VID_PID_TABLE DISABLE |
The host controller will be limited to the strict VID/PID list. More... | |
#define | Host_suspend_action() |
#define | HOST_VBUS_LOW_TIMEOUT ((2000 * (unsigned long long) 60000000) / 1000) |
The time in cycle number that the VBus need to be dropped down after a "device unplugged" has been detected if no timeouts are needed, then this constant should not be defined. More... | |
#define | ID_PIN_CHANGE_GENERATE_RESET ENABLE |
Force CPU reset upon ID pin change. More... | |
#define | LOG_STR(str) ((void)(str)) |
Debug trace macro. More... | |
#define | MAX_EP_PER_INTERFACE 3 |
The maximal number of endpoints per interface supported. More... | |
#define | NAK_RECEIVE_TIMEOUT 0x0FFF |
Number of NAK handshakes before time-out for receive functions (up to 0xFFFF) More... | |
#define | NAK_SEND_TIMEOUT 0x0FFF |
Number of NAK handshakes before time-out for transmit functions (up to 0xFFFF) More... | |
#define | NAK_TIMEOUT_ENABLE DISABLE |
Enable cpt NAK time-out for host transfer. More... | |
#define | SIZEOF_DATA_STAGE 250 |
The size of RAM buffer reserved for descriptor handling. More... | |
#define | TIMEOUT_DELAY 10 |
Delay (unit is in 1/4 s - 250 ms) before time-out value. More... | |
#define | TIMEOUT_DELAY_ENABLE ENABLE |
Enable time-out delay for host transfer. More... | |
#define | TIMER_USB_STREAM_MONITOR 700 |
Period (in ms) of the polling of the buffers monitoring. More... | |
#define | USB_HOST_PIPE_INTERRUPT_TRANSFER DISABLE |
USB host pipes transfers use USB communication interrupt (allows to use non-blocking functions) More... | |
#define | Usb_id_transition_action() |
#define | USB_INT_LEVEL 3 |
USB interrupt priority level. More... | |
#define | USB_RESYNC_AUDIO_STREAM true |
true to activate the USB audio resynchronization More... | |
#define | USB_STREAM_BUFFER_NUMBER 16 |
Number of buffers used in the USB stream FIFO. More... | |
#define | USB_STREAM_BUFFER_SIZE 256 |
Size of a buffer (in bytes) used in the USB stream FIFO. More... | |
#define | USB_STREAM_RESYNC_PPM_STEPS 10 |
Steps in PPM for the resynchronization. More... | |