Microchip® Advanced Software Framework

S_usb_setup_data Struct Reference

USB Setup Data.

#include <usb_host_enum.h>

Data Fields

uint8_t bmRequestType
 Characteristics of the request. More...
 
uint8_t bRequest
 Specific request. More...
 
bool incomplete_read
 true: only one read More...
 
uint16_t wIndex
 Field that varies according to request. More...
 
uint16_t wLength
 Number of bytes to transfer if Data. More...
 
uint16_t wValue
 Field that varies according to request. More...
 

uint8_t S_usb_setup_data::bmRequestType

Characteristics of the request.

Referenced by host_transfer_control().

uint8_t S_usb_setup_data::bRequest

Specific request.

Referenced by host_transfer_control().

bool S_usb_setup_data::incomplete_read

true: only one read

Referenced by host_transfer_control().

uint16_t S_usb_setup_data::wIndex

Field that varies according to request.

Referenced by host_transfer_control().

uint16_t S_usb_setup_data::wLength

Number of bytes to transfer if Data.

Referenced by host_transfer_control().

uint16_t S_usb_setup_data::wValue

Field that varies according to request.

Referenced by host_transfer_control().