Microchip® Advanced Software Framework

unicode.c File Reference
#include "compiler.h"
#include "unicode.h"

Functions

uint8_t unicode_header_get (uint8_t *header, uint8_t txt_format)
 Return the header corresponding at text format identifier. More...
 
uint8_t unicode_header_scan (uint8_t *header)
 Detect the text format via a header (3 bytes) More...
 
uint8_t utf8_to_unicode (uint8_t *utf8, uint16_t *unicode)
 Conversion UTF-8 to unicode. More...
 

uint8_t unicode_header_get ( uint8_t *  header,
uint8_t  txt_format 
)

Return the header corresponding at text format identifier.

Parameters
txt_formatUNI_TYPE_UTF8, UNI_TYPE_UTF16BE, UNI_TYPE_UTF16LE, UNI_TYPE_ASCII
headerheader to fill (array of 3B)
Returns
the size of header

References UNI_TYPE_UTF16BE, UNI_TYPE_UTF16LE, and UNI_TYPE_UTF8.

Referenced by reader_txt_beg(), and reader_txt_new().

uint8_t unicode_header_scan ( uint8_t *  header)

Detect the text format via a header (3 bytes)

Parameters
headerheader to analyze (array of 3B)
Returns
text format identifier

References UNI_TYPE_ASCII, UNI_TYPE_UTF16BE, UNI_TYPE_UTF16LE, and UNI_TYPE_UTF8.

Referenced by reader_txt_beg().

uint8_t utf8_to_unicode ( uint8_t *  utf8,
uint16_t *  unicode 
)

Conversion UTF-8 to unicode.

Parameters
utf8array with utf8 codes (array of 3B max)
unicodepointer used to store the character unicode decoded
Returns
the size of UTF8 decoded

Referenced by reader_txt_get_line().