Microchip® Advanced Software Framework

 All Data Structures Files Functions Variables Typedefs Enumerations Enumerator Macros Groups Pages
USB host operating mode configuration

Modules

 USB host custom actions
 
 USB device operating mode configuration
 

Macros

#define CPU_RESET_CALLBACK()
 Reset callback - called just before the CPU reset takes in place. More...
 
#define DEVICE_ADDRESS   0x05
 The address that will be assigned to the connected device. More...
 
#define HOST_AUTO_CFG_ENDPOINT   ENABLE
 Try to configure the host pipe according to the device descriptors received. More...
 
#define HOST_CONTINUOUS_SOF_INTERRUPT   DISABLE
 Host Start-of-Frame interrupt always enabled. More...
 
#define HOST_ERROR_RESTART   DISABLE
 When host error state detected, go to detached state. More...
 
#define HOST_STRICT_VID_PID_TABLE   DISABLE
 The host controller will be limited to the strict VID/PID list. More...
 
#define HOST_VBUS_LOW_TIMEOUT   ((2000 * (unsigned long long) 60000000) / 1000)
 The time in cycle number that the VBus need to be dropped down after a "device unplugged" has been detected if no timeouts are needed, then this constant should not be defined. More...
 
#define ID_PIN_CHANGE_GENERATE_RESET   ENABLE
 Force CPU reset upon ID pin change. More...
 
#define MAX_EP_PER_INTERFACE   3
 The maximal number of endpoints per interface supported. More...
 
#define NAK_RECEIVE_TIMEOUT   0x0FFF
 Number of NAK handshakes before time-out for receive functions (up to 0xFFFF) More...
 
#define NAK_SEND_TIMEOUT   0x0FFF
 Number of NAK handshakes before time-out for transmit functions (up to 0xFFFF) More...
 
#define NAK_TIMEOUT_ENABLE   DISABLE
 Enable cpt NAK time-out for host transfer. More...
 
#define SIZEOF_DATA_STAGE   250
 The size of RAM buffer reserved for descriptor handling. More...
 
#define TIMEOUT_DELAY   10
 Delay (unit is in 1/4 s - 250 ms) before time-out value. More...
 
#define TIMEOUT_DELAY_ENABLE   ENABLE
 Enable time-out delay for host transfer. More...
 
#define USB_HOST_PIPE_INTERRUPT_TRANSFER   DISABLE
 USB host pipes transfers use USB communication interrupt (allows to use non-blocking functions) More...
 

#define CPU_RESET_CALLBACK ( )
Value:
{ \
extern void controller_shutdown(void); \
extern void gui_shutdown(void); \
extern void twi_disable_interrupt(volatile avr32_twi_t *twi); \
twi_disable_interrupt(&AVR32_TWI); \
}
#define avr32_twi_t
Definition: twim.h:94
void controller_shutdown(void)
Shutdown the controller.
Definition: qt60168_controller.c:227
void pdca_disable_interrupt_transfer_complete(uint8_t pdca_ch_number)
Disable PDCA transfer interrupt when completed (ie TCR and TCRR are both zero)
Definition: pdca.c:235
void pdca_disable_interrupt_reload_counter_zero(uint8_t pdca_ch_number)
Disable PDCA transfer interrupt when TCRR reaches zero.
Definition: pdca.c:258
void gui_shutdown()
Shutdown the GUI.
Definition: et024006dhu_gui.c:97

Reset callback - called just before the CPU reset takes in place.

#define DEVICE_ADDRESS   0x05

The address that will be assigned to the connected device.

Referenced by usb_host_task().

#define HOST_AUTO_CFG_ENDPOINT   ENABLE

Try to configure the host pipe according to the device descriptors received.

#define HOST_CONTINUOUS_SOF_INTERRUPT   DISABLE

Host Start-of-Frame interrupt always enabled.

#define HOST_ERROR_RESTART   DISABLE

When host error state detected, go to detached state.

#define HOST_STRICT_VID_PID_TABLE   DISABLE

The host controller will be limited to the strict VID/PID list.

When enabled, if the device VID/PID does not belong to the supported list, the host controller software will not go to deeper configuration, but to error state.

#define HOST_VBUS_LOW_TIMEOUT   ((2000 * (unsigned long long) 60000000) / 1000)

The time in cycle number that the VBus need to be dropped down after a "device unplugged" has been detected if no timeouts are needed, then this constant should not be defined.

#define ID_PIN_CHANGE_GENERATE_RESET   ENABLE

Force CPU reset upon ID pin change.

#define MAX_EP_PER_INTERFACE   3

The maximal number of endpoints per interface supported.

Referenced by host_check_class().

#define NAK_RECEIVE_TIMEOUT   0x0FFF

Number of NAK handshakes before time-out for receive functions (up to 0xFFFF)

Referenced by host_get_data().

#define NAK_SEND_TIMEOUT   0x0FFF

Number of NAK handshakes before time-out for transmit functions (up to 0xFFFF)

Referenced by host_send_data().

#define NAK_TIMEOUT_ENABLE   DISABLE

Enable cpt NAK time-out for host transfer.

#define SIZEOF_DATA_STAGE   250

The size of RAM buffer reserved for descriptor handling.

Referenced by host_check_class().

#define TIMEOUT_DELAY   10

Delay (unit is in 1/4 s - 250 ms) before time-out value.

Referenced by host_get_data(), and host_send_data().

#define TIMEOUT_DELAY_ENABLE   ENABLE

Enable time-out delay for host transfer.

#define USB_HOST_PIPE_INTERRUPT_TRANSFER   DISABLE

USB host pipes transfers use USB communication interrupt (allows to use non-blocking functions)