Driver for the ADCIFA (Analog-to-Digital Converter Interface A).
Provides functions for configuration of conversion parameters (up to 12-bit signed at 1.5 Msps), channel sequencing (max. 16 channels, w/ 16 different inputs and up to 64x gain), window monitoring, interrupt and conversion triggering.
Data Structures | |
struct | adcifa_opt_t |
Parameters for the ADCIFA peripheral. More... | |
struct | adcifa_sequencer_conversion_opt_t |
Parameters for an conversion in the Sequencer. More... | |
struct | adcifa_sequencer_opt_t |
Parameters for the configuration of the Sequencer. More... | |
struct | adcifa_window_monitor_opt_t |
Parameters for the windows monitor mode. More... | |
Macros | |
#define | ADCIFA_clear_eoc_sequencer_0() ((AVR32_ADCIFA.scr) |= (1 << AVR32_ADCIFA_SCR_SEOC0)) |
Sequencer 0 : Ack end of Conversion. More... | |
#define | ADCIFA_clear_eoc_sequencer_1() ((AVR32_ADCIFA.scr) |= (1 << AVR32_ADCIFA_SCR_SEOC1) |
Sequencer 1 : Ack end of Conversion. More... | |
#define | ADCIFA_clear_eos_sequencer_0() ((AVR32_ADCIFA.scr) |= (1 << AVR32_ADCIFA_SCR_SEOS0)) |
Sequencer 0 : Ack end of Sequence. More... | |
#define | ADCIFA_clear_eos_sequencer_1() ((AVR32_ADCIFA.scr) |= (1 << AVR32_ADCIFA_SCR_SEOS1)) |
Sequencer 1 : Ack end of Sequence. More... | |
#define | ADCIFA_clear_window_0() ((AVR32_ADCIFA.scr) |= (1 << AVR32_ADCIFA_SCR_WM0)) |
Window Monitor 0 : Ack the Window Monitor 0 Status Bit. More... | |
#define | ADCIFA_clear_window_1() ((AVR32_ADCIFA.scr) |= (1 << AVR32_ADCIFA_SCR_WM1)) |
Window Monitor 1 : Ack the Window Monitor 1 Status Bit. More... | |
#define | ADCIFA_CONFIGURATION_ACCEPTED 0x1 |
This constant is used as return value for adcifa_configure and adcifa_configure_sequencer functions. More... | |
#define | ADCIFA_CONFIGURATION_REFUSED 0x0 |
This constant is used as return value for adcifa_configure and adcifa_configure_sequencer functions. More... | |
#define | ADCIFA_configure_muxsel0n(m7, m6, m5, m4, m3, m2, m1, m0) |
Configuration of Mux Negative for Sequencer 0. More... | |
#define | ADCIFA_configure_muxsel0p(m7, m6, m5, m4, m3, m2, m1, m0) |
Configuration of Mux Positive for Sequencer 0. More... | |
#define | ADCIFA_configure_muxsel1n(m7, m6, m5, m4, m3, m2, m1, m0) |
Configuration of Mux Negative for Sequencer 1. More... | |
#define | ADCIFA_configure_muxsel1p(m7, m6, m5, m4, m3, m2, m1, m0) |
Configuration of Mux Positive for Sequencer 1. More... | |
#define | ADCIFA_configure_sequencer_0(cnvnb, sres, trgsel, socb, sh_mode, hwla, sa) |
Configuration of Sequencer 0. More... | |
#define | ADCIFA_configure_sequencer_1(cnvnb, sres, trgsel, socb, csws, hwla, sa) |
Configuration of Sequencer 1. More... | |
#define | ADCIFA_configure_sh0gain(g7, g6, g5, g4, g3, g2, g1, g0) |
Configuration of Gain for Sequencer 0. More... | |
#define | ADCIFA_configure_sh1gain(g7, g6, g5, g4, g3, g2, g1, g0) |
Configuration of Gain for Sequencer 1. More... | |
#define | ADCIFA_disable() |
Enable the ADCIFA. More... | |
#define | ADCIFA_enable() |
Enable the ADCIFA. More... | |
#define | ADCIFA_is_eoc_sequencer_0() |
Sequencer 0 : Check end of Conversion. More... | |
#define | ADCIFA_is_eoc_sequencer_1() |
Sequencer 1 : Check end of Conversion. More... | |
#define | ADCIFA_is_eos_sequencer_0() |
Sequencer 0 : Check end of Sequence. More... | |
#define | ADCIFA_is_eos_sequencer_1() |
Sequencer 1 : Check end of Sequence. More... | |
#define | ADCIFA_is_startup_time() |
Check Startup Time flag. More... | |
#define | ADCIFA_is_window_0_set() |
Window Monitor 0 : Check the Window Monitor 0 Status Bit. More... | |
#define | ADCIFA_is_window_1_set() |
Window Monitor 1 : Check the Window Monitor 1 Status Bit. More... | |
#define | ADCIFA_NONE 0xFF |
Parameter. More... | |
#define | ADCIFA_read_resx_sequencer_0(ind) ((int32_t)AVR32_ADCIFA.resx[(ind)]) |
Return result for conversion for Sequencer 0. More... | |
#define | ADCIFA_read_resx_sequencer_1(ind) ((int)AVR32_ADCIFA.resx[(ind) + 8]) |
Return result for conversion for Sequencer 1. More... | |
#define | ADCIFA_set_gain_calibration(gcal) |
Set Gain Calibration. More... | |
#define | ADCIFA_set_offset_calibration(ocal) |
Set Offset Calibration. More... | |
#define | ADCIFA_set_sh0_gain_calibration(scal) |
Set Sample & Hold Gain Calibration for Seq 0. More... | |
#define | ADCIFA_set_sh1_gain_calibration(scal) |
Set Sample & Hold Gain Calibration for Seq 0. More... | |
#define | ADCIFA_softsoc_sequencer(seq) |
#define | ADCIFA_softsoc_sequencer_0() { AVR32_ADCIFA.cr = AVR32_ADCIFA_CR_SOC0_MASK; } |
Sequencer 0 : Software Start of Conversion. More... | |
#define | ADCIFA_softsoc_sequencer_1() { AVR32_ADCIFA.cr = AVR32_ADCIFA_CR_SOC1_MASK; } |
Sequencer 1 : Software Start of Conversion. More... | |
#define | ADCIFA_START_UP_TIME 1000 |
ADCIFA Start-Up time (us) More... | |
#define | ADCIFA_STATUS_COMPLETED 0x2 |
This constant is used as return value for the adcifa_get_values_from_sequencer function. More... | |
#define | ADCIFA_STATUS_NOT_COMPLETED 0x3 |
This constant is used as return value for the adcifa_get_values_from_sequencer function. More... | |
#define | AVR32_FLASHC_FACTORY_PAGE_ADDRESS 0x80800200 |
#define | AVR32_FLASHC_FROW_GAIN0_MASK 0x000003FF |
#define | AVR32_FLASHC_FROW_GAIN0_OFFSET 0 |
#define | AVR32_FLASHC_FROW_GAIN0_WORD 8 |
#define | AVR32_FLASHC_FROW_GAIN1_MASK 0x03FF0000 |
#define | AVR32_FLASHC_FROW_GAIN1_OFFSET 16 |
#define | AVR32_FLASHC_FROW_GAIN1_WORD 8 |
#define | AVR32_FLASHC_FROW_GCAL_MASK 0x00007FFF |
#define | AVR32_FLASHC_FROW_GCAL_OFFSET 0 |
#define | AVR32_FLASHC_FROW_GCAL_WORD 4 |
#define | AVR32_FLASHC_FROW_OCAL_MASK 0x3F000000 |
#define | AVR32_FLASHC_FROW_OCAL_OFFSET 24 |
#define | AVR32_FLASHC_FROW_OCAL_WORD 4 |
Functions | |
void | adcifa_calibrate_offset (volatile avr32_adcifa_t *adcifa, adcifa_opt_t *p_adcifa_opt, uint32_t pb_hz) |
bool | adcifa_check_eoc (volatile avr32_adcifa_t *adcifa, uint8_t sequencer) |
Get End of Conversion status bit. More... | |
bool | adcifa_check_eos (volatile avr32_adcifa_t *adcifa, uint8_t sequencer) |
Get End of Conversion status bit. More... | |
void | adcifa_clear_interrupt (volatile avr32_adcifa_t *adcifa, uint32_t interrupt_flags) |
Clear any ADCIFA interrupt. More... | |
uint8_t | adcifa_configure (volatile avr32_adcifa_t *adcifa, adcifa_opt_t *p_adcifa_opt, uint32_t pb_hz) |
Configure ADCIFA. More... | |
uint8_t | adcifa_configure_sequencer (volatile avr32_adcifa_t *adcifa, uint8_t sequencer, adcifa_sequencer_opt_t *p_adcifa_sequencer_opt, adcifa_sequencer_conversion_opt_t *p_adcifa_sequencer_conversion_opt) |
Configure ADCIFA specific sequencer. More... | |
void | adcifa_configure_window_monitor (volatile avr32_adcifa_t *adcifa, uint8_t sequencer, adcifa_window_monitor_opt_t *adc_window_monitor_opt) |
Configure ADCIFA specific window monitor. More... | |
void | adcifa_disable_interrupt (volatile avr32_adcifa_t *adcifa, uint32_t interrupt_flags) |
Disable any ADCIFA interrupt. More... | |
void | adcifa_enable_interrupt (volatile avr32_adcifa_t *adcifa, uint32_t interrupt_flags) |
Enable any ADCIFA interrupt. More... | |
void | adcifa_get_calibration_data (volatile avr32_adcifa_t *adcifa, adcifa_opt_t *p_adcifa_opt) |
Get ADCIFA Calibration Data. More... | |
uint8_t | adcifa_get_values_from_sequencer (volatile avr32_adcifa_t *adcifa, uint8_t sequencer, adcifa_sequencer_opt_t *p_adcifa_sequencer_opt, int16_t *adcifa_values) |
Get channel values for a specific sequence. More... | |
void | adcifa_start_itimer (volatile avr32_adcifa_t *adcifa, uint32_t timer_count) |
Start the ADCIFA timer. More... | |
void | adcifa_start_sequencer (volatile avr32_adcifa_t *adcifa, uint8_t sequencer) |
Start analog to digital conversion for a specific sequencer. More... | |
void | adcifa_stop_itimer (volatile avr32_adcifa_t *adcifa) |
Stop the ADCIFA timer. More... | |
Positive Inputs used by the ADC | |
#define | AVR32_ADCIFA_INP_ADCIN0 0 |
#define | AVR32_ADCIFA_INP_ADCIN1 1 |
#define | AVR32_ADCIFA_INP_ADCIN2 2 |
#define | AVR32_ADCIFA_INP_ADCIN3 3 |
#define | AVR32_ADCIFA_INP_ADCIN4 4 |
#define | AVR32_ADCIFA_INP_ADCIN5 5 |
#define | AVR32_ADCIFA_INP_ADCIN6 6 |
#define | AVR32_ADCIFA_INP_ADCIN7 7 |
#define | AVR32_ADCIFA_INP_DAC0_INT 8 |
#define | AVR32_ADCIFA_INP_TSENSE 9 |
#define | AVR32_ADCIFA_INP_GNDANA 10 |
Negative Inputs used by the ADC | |
#define | AVR32_ADCIFA_INN_ADCIN8 0 |
#define | AVR32_ADCIFA_INN_ADCIN9 1 |
#define | AVR32_ADCIFA_INN_ADCIN10 2 |
#define | AVR32_ADCIFA_INN_ADCIN11 3 |
#define | AVR32_ADCIFA_INN_ADCIN12 4 |
#define | AVR32_ADCIFA_INN_ADCIN13 5 |
#define | AVR32_ADCIFA_INN_ADCIN14 6 |
#define | AVR32_ADCIFA_INN_ADCIN15 7 |
#define | AVR32_ADCIFA_INN_DAC1_INT 8 |
#define | AVR32_ADCIFA_INN_GNDANA 9 |
References used by the ADC | |
#define | ADCIFA_REF1V 0x0 /** Internal 1V reference */ |
#define | ADCIFA_REF06VDD 0x1 /** Internal 0.6 x VDDANA reference */ |
#define | ADCIFA_ADCREF0 0x2 /** External 0 reference ADCREF0 */ |
#define | ADCIFA_ADCREF1 0x3 /** External 1 reference ADCREF1 */ |
#define | ADCIFA_ADCREF 0x10 /** External reference ADCREFP/ADCREFN */ |
Triggering Source used by the ADC | |
#define | ADCIFA_TRGSEL_SOFT 0x0 /** Trigger Source Software */ |
#define | ADCIFA_TRGSEL_ITIMER 0x1 /** Trigger Source Timer */ |
#define | ADCIFA_TRGSEL_EVT 0x2 /** Trigger Source Event */ |
#define | ADCIFA_TRGSEL_CONTINUOUS 0x3 /** Trigger Source Continuous */ |
Resolution selected by the ADC | |
#define | ADCIFA_SRES_8B 0x2 /** Resolution 8-Bits */ |
#define | ADCIFA_SRES_10B 0x1 /** Resolution 10-Bits */ |
#define | ADCIFA_SRES_12B 0x0 /** Resolution 12-Bits */ |
Gain selected on a Conversion by the ADC | |
#define | ADCIFA_SHG_1 0x0 /** Gain Conversion = 1 */ |
#define | ADCIFA_SHG_2 0x1 /** Gain Conversion = 2 */ |
#define | ADCIFA_SHG_4 0x2 /** Gain Conversion = 4 */ |
#define | ADCIFA_SHG_8 0x3 /** Gain Conversion = 8 */ |
#define | ADCIFA_SHG_16 0x4 /** Gain Conversion = 16 */ |
#define | ADCIFA_SHG_32 0x5 /** Gain Conversion = 32 */ |
#define | ADCIFA_SHG_64 0x6 /** Gain Conversion = 64 */ |
Conversion Management of the Sequence | |
#define | ADCIFA_SOCB_ALLSEQ |
#define | ADCIFA_SOCB_SINGLECONV |
Sampling Mode (OVSX2 & SHDYN) | |
#define | ADCIFA_SH_MODE_STANDARD 0x0 /** No dynamic over sampling */ |
#define | ADCIFA_SH_MODE_OVERSAMP 0x1 /** Over sampling: OVSX2 = 1 */ |
#define | ADCIFA_SH_MODE_DYNAMIC 0x2 /** Dynamic: SHDYN = 1 */ |
Half Word Left Adjustment (HWLA) | |
#define | ADCIFA_HWLA_NOADJ 0x0 /** Disable the HWLA mode */ |
#define | ADCIFA_HWLA_LEFTADJ 0x1 /** Enable the HWLA mode */ |
Software Acknowledge (SA) | |
#define | ADCIFA_SA_EOS_SOFTACK 0x0 /** Disable the SA mode */ |
#define | ADCIFA_SA_NO_EOS_SOFTACK 0x1 /** Enable the SA mode */ |
Sequence numbers | |
#define | ADCIFA_SEQ0 0x0 |
#define | ADCIFA_SEQ1 0x1 |
#define | ADCIFA_SEQ0_SEQ1 0x3 |
Window monitor | |
#define | ADCIFA_WINDOW_MODE_NONE 0 /** No Window Mode : Default */ |
#define | ADCIFA_WINDOW_MODE_BELOW 1 /** Active : Result < High Threshold */ |
#define | ADCIFA_WINDOW_MODE_ABOVE 2 /** Active : Result > Low Threshold */ |
#define | ADCIFA_WINDOW_MODE_INSIDE 3 /** Active : Low Threshold < Result < High Threshold */ |
#define | ADCIFA_WINDOW_MODE_OUTSIDE 4 /** Active : Result >= Low Threshold or Result >= High Threshold */ |
#define ADCIFA_ADCREF 0x10 /** External reference ADCREFP/ADCREFN */ |
#define ADCIFA_ADCREF0 0x2 /** External 0 reference ADCREF0 */ |
#define ADCIFA_ADCREF1 0x3 /** External 1 reference ADCREF1 */ |
#define ADCIFA_clear_eoc_sequencer_0 | ( | ) | ((AVR32_ADCIFA.scr) |= (1 << AVR32_ADCIFA_SCR_SEOC0)) |
Sequencer 0 : Ack end of Conversion.
#define ADCIFA_clear_eoc_sequencer_1 | ( | ) | ((AVR32_ADCIFA.scr) |= (1 << AVR32_ADCIFA_SCR_SEOC1) |
Sequencer 1 : Ack end of Conversion.
#define ADCIFA_clear_eos_sequencer_0 | ( | ) | ((AVR32_ADCIFA.scr) |= (1 << AVR32_ADCIFA_SCR_SEOS0)) |
Sequencer 0 : Ack end of Sequence.
#define ADCIFA_clear_eos_sequencer_1 | ( | ) | ((AVR32_ADCIFA.scr) |= (1 << AVR32_ADCIFA_SCR_SEOS1)) |
Sequencer 1 : Ack end of Sequence.
#define ADCIFA_clear_window_0 | ( | ) | ((AVR32_ADCIFA.scr) |= (1 << AVR32_ADCIFA_SCR_WM0)) |
Window Monitor 0 : Ack the Window Monitor 0 Status Bit.
#define ADCIFA_clear_window_1 | ( | ) | ((AVR32_ADCIFA.scr) |= (1 << AVR32_ADCIFA_SCR_WM1)) |
Window Monitor 1 : Ack the Window Monitor 1 Status Bit.
#define ADCIFA_CONFIGURATION_ACCEPTED 0x1 |
This constant is used as return value for adcifa_configure and adcifa_configure_sequencer functions.
Referenced by adcifa_configure(), and adcifa_configure_sequencer().
#define ADCIFA_CONFIGURATION_REFUSED 0x0 |
This constant is used as return value for adcifa_configure and adcifa_configure_sequencer functions.
#define ADCIFA_configure_muxsel0n | ( | m7, | |
m6, | |||
m5, | |||
m4, | |||
m3, | |||
m2, | |||
m1, | |||
m0 | |||
) |
Configuration of Mux Negative for Sequencer 0.
m(x) : ADC Channel for element x of Sequencer 0
Referenced by adcifa_configure_sequencer().
#define ADCIFA_configure_muxsel0p | ( | m7, | |
m6, | |||
m5, | |||
m4, | |||
m3, | |||
m2, | |||
m1, | |||
m0 | |||
) |
Configuration of Mux Positive for Sequencer 0.
m(x) : ADC Channel for element x of Sequencer 0
Referenced by adcifa_configure_sequencer().
#define ADCIFA_configure_muxsel1n | ( | m7, | |
m6, | |||
m5, | |||
m4, | |||
m3, | |||
m2, | |||
m1, | |||
m0 | |||
) |
Configuration of Mux Negative for Sequencer 1.
m(x) : ADC Channel for element x of Sequencer 1
Referenced by adcifa_configure_sequencer().
#define ADCIFA_configure_muxsel1p | ( | m7, | |
m6, | |||
m5, | |||
m4, | |||
m3, | |||
m2, | |||
m1, | |||
m0 | |||
) |
Configuration of Mux Positive for Sequencer 1.
m(x) : ADC Channel for element x of Sequencer 1
Referenced by adcifa_configure_sequencer().
#define ADCIFA_configure_sequencer_0 | ( | cnvnb, | |
sres, | |||
trgsel, | |||
socb, | |||
sh_mode, | |||
hwla, | |||
sa | |||
) |
Configuration of Sequencer 0.
cnvb : Number of conversion sres : ADCIFA Resolution trgsel : Trigger Selection socb : Start of Conversion Selection csws : CSWS Mode Selection hwla : HWLA Mode Selection sa : SA Mode Selection
Referenced by adcifa_configure_sequencer().
#define ADCIFA_configure_sequencer_1 | ( | cnvnb, | |
sres, | |||
trgsel, | |||
socb, | |||
csws, | |||
hwla, | |||
sa | |||
) |
Configuration of Sequencer 1.
cnvb : Number of conversion sres : ADCIFA Resolution trgsel : Trigger Selection socb : Start of Conversion Selection csws : CSWS Mode Selection hwla : HWLA Mode Selection sa : SA Mode Selection
Referenced by adcifa_configure_sequencer().
#define ADCIFA_configure_sh0gain | ( | g7, | |
g6, | |||
g5, | |||
g4, | |||
g3, | |||
g2, | |||
g1, | |||
g0 | |||
) |
Configuration of Gain for Sequencer 0.
g(x) : Gain for element x of Sequencer 0
Referenced by adcifa_configure_sequencer().
#define ADCIFA_configure_sh1gain | ( | g7, | |
g6, | |||
g5, | |||
g4, | |||
g3, | |||
g2, | |||
g1, | |||
g0 | |||
) |
Configuration of Gain for Sequencer 1.
g(x) : Gain for element x of Sequencer 1
Referenced by adcifa_configure_sequencer().
#define ADCIFA_disable | ( | ) |
Enable the ADCIFA.
#define ADCIFA_enable | ( | ) |
Enable the ADCIFA.
Referenced by adcifa_configure().
#define ADCIFA_HWLA_LEFTADJ 0x1 /** Enable the HWLA mode */ |
#define ADCIFA_HWLA_NOADJ 0x0 /** Disable the HWLA mode */ |
Referenced by adcifa_calibrate_offset().
#define ADCIFA_is_eoc_sequencer_0 | ( | ) |
Sequencer 0 : Check end of Conversion.
Referenced by adcifa_check_eoc().
#define ADCIFA_is_eoc_sequencer_1 | ( | ) |
Sequencer 1 : Check end of Conversion.
Referenced by adcifa_check_eoc().
#define ADCIFA_is_eos_sequencer_0 | ( | ) |
Sequencer 0 : Check end of Sequence.
Referenced by adcifa_calibrate_offset(), and adcifa_check_eos().
#define ADCIFA_is_eos_sequencer_1 | ( | ) |
Sequencer 1 : Check end of Sequence.
Referenced by adcifa_check_eos().
#define ADCIFA_is_startup_time | ( | ) |
Check Startup Time flag.
Referenced by adcifa_configure().
#define ADCIFA_is_window_0_set | ( | ) |
Window Monitor 0 : Check the Window Monitor 0 Status Bit.
#define ADCIFA_is_window_1_set | ( | ) |
Window Monitor 1 : Check the Window Monitor 1 Status Bit.
#define ADCIFA_NONE 0xFF |
Parameter.
#define ADCIFA_read_resx_sequencer_0 | ( | ind | ) | ((int32_t)AVR32_ADCIFA.resx[(ind)]) |
Return result for conversion for Sequencer 0.
ind : Index on element of Sequencer 0
Referenced by adcifa_calibrate_offset(), and adcifa_get_values_from_sequencer().
#define ADCIFA_read_resx_sequencer_1 | ( | ind | ) | ((int)AVR32_ADCIFA.resx[(ind) + 8]) |
Return result for conversion for Sequencer 1.
Referenced by adcifa_get_values_from_sequencer().
#define ADCIFA_REF06VDD 0x1 /** Internal 0.6 x VDDANA reference */ |
#define ADCIFA_REF1V 0x0 /** Internal 1V reference */ |
#define ADCIFA_SA_EOS_SOFTACK 0x0 /** Disable the SA mode */ |
#define ADCIFA_SA_NO_EOS_SOFTACK 0x1 /** Enable the SA mode */ |
Referenced by adcifa_calibrate_offset().
#define ADCIFA_SEQ0 0x0 |
Referenced by adcifa_start_sequencer().
#define ADCIFA_SEQ0_SEQ1 0x3 |
Referenced by adcifa_start_sequencer().
#define ADCIFA_SEQ1 0x1 |
Referenced by adcifa_start_sequencer().
#define ADCIFA_set_gain_calibration | ( | gcal | ) |
Set Gain Calibration.
Referenced by adcifa_configure().
#define ADCIFA_set_offset_calibration | ( | ocal | ) |
Set Offset Calibration.
Referenced by adcifa_configure().
#define ADCIFA_set_sh0_gain_calibration | ( | scal | ) |
Set Sample & Hold Gain Calibration for Seq 0.
Referenced by adcifa_configure().
#define ADCIFA_set_sh1_gain_calibration | ( | scal | ) |
Set Sample & Hold Gain Calibration for Seq 0.
Referenced by adcifa_configure().
#define ADCIFA_SH_MODE_DYNAMIC 0x2 /** Dynamic: SHDYN = 1 */ |
#define ADCIFA_SH_MODE_OVERSAMP 0x1 /** Over sampling: OVSX2 = 1 */ |
Referenced by adcifa_calibrate_offset().
#define ADCIFA_SH_MODE_STANDARD 0x0 /** No dynamic over sampling */ |
#define ADCIFA_SHG_1 0x0 /** Gain Conversion = 1 */ |
Referenced by adcifa_calibrate_offset().
#define ADCIFA_SHG_16 0x4 /** Gain Conversion = 16 */ |
#define ADCIFA_SHG_2 0x1 /** Gain Conversion = 2 */ |
#define ADCIFA_SHG_32 0x5 /** Gain Conversion = 32 */ |
#define ADCIFA_SHG_4 0x2 /** Gain Conversion = 4 */ |
#define ADCIFA_SHG_64 0x6 /** Gain Conversion = 64 */ |
#define ADCIFA_SHG_8 0x3 /** Gain Conversion = 8 */ |
#define ADCIFA_SOCB_ALLSEQ |
Referenced by adcifa_calibrate_offset().
#define ADCIFA_SOCB_SINGLECONV |
#define ADCIFA_softsoc_sequencer | ( | seq | ) |
Referenced by adcifa_start_sequencer().
#define ADCIFA_softsoc_sequencer_0 | ( | ) | { AVR32_ADCIFA.cr = AVR32_ADCIFA_CR_SOC0_MASK; } |
Sequencer 0 : Software Start of Conversion.
#define ADCIFA_softsoc_sequencer_1 | ( | ) | { AVR32_ADCIFA.cr = AVR32_ADCIFA_CR_SOC1_MASK; } |
Sequencer 1 : Software Start of Conversion.
#define ADCIFA_SRES_10B 0x1 /** Resolution 10-Bits */ |
#define ADCIFA_SRES_12B 0x0 /** Resolution 12-Bits */ |
Referenced by adcifa_calibrate_offset().
#define ADCIFA_SRES_8B 0x2 /** Resolution 8-Bits */ |
#define ADCIFA_START_UP_TIME 1000 |
ADCIFA Start-Up time (us)
Referenced by adcifa_configure().
#define ADCIFA_STATUS_COMPLETED 0x2 |
This constant is used as return value for the adcifa_get_values_from_sequencer function.
Referenced by adc_process_task(), and adcifa_get_values_from_sequencer().
#define ADCIFA_STATUS_NOT_COMPLETED 0x3 |
This constant is used as return value for the adcifa_get_values_from_sequencer function.
Referenced by adcifa_get_values_from_sequencer().
#define ADCIFA_TRGSEL_CONTINUOUS 0x3 /** Trigger Source Continuous */ |
#define ADCIFA_TRGSEL_EVT 0x2 /** Trigger Source Event */ |
#define ADCIFA_TRGSEL_ITIMER 0x1 /** Trigger Source Timer */ |
#define ADCIFA_TRGSEL_SOFT 0x0 /** Trigger Source Software */ |
Referenced by adcifa_calibrate_offset().
#define ADCIFA_WINDOW_MODE_ABOVE 2 /** Active : Result > Low Threshold */ |
#define ADCIFA_WINDOW_MODE_BELOW 1 /** Active : Result < High Threshold */ |
#define ADCIFA_WINDOW_MODE_INSIDE 3 /** Active : Low Threshold < Result < High Threshold */ |
#define ADCIFA_WINDOW_MODE_NONE 0 /** No Window Mode : Default */ |
#define ADCIFA_WINDOW_MODE_OUTSIDE 4 /** Active : Result >= Low Threshold or Result >= High Threshold */ |
#define AVR32_ADCIFA_INN_ADCIN10 2 |
#define AVR32_ADCIFA_INN_ADCIN11 3 |
#define AVR32_ADCIFA_INN_ADCIN12 4 |
#define AVR32_ADCIFA_INN_ADCIN13 5 |
#define AVR32_ADCIFA_INN_ADCIN14 6 |
#define AVR32_ADCIFA_INN_ADCIN15 7 |
#define AVR32_ADCIFA_INN_ADCIN8 0 |
#define AVR32_ADCIFA_INN_ADCIN9 1 |
#define AVR32_ADCIFA_INN_DAC1_INT 8 |
#define AVR32_ADCIFA_INN_GNDANA 9 |
Referenced by adcifa_calibrate_offset().
#define AVR32_ADCIFA_INP_ADCIN0 0 |
#define AVR32_ADCIFA_INP_ADCIN1 1 |
#define AVR32_ADCIFA_INP_ADCIN2 2 |
#define AVR32_ADCIFA_INP_ADCIN3 3 |
#define AVR32_ADCIFA_INP_ADCIN4 4 |
#define AVR32_ADCIFA_INP_ADCIN5 5 |
#define AVR32_ADCIFA_INP_ADCIN6 6 |
#define AVR32_ADCIFA_INP_ADCIN7 7 |
#define AVR32_ADCIFA_INP_DAC0_INT 8 |
#define AVR32_ADCIFA_INP_GNDANA 10 |
Referenced by adcifa_calibrate_offset().
#define AVR32_ADCIFA_INP_TSENSE 9 |
#define AVR32_FLASHC_FACTORY_PAGE_ADDRESS 0x80800200 |
Referenced by adcifa_get_calibration_data().
#define AVR32_FLASHC_FROW_GAIN0_MASK 0x000003FF |
Referenced by adcifa_get_calibration_data().
#define AVR32_FLASHC_FROW_GAIN0_OFFSET 0 |
Referenced by adcifa_get_calibration_data().
#define AVR32_FLASHC_FROW_GAIN0_WORD 8 |
Referenced by adcifa_get_calibration_data().
#define AVR32_FLASHC_FROW_GAIN1_MASK 0x03FF0000 |
Referenced by adcifa_get_calibration_data().
#define AVR32_FLASHC_FROW_GAIN1_OFFSET 16 |
Referenced by adcifa_get_calibration_data().
#define AVR32_FLASHC_FROW_GAIN1_WORD 8 |
Referenced by adcifa_get_calibration_data().
#define AVR32_FLASHC_FROW_GCAL_MASK 0x00007FFF |
Referenced by adcifa_get_calibration_data().
#define AVR32_FLASHC_FROW_GCAL_OFFSET 0 |
Referenced by adcifa_get_calibration_data().
#define AVR32_FLASHC_FROW_GCAL_WORD 4 |
Referenced by adcifa_get_calibration_data().
#define AVR32_FLASHC_FROW_OCAL_MASK 0x3F000000 |
Referenced by adcifa_get_calibration_data().
#define AVR32_FLASHC_FROW_OCAL_OFFSET 24 |
Referenced by adcifa_get_calibration_data().
#define AVR32_FLASHC_FROW_OCAL_WORD 4 |
Referenced by adcifa_get_calibration_data().
void adcifa_calibrate_offset | ( | volatile avr32_adcifa_t * | adcifa, |
adcifa_opt_t * | p_adcifa_opt, | ||
uint32_t | pb_hz | ||
) |
References adcifa_configure(), adcifa_configure_sequencer(), ADCIFA_HWLA_NOADJ, ADCIFA_is_eos_sequencer_0, ADCIFA_read_resx_sequencer_0, ADCIFA_SA_NO_EOS_SOFTACK, adcifa_sequence_opt, ADCIFA_SH_MODE_OVERSAMP, ADCIFA_SHG_1, ADCIFA_SOCB_ALLSEQ, ADCIFA_SRES_12B, adcifa_start_sequencer(), ADCIFA_TRGSEL_SOFT, AVR32_ADCIFA_INN_GNDANA, AVR32_ADCIFA_INP_GNDANA, CALIBRATION_ADCIFA_NUMBER_OF_SEQUENCE, adcifa_sequencer_conversion_opt_t::channel_n, adcifa_sequencer_conversion_opt_t::channel_p, adcifa_sequencer_opt_t::convnb, adcifa_opt_t::free_running_mode_enable, adcifa_sequencer_conversion_opt_t::gain, adcifa_sequencer_opt_t::half_word_adjustment, adcifa_opt_t::mux_settle_more_time, adcifa_opt_t::offset_calibration_value, adcifa_sequencer_opt_t::resolution, adcifa_opt_t::sample_and_hold_disable, adcifa_sequencer_opt_t::sh_mode, adcifa_opt_t::single_sequencer_mode, adcifa_opt_t::sleep_mode_enable, adcifa_sequencer_opt_t::software_acknowledge, adcifa_sequencer_opt_t::start_of_conversion, and adcifa_sequencer_opt_t::trigger_selection.
bool adcifa_check_eoc | ( | volatile avr32_adcifa_t * | adcifa, |
uint8_t | sequencer | ||
) |
Get End of Conversion status bit.
adcifa | Base address of the ADCIFA |
sequencer | Sequencer index |
References ADCIFA_is_eoc_sequencer_0, ADCIFA_is_eoc_sequencer_1, and Assert.
bool adcifa_check_eos | ( | volatile avr32_adcifa_t * | adcifa, |
uint8_t | sequencer | ||
) |
Get End of Conversion status bit.
adcifa | Base address of the ADCIFA |
sequencer | Sequencer index |
References ADCIFA_is_eos_sequencer_0, ADCIFA_is_eos_sequencer_1, and Assert.
Referenced by adcifa_get_values_from_sequencer().
void adcifa_clear_interrupt | ( | volatile avr32_adcifa_t * | adcifa, |
uint32_t | interrupt_flags | ||
) |
Clear any ADCIFA interrupt.
*adcifa | Base address of the ADCIFA |
interrupt_flags | Interrupt mask |
uint8_t adcifa_configure | ( | volatile avr32_adcifa_t * | adcifa, |
adcifa_opt_t * | p_adcifa_opt, | ||
uint32_t | pb_hz | ||
) |
Configure ADCIFA.
Mandatory to call.
If not called, ADC channels will have side effects
adcifa | Base address of the ADCIFA |
p_adcifa_opt | Structure for the ADCIFA core configuration |
pb_hz | Peripheral Bus frequency |
References ADCIFA_CONFIGURATION_ACCEPTED, ADCIFA_enable, ADCIFA_is_startup_time, ADCIFA_set_gain_calibration, ADCIFA_set_offset_calibration, ADCIFA_set_sh0_gain_calibration, ADCIFA_set_sh1_gain_calibration, ADCIFA_START_UP_TIME, Assert, adcifa_opt_t::free_running_mode_enable, adcifa_opt_t::frequency, adcifa_opt_t::gain_calibration_value, adcifa_opt_t::mux_settle_more_time, adcifa_opt_t::offset_calibration_value, adcifa_opt_t::reference_source, adcifa_opt_t::sample_and_hold_disable, adcifa_opt_t::sh0_calibration_value, adcifa_opt_t::sh1_calibration_value, adcifa_opt_t::single_sequencer_mode, and adcifa_opt_t::sleep_mode_enable.
Referenced by adc_process_init(), and adcifa_calibrate_offset().
uint8_t adcifa_configure_sequencer | ( | volatile avr32_adcifa_t * | adcifa, |
uint8_t | sequencer, | ||
adcifa_sequencer_opt_t * | p_adcifa_sequencer_opt, | ||
adcifa_sequencer_conversion_opt_t * | p_adcifa_sequencer_conversion_opt | ||
) |
Configure ADCIFA specific sequencer.
- Sequence, Gain and Mux
adcifa | Base address of the ADCIFA |
sequencer | Sequencer index |
p_adcifa_sequencer_opt | Structure for the sequencer configuration |
p_adcifa_sequencer_conversion_opt | Pointer on a buffer for each conversion on a sequencer |
References ADCIFA_CONFIGURATION_ACCEPTED, ADCIFA_configure_muxsel0n, ADCIFA_configure_muxsel0p, ADCIFA_configure_muxsel1n, ADCIFA_configure_muxsel1p, ADCIFA_configure_sequencer_0, ADCIFA_configure_sequencer_1, ADCIFA_configure_sh0gain, ADCIFA_configure_sh1gain, adcifa_seq1_configured, Assert, adcifa_sequencer_conversion_opt_t::channel_n, adcifa_sequencer_conversion_opt_t::channel_p, adcifa_sequencer_opt_t::convnb, adcifa_sequencer_conversion_opt_t::gain, adcifa_sequencer_opt_t::half_word_adjustment, adcifa_sequencer_opt_t::resolution, adcifa_sequencer_opt_t::sh_mode, adcifa_sequencer_opt_t::software_acknowledge, adcifa_sequencer_opt_t::start_of_conversion, and adcifa_sequencer_opt_t::trigger_selection.
Referenced by adc_process_init(), and adcifa_calibrate_offset().
void adcifa_configure_window_monitor | ( | volatile avr32_adcifa_t * | adcifa, |
uint8_t | sequencer, | ||
adcifa_window_monitor_opt_t * | adc_window_monitor_opt | ||
) |
Configure ADCIFA specific window monitor.
adcifa | Base address of the ADCIFA |
sequencer | Sequencer index |
adc_window_monitor_opt | Structure for the sequencer configuration |
References adcifa_window_monitor_opt_t::high_threshold, adcifa_window_monitor_opt_t::low_threshold, adcifa_window_monitor_opt_t::mode, and adcifa_window_monitor_opt_t::source_index.
void adcifa_disable_interrupt | ( | volatile avr32_adcifa_t * | adcifa, |
uint32_t | interrupt_flags | ||
) |
Disable any ADCIFA interrupt.
adcifa | Base address of the ADCIFA |
interrupt_flags | Interrupt mask |
void adcifa_enable_interrupt | ( | volatile avr32_adcifa_t * | adcifa, |
uint32_t | interrupt_flags | ||
) |
Enable any ADCIFA interrupt.
adcifa | Base address of the ADCIFA |
interrupt_flags | Interrupt mask |
void adcifa_get_calibration_data | ( | volatile avr32_adcifa_t * | adcifa, |
adcifa_opt_t * | p_adcifa_opt | ||
) |
Get ADCIFA Calibration Data.
Mandatory to call if factory calibration data are wanted to be used. If not called, Calibration Data should be set by the application.
adcifa | Base address of the ADCIFA |
p_adcifa_opt | Structure for the ADCIFA core configuration |
References AVR32_FLASHC_FACTORY_PAGE_ADDRESS, AVR32_FLASHC_FROW_GAIN0_MASK, AVR32_FLASHC_FROW_GAIN0_OFFSET, AVR32_FLASHC_FROW_GAIN0_WORD, AVR32_FLASHC_FROW_GAIN1_MASK, AVR32_FLASHC_FROW_GAIN1_OFFSET, AVR32_FLASHC_FROW_GAIN1_WORD, AVR32_FLASHC_FROW_GCAL_MASK, AVR32_FLASHC_FROW_GCAL_OFFSET, AVR32_FLASHC_FROW_GCAL_WORD, AVR32_FLASHC_FROW_OCAL_MASK, AVR32_FLASHC_FROW_OCAL_OFFSET, AVR32_FLASHC_FROW_OCAL_WORD, adcifa_opt_t::gain_calibration_value, adcifa_opt_t::offset_calibration_value, adcifa_opt_t::sh0_calibration_value, and adcifa_opt_t::sh1_calibration_value.
Referenced by adc_process_init().
uint8_t adcifa_get_values_from_sequencer | ( | volatile avr32_adcifa_t * | adcifa, |
uint8_t | sequencer, | ||
adcifa_sequencer_opt_t * | p_adcifa_sequencer_opt, | ||
int16_t * | adcifa_values | ||
) |
Get channel values for a specific sequence.
adcifa | Base address of the ADCIFA |
sequencer | Sequencer index |
p_adcifa_sequencer_opt | Structure for the sequencer configuration |
adcifa_values | Pointer on the converter values |
References adcifa_check_eos(), ADCIFA_read_resx_sequencer_0, ADCIFA_read_resx_sequencer_1, ADCIFA_STATUS_COMPLETED, ADCIFA_STATUS_NOT_COMPLETED, Assert, and adcifa_sequencer_opt_t::convnb.
Referenced by adc_process_task().
void adcifa_start_itimer | ( | volatile avr32_adcifa_t * | adcifa, |
uint32_t | timer_count | ||
) |
Start the ADCIFA timer.
adcifa | Base address of the ADCIFA |
timer_count | Fs = Fadc / (timer_counter + 1) |
void adcifa_start_sequencer | ( | volatile avr32_adcifa_t * | adcifa, |
uint8_t | sequencer | ||
) |
Start analog to digital conversion for a specific sequencer.
adcifa | Base address of the ADCIFA |
sequencer | Sequencer index |
References ADCIFA_SEQ0, ADCIFA_SEQ0_SEQ1, ADCIFA_SEQ1, ADCIFA_softsoc_sequencer, and Assert.
Referenced by adc_process_task(), and adcifa_calibrate_offset().
void adcifa_stop_itimer | ( | volatile avr32_adcifa_t * | adcifa | ) |
Stop the ADCIFA timer.
adcifa | Base address of the ADCIFA |