Microchip® Advanced Software Framework

Todo List
Global do_listen (struct api_msg_msg *msg)
: should we drain the recvmbox here?
Global get_cur_lun (void)
Implement.
Global host_get_data (U8 pipe, U16 *nb_data, void *ptr_buf)
Error code management
Global host_mass_storage_task_sync_drives (signed short FsNavId, U8 sync_direction, const char *pcdir_name, bool bDeleteSrc)
Do recursive directory copy...
Global host_suspend_action (void)
Implement this on the silicon version
Global host_transfer_control (void *data_pointer)
Fix all time-out errors and disconnections in active wait loop.
Global ISR (func, int_grp, int_lvl)
Update to use IRQ numbers when these are made available in the device header files of both IAR and GCC.
Global LWIP_NETIF_TX_SINGLE_PBUF
: TCP and IP-frag do not work with this, yet:
Global netconn_is_nonblocking (conn)
: write/send is missing)
Global netconn_set_nonblocking (conn, val)
: write/send is missing)
Global pll_wait_for_lock (unsigned int pll_id)
Use a timeout to avoid waiting forever and hanging the system
File snmp_structs.h
namespace prefixes
Global stream_state (U8 id)
Implement.
Global stream_stop (U8 id)
Implement.
Global sysclk_get_cpu_hz (void)
This function assumes that the CPU always runs at the system clock frequency. We want to support at least two more scenarios: Fixed CPU/bus clock dividers (config symbols) and dynamic CPU/bus clock dividers (which may change at run time). Ditto for all the bus clocks.
Global sysclk_get_main_hz (void)
This function assumes that the main clock source never changes once it's been set up, and that PLL0 always runs at the compile-time configured default rate. While this is probably the most common configuration, which we want to support as a special case for performance reasons, we will at some point need to support more dynamic setups as well.
Global usb_device_task_init (void)
Implement this on the silicon version
Global usb_general_interrupt_non_naked (void)

ID pin hot state change!!!

Implement this on the silicon version

Global usb_host_task (void *pvParameters)
Global usb_host_task_init (void)
Implement this on the silicon version
Group USBB_host_driver
Implement macros for endpoint DMA registers and descriptors