#include "conf_explorer.h"
Data Structures | |
struct | Fs_index |
Macros | |
#define | _GLOBEXT_ extern |
Used to have a clear code with only one segment to define a variable in project. More... | |
Modes of file name control functions | |
#define | FS_NAME_GET true |
#define | FS_NAME_CHECK false |
Modes of disk serial number function | |
#define | FS_SN_READ true |
#define | FS_SN_WRITE false |
Modes of disk label function | |
#define | FS_LABEL_READ true |
#define | FS_LABEL_WRITE false |
Status returned by paste file function | |
#define | COPY_BUSY 0x00 |
#define | COPY_FAIL 0x01 |
#define | COPY_FINISH 0x02 |
Date field managed by date control functions | |
#define | FS_DATE_CREATION true |
#define | FS_DATE_LAST_WRITE false |
File entry types used by many functions | |
#define | FS_FILE true |
#define | FS_DIR false |
Directory identifier, which corresponding at the first cluster of directory cluster list | |
#define | FS_ID_DIR_EMPTY 0xFFFFFFFF |
#define | FS_ID_DIR_ROOT 0 |
File entry attributes | |
#define | FS_ATTR_FILE ((Byte)0x00) |
#define | FS_ATTR_READ_ONLY ((Byte)0x01) |
#define | FS_ATTR_HIDDEN ((Byte)0x02) |
#define | FS_ATTR_SYSTEM ((Byte)0x04) |
#define | FS_ATTR_VOLUME_ID ((Byte)0x08) |
#define | FS_ATTR_DIRECTORY ((Byte)0x10) |
#define | FS_ATTR_ARCHIVE ((Byte)0x20) |
#define | FS_ATTR_LFN_ENTRY ((Byte)0x0F) |
#define | Fat_is_not_a_file ((FS_ATTR_DIRECTORY & fs_g_nav_entry.u8_attr) || (FS_ATTR_VOLUME_ID & fs_g_nav_entry.u8_attr)) |
File open modes | |
#define | FOPEN_READ_ACCESS 0x01 |
#define | FOPEN_WRITE_ACCESS 0x02 |
#define | FOPEN_CLEAR_SIZE 0x04 |
#define | FOPEN_CLEAR_PTR 0x08 |
#define | FOPEN_MODE_R (FOPEN_READ_ACCESS|FOPEN_CLEAR_PTR) |
R access, flux pointer = 0, size not modify. More... | |
#define | FOPEN_MODE_R_PLUS (FOPEN_READ_ACCESS|FOPEN_WRITE_ACCESS|FOPEN_CLEAR_PTR) |
R/W access, flux pointer = 0, size not modify. More... | |
#define | FOPEN_MODE_W (FOPEN_WRITE_ACCESS|FOPEN_CLEAR_PTR|FOPEN_CLEAR_SIZE) |
W access, flux pointer = 0, size = 0. More... | |
#define | FOPEN_MODE_W_PLUS (FOPEN_READ_ACCESS|FOPEN_WRITE_ACCESS|FOPEN_CLEAR_PTR|FOPEN_CLEAR_SIZE) |
R/W access, flux pointer = 0, size = 0. More... | |
#define | FOPEN_MODE_APPEND (FOPEN_WRITE_ACCESS) |
W access, flux pointer = at the end, size not modify. More... | |
Value to signal the end of file after a file_getc() call | |
#define | FS_EOF 0xFFFF |
Options of format function | |
#define | FS_FORMAT_DEFAULT 0x01 |
The format routine chooses the better FAT for the device. More... | |
#define | FS_FORMAT_FAT 0x02 |
Force FAT12 or FAT16 format. More... | |
#define | FS_FORMAT_FAT32 0x03 |
Force FAT32 format. More... | |
#define | FS_FORMAT_NOMBR_FLAG 0x80 |
MBR is mandatory for USB device on MacOS, and no MBR is mandatory for CD-ROM USB device on Windows. More... | |
#define | FS_FORMAT_DEFAULT_NOMBR (FS_FORMAT_NOMBR_FLAG | FS_FORMAT_DEFAULT) |
#define | FS_FORMAT_FAT_NOMBR (FS_FORMAT_NOMBR_FLAG | FS_FORMAT_FAT) |
#define | FS_FORMAT_FAT32_NOMBR (FS_FORMAT_NOMBR_FLAG | FS_FORMAT_FAT32) |
File System errors list | |
#define | FS_ERR_HW (FAIL+0) |
Hardware driver error. More... | |
#define | FS_ERR_NO_FORMAT (FAIL+1) |
The selected drive isn't formated. More... | |
#define | FS_ERR_NO_PART (FAIL+2) |
The selected partition doesn't existed. More... | |
#define | FS_ERR_NO_SUPPORT_PART (FAIL+3) |
The selected partition isn't supported. More... | |
#define | FS_ERR_TOO_FILE_OPEN (FAIL+4) |
The navigation have already opened a file. More... | |
#define | FS_ERR_END_OF_DRIVE (FAIL+5) |
There are not other driver. More... | |
#define | FS_ERR_BAD_POS (FAIL+6) |
The position is over the file. More... | |
#define | FS_ERR_FS (FAIL+7) |
File system error. More... | |
#define | FS_ERR_NO_FIND (FAIL+8) |
File no found. More... | |
#define | FS_ERR_ENTRY_EMPTY (FAIL+9) |
File entry empty. More... | |
#define | FS_ERR_ENTRY_BAD (FAIL+10) |
File entry bad. More... | |
#define | FS_ERR_ENTRY_BADTYPE (FAIL+11) |
File entry type don't corresponding. More... | |
#define | FS_ERR_NO_DIR (FAIL+12) |
The selected file isn't a directory. More... | |
#define | FS_ERR_NO_MOUNT (FAIL+13) |
The partition isn't mounted. More... | |
#define | FS_ERR_NO_FILE_SEL (FAIL+14) |
There are no selected file. More... | |
#define | FS_NO_LAST_LFN_ENTRY (FAIL+15) |
The file entry isn't the last long file entry. More... | |
#define | FS_ERR_ID_FILE (FAIL+17) |
The file identifier is bad. More... | |
#define | FS_ERR_NO_FILE (FAIL+18) |
The selected file entry isn't a file. More... | |
#define | FS_LUN_WP (FAIL+19) |
Drive is in read only mode. More... | |
#define | FS_ERR_READ_ONLY (FAIL+20) |
File is on read access only. More... | |
#define | FS_ERR_NAME_INCORRECT (FAIL+21) |
The name don't corresponding at the filter name. More... | |
#define | FS_ERR_FILE_NO_OPEN (FAIL+22) |
No file is opened. More... | |
#define | FS_ERR_HW_NO_PRESENT (FAIL+23) |
Device is not present. More... | |
#define | FS_ERR_IS_ROOT (FAIL+24) |
There aren't parent because the current directory is a root directory. More... | |
#define | FS_ERR_OUT_LIST (FAIL+25) |
The position is outside the cluster list. More... | |
#define | FS_ERR_NO_FREE_SPACE (FAIL+26) |
No free cluster found in FAT. More... | |
#define | FS_ERR_INCORRECT_NAME (FAIL+27) |
Incorrect name, this one cannot contain any of the following characters \/:*?"<>|. More... | |
#define | FS_ERR_DIR_NOT_EMPTY (FAIL+28) |
This function erases only file and empty directory. More... | |
#define | FS_ERR_WRITE_ONLY (FAIL+29) |
File is on write access only. More... | |
#define | FS_ERR_MODE_NOAVIALABLE (FAIL+30) |
This open mode isn't available. More... | |
#define | FS_ERR_EOF (FAIL+31) |
End of file. More... | |
#define | FS_ERR_BAD_SIZE_FAT (FAIL+32) |
The disk size is not supported by selected FAT format. More... | |
#define | FS_ERR_COMMAND (FAIL+33) |
This command is not supported. More... | |
#define | FS_ERR_BUFFER_FULL (FAIL+34) |
Buffer is too small. More... | |
#define | FS_ERR_COPY_DIR (FAIL+35) |
Directory copy is not supported. More... | |
#define | FS_ERR_COPY_RUNNING (FAIL+36) |
A copy action is always running. More... | |
#define | FS_ERR_COPY_IMPOSSIBLE (FAIL+37) |
The copy is impossible. More... | |
#define | FS_ERR_BAD_NAV (FAIL+38) |
The navigator identifier doesn't existed. More... | |
#define | FS_ERR_FILE_OPEN (FAIL+39) |
The file is already opened. More... | |
#define | FS_ERR_FILE_OPEN_WR (FAIL+40) |
The file is already opened in write mode. More... | |
#define | FS_ERR_FILE_EXIST (FAIL+41) |
The file is already existed. More... | |
#define | FS_ERR_NAME_TOO_LARGE (FAIL+42) |
The file name is too large (>260 characters) More... | |
#define | FS_ERR_DEVICE_TOO_SMALL (FAIL+43) |
The disk size is too small for format routine. More... | |
#define | FS_ERR_PL_NOT_OPEN (FAIL+50) |
The play list isn't opened. More... | |
#define | FS_ERR_PL_ALREADY_OPEN (FAIL+51) |
The play list is already opened. More... | |
#define | FS_ERR_PL_LST_END (FAIL+52) |
You are at the end of play list. More... | |
#define | FS_ERR_PL_LST_BEG (FAIL+53) |
You are at the beginning of play list. More... | |
#define | FS_ERR_PL_OUT_LST (FAIL+54) |
You are outside of the play list. More... | |
#define | FS_ERR_PL_READ_ONLY (FAIL+55) |
Impossible to modify the play list. More... | |
Compilation feature levels | |
#define | FSFEATURE_READ 0x00 |
All read functions. More... | |
#define | FSFEATURE_WRITE 0x02 |
nav_file_copy(), nav_file_paste(), nav_file_del(), file_create(), file_open(MODE_WRITE), file_write(), file_putc() More... | |
#define | FSFEATURE_WRITE_COMPLET 0x06 |
FSFEATURE_WRITE + nav_drive_format(), nav_dir_make(), nav_file_rename(), nav_file_dateset(), nav_file_attributset() More... | |
#define | FSFEATURE_ALL 0xFF |
All file system module. More... | |
Typedefs | |
String types depend of ASCII and UNICODE options | |
typedef uint16_t | UNICODE |
typedef char _MEM_TYPE_SLOW_ * | FS_STRING |
typedef UNICODE _MEM_TYPE_SLOW_ * | FS_STR_UNICODE |
Status type for the file system | |
typedef uint8_t | Fs_status |
Variables | |
Global status of file system module (used to return error number) | |
_GLOBEXT_ _MEM_TYPE_SLOW_ Fs_status | fs_g_status |
#define _GLOBEXT_ extern |
Used to have a clear code with only one segment to define a variable in project.
#define COPY_BUSY 0x00 |
Referenced by nav_file_paste_state().
#define COPY_FAIL 0x01 |
Referenced by nav_file_paste_state().
#define COPY_FINISH 0x02 |
Referenced by nav_file_paste_state().
#define Fat_is_not_a_file ((FS_ATTR_DIRECTORY & fs_g_nav_entry.u8_attr) || (FS_ATTR_VOLUME_ID & fs_g_nav_entry.u8_attr)) |
Referenced by fat_check_is_file().
#define FOPEN_CLEAR_PTR 0x08 |
Referenced by file_open().
#define FOPEN_CLEAR_SIZE 0x04 |
Referenced by file_open().
#define FOPEN_MODE_APPEND (FOPEN_WRITE_ACCESS) |
W access, flux pointer = at the end, size not modify.
#define FOPEN_MODE_R (FOPEN_READ_ACCESS|FOPEN_CLEAR_PTR) |
R access, flux pointer = 0, size not modify.
Referenced by nav_file_paste_start().
#define FOPEN_MODE_R_PLUS (FOPEN_READ_ACCESS|FOPEN_WRITE_ACCESS|FOPEN_CLEAR_PTR) |
R/W access, flux pointer = 0, size not modify.
#define FOPEN_MODE_W (FOPEN_WRITE_ACCESS|FOPEN_CLEAR_PTR|FOPEN_CLEAR_SIZE) |
W access, flux pointer = 0, size = 0.
#define FOPEN_MODE_W_PLUS (FOPEN_READ_ACCESS|FOPEN_WRITE_ACCESS|FOPEN_CLEAR_PTR|FOPEN_CLEAR_SIZE) |
R/W access, flux pointer = 0, size = 0.
Referenced by nav_file_paste_start().
#define FOPEN_READ_ACCESS 0x01 |
Referenced by file_getc(), file_read(), and file_read_buf().
#define FOPEN_WRITE_ACCESS 0x02 |
Referenced by fat_check_nav_access_file(), file_close(), file_open(), file_putc(), file_set_eof(), and file_write_buf().
#define FS_ATTR_ARCHIVE ((Byte)0x20) |
#define FS_ATTR_DIRECTORY ((Byte)0x10) |
Referenced by fat_entry_check(), and fat_entry_is_dir().
#define FS_ATTR_FILE ((Byte)0x00) |
#define FS_ATTR_HIDDEN ((Byte)0x02) |
#define FS_ATTR_LFN_ENTRY ((Byte)0x0F) |
Referenced by fat_create_long_name_entry(), fat_delete_file(), fat_entry_longname(), and fat_entry_shortname_compare().
#define FS_ATTR_READ_ONLY ((Byte)0x01) |
Referenced by file_open(), and nav_file_isreadonly().
#define FS_ATTR_SYSTEM ((Byte)0x04) |
#define FS_ATTR_VOLUME_ID ((Byte)0x08) |
Referenced by fat_entry_check(), and fat_entry_label().
#define FS_DATE_CREATION true |
#define FS_DATE_LAST_WRITE false |
Referenced by fat_get_date().
#define FS_DIR false |
Referenced by fat_clear_entry_info_and_ptr(), fat_entry_check(), nav_dir_gotoparent(), nav_filelist_eol(), and nav_filelist_set().
#define FS_EOF 0xFFFF |
Referenced by file_getc().
#define FS_ERR_BAD_NAV (FAIL+38) |
The navigator identifier doesn't existed.
Referenced by nav_select().
#define FS_ERR_BAD_POS (FAIL+6) |
The position is over the file.
Referenced by file_seek().
#define FS_ERR_BAD_SIZE_FAT (FAIL+32) |
The disk size is not supported by selected FAT format.
Referenced by fat_select_filesystem().
#define FS_ERR_BUFFER_FULL (FAIL+34) |
Buffer is too small.
Referenced by nav_getcwd().
#define FS_ERR_COMMAND (FAIL+33) |
This command is not supported.
Referenced by fat_cluster_val().
#define FS_ERR_COPY_DIR (FAIL+35) |
Directory copy is not supported.
Referenced by nav_file_copy().
#define FS_ERR_COPY_IMPOSSIBLE (FAIL+37) |
The copy is impossible.
#define FS_ERR_COPY_RUNNING (FAIL+36) |
A copy action is always running.
Referenced by nav_file_paste_start().
#define FS_ERR_DEVICE_TOO_SMALL (FAIL+43) |
The disk size is too small for format routine.
Referenced by fat_select_filesystem().
#define FS_ERR_DIR_NOT_EMPTY (FAIL+28) |
This function erases only file and empty directory.
#define FS_ERR_END_OF_DRIVE (FAIL+5) |
There are not other driver.
Referenced by nav_drive_set().
#define FS_ERR_ENTRY_BAD (FAIL+10) |
File entry bad.
Referenced by fat_entry_check(), fat_entry_label(), fat_entry_longname(), fat_entry_shortname_compare(), and nav_file_name().
#define FS_ERR_ENTRY_BADTYPE (FAIL+11) |
File entry type don't corresponding.
#define FS_ERR_ENTRY_EMPTY (FAIL+9) |
File entry empty.
Referenced by fat_entry_check(), fat_entry_label(), fat_entry_shortname_compare(), fat_find_short_entry_name(), nav_filelist_set(), and nav_partition_label().
#define FS_ERR_EOF (FAIL+31) |
End of file.
Referenced by file_getc(), file_read(), and file_read_buf().
#define FS_ERR_FILE_EXIST (FAIL+41) |
The file is already existed.
Referenced by nav_file_create().
#define FS_ERR_FILE_NO_OPEN (FAIL+22) |
No file is opened.
Referenced by fat_check_open().
#define FS_ERR_FILE_OPEN (FAIL+39) |
The file is already opened.
Referenced by fat_check_nav_access_file().
#define FS_ERR_FILE_OPEN_WR (FAIL+40) |
The file is already opened in write mode.
Referenced by fat_check_nav_access_file().
#define FS_ERR_FS (FAIL+7) |
File system error.
Referenced by fat_cluster_list(), nav_dir_gotoparent(), and nav_filelist_set().
#define FS_ERR_HW (FAIL+0) |
Hardware driver error.
Referenced by fat_cache_flush(), fat_cache_read_sector(), fat_check_device(), file_read_buf(), and file_write_buf().
#define FS_ERR_HW_NO_PRESENT (FAIL+23) |
Device is not present.
Referenced by fat_check_device().
#define FS_ERR_ID_FILE (FAIL+17) |
The file identifier is bad.
#define FS_ERR_INCORRECT_NAME (FAIL+27) |
Incorrect name, this one cannot contain any of the following characters \/:*?"<>|.
Referenced by fat_check_name().
#define FS_ERR_IS_ROOT (FAIL+24) |
There aren't parent because the current directory is a root directory.
Referenced by nav_dir_gotoparent(), and nav_getcwd().
#define FS_ERR_MODE_NOAVIALABLE (FAIL+30) |
This open mode isn't available.
Referenced by file_open().
#define FS_ERR_NAME_INCORRECT (FAIL+21) |
The name don't corresponding at the filter name.
Referenced by fat_entry_label(), fat_entry_longname(), and fat_entry_shortname().
#define FS_ERR_NAME_TOO_LARGE (FAIL+42) |
The file name is too large (>260 characters)
Referenced by fat_check_name().
#define FS_ERR_NO_DIR (FAIL+12) |
The selected file isn't a directory.
Referenced by fat_entry_is_dir().
#define FS_ERR_NO_FILE (FAIL+18) |
The selected file entry isn't a file.
Referenced by fat_check_is_file().
#define FS_ERR_NO_FILE_SEL (FAIL+14) |
There are no selected file.
Referenced by fat_check_select().
#define FS_ERR_NO_FIND (FAIL+8) |
File no found.
Referenced by nav_filelist_first(), nav_filelist_last(), and nav_filelist_set().
#define FS_ERR_NO_FORMAT (FAIL+1) |
The selected drive isn't formated.
Referenced by fat_mount().
#define FS_ERR_NO_FREE_SPACE (FAIL+26) |
No free cluster found in FAT.
Referenced by fat_alloc_entry_free().
#define FS_ERR_NO_MOUNT (FAIL+13) |
The partition isn't mounted.
Referenced by fat_check_mount().
#define FS_ERR_NO_PART (FAIL+2) |
The selected partition doesn't existed.
Referenced by fat_mount().
#define FS_ERR_NO_SUPPORT_PART (FAIL+3) |
The selected partition isn't supported.
Referenced by fat_mount().
#define FS_ERR_OUT_LIST (FAIL+25) |
The position is outside the cluster list.
Referenced by fat_alloc_entry_free(), fat_cluster_list(), fat_find_short_entry_name(), fat_garbage_collector_entry(), fat_read_file(), file_getc(), file_read(), file_read_buf(), and nav_filelist_set().
#define FS_ERR_PL_ALREADY_OPEN (FAIL+51) |
The play list is already opened.
#define FS_ERR_PL_LST_BEG (FAIL+53) |
You are at the beginning of play list.
#define FS_ERR_PL_LST_END (FAIL+52) |
You are at the end of play list.
#define FS_ERR_PL_NOT_OPEN (FAIL+50) |
The play list isn't opened.
#define FS_ERR_PL_OUT_LST (FAIL+54) |
You are outside of the play list.
#define FS_ERR_PL_READ_ONLY (FAIL+55) |
Impossible to modify the play list.
#define FS_ERR_READ_ONLY (FAIL+20) |
File is on read access only.
Referenced by file_open(), file_putc(), file_set_eof(), and file_write_buf().
#define FS_ERR_TOO_FILE_OPEN (FAIL+4) |
The navigation have already opened a file.
Referenced by fat_check_noopen().
#define FS_ERR_WRITE_ONLY (FAIL+29) |
File is on write access only.
Referenced by file_getc(), file_read(), and file_read_buf().
#define FS_FILE true |
Referenced by fat_entry_check(), nav_dir_name(), nav_file_create(), nav_filelist_nb(), and nav_filelist_set().
#define FS_FORMAT_DEFAULT 0x01 |
The format routine chooses the better FAT for the device.
#define FS_FORMAT_DEFAULT_NOMBR (FS_FORMAT_NOMBR_FLAG | FS_FORMAT_DEFAULT) |
#define FS_FORMAT_FAT 0x02 |
Force FAT12 or FAT16 format.
Referenced by fat_select_filesystem().
#define FS_FORMAT_FAT32 0x03 |
Force FAT32 format.
Referenced by fat_select_filesystem().
#define FS_FORMAT_FAT32_NOMBR (FS_FORMAT_NOMBR_FLAG | FS_FORMAT_FAT32) |
#define FS_FORMAT_FAT_NOMBR (FS_FORMAT_NOMBR_FLAG | FS_FORMAT_FAT) |
#define FS_FORMAT_NOMBR_FLAG 0x80 |
MBR is mandatory for USB device on MacOS, and no MBR is mandatory for CD-ROM USB device on Windows.
Referenced by fat_format().
#define FS_ID_DIR_EMPTY 0xFFFFFFFF |
#define FS_ID_DIR_ROOT 0 |
#define FS_LABEL_READ true |
Referenced by fat_entry_label(), and nav_partition_label().
#define FS_LABEL_WRITE false |
Referenced by fat_entry_label(), and nav_partition_label().
#define FS_LUN_WP (FAIL+19) |
Drive is in read only mode.
Referenced by fat_cache_flush(), and file_open().
#define FS_NAME_CHECK false |
Referenced by nav_filelist_findname().
#define FS_NAME_GET true |
Referenced by fat_entry_longname(), fat_entry_shortname(), nav_dir_name(), nav_file_getname(), nav_file_name(), and nav_getcwd().
#define FS_NO_LAST_LFN_ENTRY (FAIL+15) |
The file entry isn't the last long file entry.
Referenced by fat_entry_longname(), and nav_file_name().
#define FS_SN_READ true |
Referenced by fat_serialnumber().
#define FS_SN_WRITE false |
#define FSFEATURE_ALL 0xFF |
All file system module.
#define FSFEATURE_READ 0x00 |
All read functions.
#define FSFEATURE_WRITE 0x02 |
nav_file_copy(), nav_file_paste(), nav_file_del(), file_create(), file_open(MODE_WRITE), file_write(), file_putc()
#define FSFEATURE_WRITE_COMPLET 0x06 |
FSFEATURE_WRITE + nav_drive_format(), nav_dir_make(), nav_file_rename(), nav_file_dateset(), nav_file_attributset()
typedef uint8_t Fs_status |
typedef UNICODE _MEM_TYPE_SLOW_* FS_STR_UNICODE |
typedef char _MEM_TYPE_SLOW_* FS_STRING |
typedef uint16_t UNICODE |
_GLOBEXT_ _MEM_TYPE_SLOW_ Fs_status fs_g_status |
Referenced by fat_alloc_entry_free(), fat_cache_flush(), fat_cache_read_sector(), fat_check_device(), fat_check_is_file(), fat_check_mount(), fat_check_name(), fat_check_nav_access_file(), fat_check_noopen(), fat_check_open(), fat_check_select(), fat_cluster_list(), fat_cluster_val(), fat_entry_check(), fat_entry_is_dir(), fat_entry_label(), fat_entry_longname(), fat_entry_shortname(), fat_entry_shortname_compare(), fat_find_short_entry_name(), fat_garbage_collector_entry(), fat_mount(), fat_read_file(), fat_select_filesystem(), file_getc(), file_open(), file_putc(), file_read(), file_read_buf(), file_seek(), file_set_eof(), file_write_buf(), nav_dir_gotoparent(), nav_drive_set(), nav_file_copy(), nav_file_create(), nav_file_name(), nav_file_paste_start(), nav_filelist_first(), nav_filelist_last(), nav_filelist_set(), nav_getcwd(), nav_partition_label(), and nav_select().