Microchip® Advanced Software Framework

 All Data Structures Files Functions Variables Typedefs Enumerations Enumerator Macros Groups Pages
Wireless USB Application UC3A AT86RF212-RZ600 Documentation

Introduction

This application is a Wireless-UART using the USB CDC class (Virtual Communication Port). If a byte is received via the serial connection from one node, the node transmits the byte to the other node. If the transmission was successful, the entered bytes are forwarded to the terminal indicating successful transmission.

Main files:

  • main.c: main file with
    • setup the clocks,
    • setup the USB
    • main loop.
  • rz600.h: board configuration for the UC3 A3 MCU (SPI config).

Device Info

This application is targeted for the UC3 A3 MCU on RZ600 boards.

Compilation Info

This software was written for the GNU GCC and IAR for AVR. Other compilers may or may not work.

Contact Information

For further information, visit Atmel AVR.