Main file of the AVR UC3 A3 Wireless UART application.
Copyright (c) 2014-2018 Microchip Technology Inc. and its subsidiaries.
#include <string.h>
#include "compiler.h"
#include "board.h"
#include "sysclk.h"
#include "conf_usb.h"
#include "conf_at86rfx.h"
#include "udd.h"
#include "udc.h"
#include "udi_cdc.h"
#include "at86rfx_driver.h"
Macros | |
#define | BUFFER_SIZE (200) |
Typedefs | |
typedef enum tx_state_tag | tx_state_t |
Enum to store the current TX state of application. More... | |
Enumerations | |
enum | tx_state_tag { TX_IDLE = 0, TX_ONGOING } |
Enum to store the current TX state of application. More... | |
Functions | |
static void | app_task (void) |
Application task responsible for transferring bytes received from USB to RF module. More... | |
void | at86rfx_tal_rx_frame_cb (uint8_t *rx_frame_array) |
Callback that is called once a frame is received. More... | |
void | at86rfx_tal_tx_status_cb (uint8_t status) |
Callback that is called once tx is done. More... | |
int | main (void) |
Main function. Execution starts here. More... | |
void | main_cdc_disable (void) |
Called by CDC interface Callback running when USB Host disable cdc interface. More... | |
bool | main_cdc_enable (void) |
Called by CDC interface Callback running when USB Host enable CDC interface. More... | |
void | usb_rx_notify (void) |
Callback that is called once a byte is received from USB. More... | |
static void | usb_task (void) |
USB task responsible for extracting the bytes received from USB buffer. More... | |
Variables | |
static volatile bool | main_b_cdc_enable = false |
static uint8_t | tx_buffer [BUFFER_SIZE] |
static tx_state_t | tx_state = TX_IDLE |
static uint8_t | usb_rx_buff_len = 0 |
static uint8_t | usb_rx_buffer [BUFFER_SIZE] |
static volatile bool | usb_rx_byte_rcvd = false |
#define BUFFER_SIZE (200) |
Referenced by usb_task().
typedef enum tx_state_tag tx_state_t |
Enum to store the current TX state of application.
enum tx_state_tag |
|
static |
Application task responsible for transferring bytes received from USB to RF module.
References at86rfx_tx_frame(), cpu_irq_disable, cpu_irq_enable, FCS_LEN, PHY_MAX_LENGTH, tx_buffer, TX_IDLE, TX_ONGOING, tx_state, usb_rx_buff_len, and usb_rx_buffer.
Referenced by main().
void at86rfx_tal_rx_frame_cb | ( | uint8_t * | rx_frame_array | ) |
Callback that is called once a frame is received.
rx_frame_array | Pointer for the received frame |
References FCS_LEN, LED0, LED_Toggle(), and udi_cdc_write_buf().
void at86rfx_tal_tx_status_cb | ( | uint8_t | status | ) |
Callback that is called once tx is done.
status | Status of the transmission procedure |
References AT86RFX_CHANNEL_ACCESS_FAILURE, AT86RFX_SUCCESS, at86rfx_tx_frame(), FCS_LEN, LED1, LED_Toggle(), tx_buffer, TX_IDLE, tx_state, and udi_cdc_write_buf().
int main | ( | void | ) |
Main function. Execution starts here.
References app_task(), Assert, at86rfx_init(), AT86RFX_SUCCESS, at86rfx_task(), board_init(), cpu_irq_enable, irq_initialize_vectors, sysclk_init(), udc_start(), and usb_task().
void main_cdc_disable | ( | void | ) |
Called by CDC interface Callback running when USB Host disable cdc interface.
References main_b_cdc_enable.
bool main_cdc_enable | ( | void | ) |
Called by CDC interface Callback running when USB Host enable CDC interface.
true | if cdc startup is successfully done |
References main_b_cdc_enable.
void usb_rx_notify | ( | void | ) |
Callback that is called once a byte is received from USB.
References usb_rx_byte_rcvd.
|
static |
USB task responsible for extracting the bytes received from USB buffer.
References BUFFER_SIZE, cpu_irq_disable, cpu_irq_enable, main_b_cdc_enable, udi_cdc_getc(), udi_cdc_is_rx_ready(), usb_rx_buff_len, usb_rx_buffer, and usb_rx_byte_rcvd.
Referenced by main().
Referenced by main_cdc_disable(), main_cdc_enable(), and usb_task().
|
static |
Referenced by app_task(), and at86rfx_tal_tx_status_cb().
|
static |
Referenced by app_task(), and at86rfx_tal_tx_status_cb().
|
static |
Referenced by app_task(), and usb_task().
|
static |
Referenced by app_task(), and usb_task().
Referenced by usb_rx_notify(), and usb_task().