Functions | |
at86rfx_retval_t | at86rfx_init (void) |
Initializes the transceiver interface. More... | |
void | at86rfx_task (void) |
RF task handling. More... | |
void | at86rfx_tx_frame (uint8_t *frame_tx) |
Transmits the frame. More... | |
uint8_t | pal_trx_bit_read (uint8_t addr, uint8_t mask, uint8_t pos) |
Subregister read. More... | |
void | pal_trx_bit_write (uint8_t reg_addr, uint8_t mask, uint8_t pos, uint8_t new_value) |
Subregister write. More... | |
void | pal_trx_frame_read (uint8_t *data, uint8_t length) |
Reads frame buffer of the transceiver. More... | |
void | pal_trx_frame_write (uint8_t *data, uint8_t length) |
Writes data into frame buffer of the transceiver. More... | |
void | pal_trx_init (void) |
Initializes the SPI and GPIO pins for transceiver access. More... | |
uint8_t | pal_trx_reg_read (uint8_t addr) |
Reads current value from a transceiver register. More... | |
void | pal_trx_reg_write (uint8_t addr, uint8_t data) |
Writes data into a transceiver register. More... | |
at86rfx_retval_t at86rfx_init | ( | void | ) |
Initializes the transceiver interface.
This function initializes the transceiver interface.
References AT86RFX_FAILURE, AT86RFX_SUCCESS, CMD_RX_ON, CURRENT_CHANNEL_DEFAULT, ENABLE_TRX_IRQ, pal_trx_bit_write(), pal_trx_init(), pal_trx_reg_write(), RG_TRX_STATE, SR_CHANNEL, tal_init(), and TRX_SUCCESS.
Referenced by main().
void at86rfx_task | ( | void | ) |
RF task handling.
This function
References at86rfx_frame_rx, at86rfx_rx_buffer, AT86RFX_RX_NOTIFY, and handle_tal_state().
Referenced by main().
void at86rfx_tx_frame | ( | uint8_t * | frame_tx | ) |
Transmits the frame.
This function configures the transceiver in TX mode and transmits the frame
[in] | frame_tx | Pointer to data to be transmitted |
References DISABLE_TRX_IRQ, ENABLE_TRX_IRQ, LENGTH_FIELD_LEN, pal_trx_frame_write(), and tx_frame_config().
Referenced by app_task(), and at86rfx_tal_tx_status_cb().
uint8_t pal_trx_bit_read | ( | uint8_t | addr, |
uint8_t | mask, | ||
uint8_t | pos | ||
) |
Subregister read.
addr | Offset of the register |
mask | Bit mask of the subregister |
pos | Bit position of the subregister |
References pal_trx_reg_read().
Referenced by generate_rand_seed(), handle_received_frame_irq(), set_trx_state(), switch_pll_on(), trx_init(), and trx_reset().
void pal_trx_bit_write | ( | uint8_t | reg_addr, |
uint8_t | mask, | ||
uint8_t | pos, | ||
uint8_t | new_value | ||
) |
Subregister write.
[in] | reg_addr | Offset of the register |
[in] | mask | Bit mask of the subregister |
[in] | pos | Bit position of the subregister |
[out] | new_value | Data, which is muxed into the register |
References pal_trx_reg_read(), and pal_trx_reg_write().
Referenced by at86rfx_init(), tal_init(), and trx_config().
void pal_trx_frame_read | ( | uint8_t * | data, |
uint8_t | length | ||
) |
Reads frame buffer of the transceiver.
This function reads the frame buffer of the transceiver.
[out] | data | Pointer to the location to store frame |
[in] | length | Number of bytes to be read from the frame buffer. |
References AT86RFX_SPI, ENTER_CRITICAL_REGION, LEAVE_CRITICAL_REGION, spi_deselect_device(), spi_read_packet(), spi_select_device(), spi_write_packet(), and TRX_CMD_FR.
Referenced by handle_received_frame_irq().
void pal_trx_frame_write | ( | uint8_t * | data, |
uint8_t | length | ||
) |
Writes data into frame buffer of the transceiver.
This function writes data into the frame buffer of the transceiver
[in] | data | Pointer to data to be written into frame buffer |
[in] | length | Number of bytes to be written into frame buffer |
References AT86RFX_SPI, ENTER_CRITICAL_REGION, LEAVE_CRITICAL_REGION, spi_deselect_device(), spi_select_device(), spi_write_packet(), and TRX_CMD_FW.
Referenced by at86rfx_tx_frame().
void pal_trx_init | ( | void | ) |
Initializes the SPI and GPIO pins for transceiver access.
This function configures the SPI in master mode and interrupt capability of GPIO pin to handle the interrupts from transceiver
References AT86RFX_SPI, AT86RFX_SPI_BAUDRATE, EXT_INT, EXT_INT_ISR_PRIORITY, gpio_clear_pin_interrupt_flag(), gpio_configure_pin(), GPIO_DIR_OUTPUT, gpio_enable_pin_interrupt(), GPIO_INIT_HIGH, GPIO_RISING_EDGE, irq_register_handler, SLP_TR, spi_deselect_device(), spi_enable(), spi_master_init(), spi_master_setup_device(), SPI_MODE_0, and TRX_RST.
Referenced by at86rfx_init().
uint8_t pal_trx_reg_read | ( | uint8_t | addr | ) |
Reads current value from a transceiver register.
This function reads the current value from a transceiver register.
addr | Specifies the address of the trx register from which the data shall be read |
References AT86RFX_SPI, ENTER_CRITICAL_REGION, LEAVE_CRITICAL_REGION, READ_ACCESS_COMMAND, spi_deselect_device(), spi_read_packet(), spi_select_device(), and spi_write_packet().
Referenced by generate_rand_seed(), pal_trx_bit_read(), pal_trx_bit_write(), switch_pll_on(), trx_init(), and trx_irq_handler_cb().
void pal_trx_reg_write | ( | uint8_t | addr, |
uint8_t | data | ||
) |
Writes data into a transceiver register.
This function writes a value into transceiver register.
addr | Address of the trx register |
data | Data to be written to trx register |
References AT86RFX_SPI, ENTER_CRITICAL_REGION, LEAVE_CRITICAL_REGION, spi_deselect_device(), spi_select_device(), spi_write_packet(), and WRITE_ACCESS_COMMAND.
Referenced by at86rfx_init(), pal_trx_bit_write(), set_trx_state(), switch_pll_on(), tal_init(), trx_config(), and trx_init().