Microchip® Advanced Software Framework

 All Data Structures Files Functions Variables Typedefs Enumerations Enumerator Macros Groups Pages
UC3-L0 Xplained demo application Documentation

Introduction

This application demonstrates the QMatrix functionality of the UC3-L0 Xplained board. On power-on, the board will initialize the required touch libraries, showing the current touch state of the slider and touch button on the board LEDs. The temperature sensor data will be sent to the USART connected to the board USB Virtual Com Port.

Contact Information

For further information, visit Atmel AVR UC3.