This is the documentation for the data structures, functions, variables, defines, enums, and typedefs for the NAND FLASH components.
The given example covers simple uses of a external NAND FLASH using EBI.
This example operates at 12MHz.
This software was written for the GNU GCC for AVR32 and IAR Systems compiler for AVR32. Other compilers may or may not work.
All AVR32 devices with a EBI module can be used. This example has been tested with the following setup:
For further information, visit Atmel AVR32.