#include "conf_access.h"
#include "conf_sd_mmc_mci.h"
#include "sd_mmc_mci.h"
#include "sd_mmc_mci_mem.h"
Macros | |
#define | Sd_mmc_mci_access_signal_off() |
#define | Sd_mmc_mci_access_signal_on() |
Functions | |
Control Interface | |
Ctrl_status | sd_mmc_mci_test_unit_ready (uint8_t slot) |
Tests the memory state and initializes the memory if required. More... | |
Ctrl_status | sd_mmc_mci_test_unit_ready_0 (void) |
Instance Declaration for sd_mmc_mci_test_unit_ready Slot O. More... | |
Ctrl_status | sd_mmc_mci_test_unit_ready_1 (void) |
Instance Declaration for sd_mmc_mci_test_unit_ready Slot 1. More... | |
Ctrl_status | sd_mmc_mci_read_capacity (uint8_t slot, uint32_t *nb_sector) |
Returns the address of the last valid sector in the memory. More... | |
Ctrl_status | sd_mmc_mci_read_capacity_0 (uint32_t *nb_sector) |
Instance Declaration for sd_mmc_mci_read_capacity Slot O. More... | |
Ctrl_status | sd_mmc_mci_read_capacity_1 (uint32_t *nb_sector) |
Instance Declaration for sd_mmc_mci_read_capacity Slot 1. More... | |
bool | sd_mmc_mci_wr_protect (uint8_t slot) |
Returns the write-protection state of the memory. More... | |
bool | sd_mmc_mci_wr_protect_0 (void) |
Instance Declaration for sd_mmc_mci_wr_protect Slot O. More... | |
bool | sd_mmc_mci_wr_protect_1 (void) |
Instance Declaration for sd_mmc_mci_wr_protect Slot 1. More... | |
bool | sd_mmc_mci_removal (uint8_t slot) |
Tells whether the memory is removable. More... | |
bool | sd_mmc_mci_removal_0 (void) |
Instance Declaration for sd_mmc_mci_removal Slot O. More... | |
bool | sd_mmc_mci_removal_1 (void) |
Instance Declaration for sd_mmc_mci_removal Slot 1. More... | |
MEM <-> RAM Interface | |
Ctrl_status | sd_mmc_mci_mem_2_ram (uint8_t slot, uint32_t addr, void *ram) |
Copies 1 data sector from the memory to RAM. More... | |
Ctrl_status | sd_mmc_mci_dma_mem_2_ram (uint8_t slot, uint32_t addr, void *ram) |
Ctrl_status | sd_mmc_mci_mem_2_ram_0 (uint32_t addr, void *ram) |
Instance Declaration for sd_mmc_mci_mem_2_ram Slot O. More... | |
Ctrl_status | sd_mmc_mci_mem_2_ram_1 (uint32_t addr, void *ram) |
Instance Declaration for sd_mmc_mci_mem_2_ram Slot 1. More... | |
Ctrl_status | sd_mmc_mci_multiple_mem_2_ram (uint8_t slot, uint32_t addr, void *ram, uint32_t nb_sectors) |
Copies nb_sectors data sector from the memory to RAM. More... | |
Ctrl_status | sd_mmc_mci_dma_multiple_mem_2_ram (uint8_t slot, uint32_t addr, void *ram, uint32_t nb_sectors) |
Ctrl_status | sd_mmc_mci_multiple_mem_2_ram_0 (uint32_t addr, void *ram, uint32_t nb_sectors) |
Instance Declaration for sd_mmc_mci_mem_2_ram Slot O. More... | |
Ctrl_status | sd_mmc_mci_multiple_mem_2_ram_1 (uint32_t addr, void *ram, uint32_t nb_sectors) |
Instance Declaration for sd_mmc_mci_mem_2_ram Slot 1. More... | |
Ctrl_status | sd_mmc_mci_ram_2_mem (uint8_t slot, uint32_t addr, const void *ram) |
Copies 1 data sector from RAM to the memory. More... | |
Ctrl_status | sd_mmc_mci_dma_ram_2_mem (uint8_t slot, uint32_t addr, const void *ram) |
Ctrl_status | sd_mmc_mci_ram_2_mem_0 (uint32_t addr, const void *ram) |
Instance Declaration for sd_mmc_mci_mem_2_ram Slot O. More... | |
Ctrl_status | sd_mmc_mci_ram_2_mem_1 (uint32_t addr, const void *ram) |
Instance Declaration for sd_mmc_mci_mem_2_ram Slot 1. More... | |
Ctrl_status | sd_mmc_mci_multiple_ram_2_mem (uint8_t slot, uint32_t addr, const void *ram, uint32_t nb_sectors) |
Copies nb_sectors data sector from RAM to the memory. More... | |
Ctrl_status | sd_mmc_mci_dma_multiple_ram_2_mem (uint8_t slot, uint32_t addr, const void *ram, uint32_t nb_sectors) |
Ctrl_status | sd_mmc_mci_multiple_ram_2_mem_0 (uint32_t addr, const void *ram, uint32_t nb_sectors) |
Instance Declaration for sd_mmc_mci_mem_2_ram Slot O. More... | |
Ctrl_status | sd_mmc_mci_multiple_ram_2_mem_1 (uint32_t addr, const void *ram, uint32_t nb_sectors) |
Instance Declaration for sd_mmc_mci_mem_2_ram Slot 1. More... | |
Variables | |
uint32_t | g_card_size [MCI_NR_SLOTS] |
SD/MMC Card Size per Slot. More... | |
bool | sd_mmc_mci_init_done [MCI_NR_SLOTS] |
Initialization sequence status per Slot. More... | |
static uint8_t | sd_mmc_mci_presence_status [MCI_NR_SLOTS] = {SD_MMC_INSERTED, SD_MMC_INSERTED} |
SD/MMC Card Presence status per Slot. More... | |
#define Sd_mmc_mci_access_signal_off | ( | ) |
Referenced by sd_mmc_mci_dma_mem_2_ram(), sd_mmc_mci_dma_multiple_mem_2_ram(), sd_mmc_mci_dma_multiple_ram_2_mem(), sd_mmc_mci_dma_ram_2_mem(), sd_mmc_mci_mem_2_ram(), sd_mmc_mci_multiple_mem_2_ram(), sd_mmc_mci_multiple_ram_2_mem(), sd_mmc_mci_ram_2_mem(), sd_mmc_mci_read_capacity(), and sd_mmc_mci_test_unit_ready().
#define Sd_mmc_mci_access_signal_on | ( | ) |
Referenced by sd_mmc_mci_read_capacity(), and sd_mmc_mci_test_unit_ready().
uint32_t g_card_size[MCI_NR_SLOTS] |
SD/MMC Card Size per Slot.
Referenced by sd_mmc_get_ext_csd(), sd_mmc_mci_get_csd(), and sd_mmc_mci_read_capacity().
bool sd_mmc_mci_init_done[MCI_NR_SLOTS] |
Initialization sequence status per Slot.
Referenced by sd_mmc_mci_card_init(), sd_mmc_mci_mem_check(), and sd_mmc_mci_test_unit_ready().
|
static |
SD/MMC Card Presence status per Slot.
Referenced by sd_mmc_mci_test_unit_ready().