Microchip® Advanced Software Framework

adcifb_sleepwalking_example.c File Reference

Example to illustrate the Sleepwalking feature with the ADCIFB module in AT32UC3L series.

Copyright (c) 2011-2018 Microchip Technology Inc. and its subsidiaries.

#include <stdint.h>
#include "compiler.h"
#include "board.h"
#include "conf_example.h"
#include "adcifb.h"
#include "gpio.h"
#include "ast.h"
#include "scif_uc3l.h"
#include "pm_uc3l.h"
#include "intc.h"
#include "sysclk.h"
#include "sleepmgr.h"
#include "delay.h"
#include "status_codes.h"

Macros

APPLICATION SPECIFIC CONFIGURATION
#define DEBUG_MESSAGES   DISABLE
 Enable Trace messages through USART terminal. More...
 
#define STATUS_LED   LED1_GPIO
 LED1_GPIO is used as status LED. More...
 
#define ERROR_LED   LED0_GPIO
 LED0_GPIO is used as error status LED. More...
 
#define LED_DELAY   10
 Delay in ms for LED blinking. More...
 
#define POWER_SUPPLY_MODE_1_8V   false
 Enable when operated in 1.8V VDDIN. More...
 
#define ADC   &AVR32_ADCIFB
 ADCIFB Module is used. More...
 
#define ADC_FREQUENCY   250000
 ADCIFB Clock Frequency - 1 MHz. More...
 
#define ADC_INTERRUPT_PRIORITY   1
 ADCIFB interrupt priority is set to 1. More...
 
#define ADC_SAMPLE_HOLD_TIME   4
 ADCIFB sample & hold time configuration - 0 Sample & Hold Time = (ADC_SAMPLE_HOLD_TIME + 3)* Tclk_adc. More...
 
#define ADC_COMPARE_VALUE   0x200
 ADCIFB compare value in Analog Compare Mode - 1.5V. More...
 
#define ADC_STARTUP_TIME   0
 ADCIFB startup time configuration - 0 Tstartup = (ADC_STARTUP_TIME + 1) * 8 * Tclk_adc (assuming Tstartup ~ 15us max) -> 1 * 8 * 1/250000 = 32us. More...
 
#define AST_CLOCK_SOURCE   AST_OSC_32KHZ
 32KHz external oscillator is used as AST source More...
 
#define AST_PRESCALER   AST_PSEL_32KHZ_1HZ
 Prescaler is set to AST_PSEL_32KHZ_1HZ to run at 1Hz. More...
 
#define AST_TRIGGER_PRESCALER   13
 Periodic interrupt prescaler is set to 12 for trigger in every 250ms. More...
 
#define NB_GPIO_USED_PINS   5
 

Functions

static status_code_t adc_init (void)
 Initializes the ADCIFB module with trigger. More...
 
static status_code_t ast_init (void)
 Initialize Asynchronous Timer to trigger ADCIFB module at regular intervals. More...
 
 ISR (ADCIFB_interrupt_handler, AVR32_ADCIFB_IRQ_GROUP, ADC_INTERRUPT_PRIORITY)
 ADCIFB ISR Routine. More...
 
int main (void)
 Main Application Routine. More...
 
static void power_save_measures_init (void)
 Initializes the power saving measures to reduce power consumption. More...
 

Variables

static uint32_t adc_output
 Static variable to store the ADCIFB output value. More...
 
volatile avr32_adcifb_t * adcifb = ADC
 Global variable to Store the ADCIFB module address. More...
 
static volatile unsigned int cycle_cnt
 
uint32_t gpio_used_pins [NB_GPIO_USED_PINS]
 Array to hold the used GPIO pins. More...
 

#define ADC   &AVR32_ADCIFB

ADCIFB Module is used.

#define ADC_COMPARE_VALUE   0x200

ADCIFB compare value in Analog Compare Mode - 1.5V.

Referenced by adc_init().

#define ADC_FREQUENCY   250000

ADCIFB Clock Frequency - 1 MHz.

Referenced by adc_init().

#define ADC_INTERRUPT_PRIORITY   1

ADCIFB interrupt priority is set to 1.

Referenced by adc_init().

#define ADC_SAMPLE_HOLD_TIME   4

ADCIFB sample & hold time configuration - 0 Sample & Hold Time = (ADC_SAMPLE_HOLD_TIME + 3)* Tclk_adc.

Referenced by adc_init().

#define ADC_STARTUP_TIME   0

ADCIFB startup time configuration - 0 Tstartup = (ADC_STARTUP_TIME + 1) * 8 * Tclk_adc (assuming Tstartup ~ 15us max) -> 1 * 8 * 1/250000 = 32us.

Referenced by adc_init().

#define AST_CLOCK_SOURCE   AST_OSC_32KHZ

32KHz external oscillator is used as AST source

Referenced by ast_init().

#define AST_PRESCALER   AST_PSEL_32KHZ_1HZ

Prescaler is set to AST_PSEL_32KHZ_1HZ to run at 1Hz.

Referenced by ast_init().

#define AST_TRIGGER_PRESCALER   13

Periodic interrupt prescaler is set to 12 for trigger in every 250ms.

Referenced by ast_init().

#define DEBUG_MESSAGES   DISABLE

Enable Trace messages through USART terminal.

#define ERROR_LED   LED0_GPIO

LED0_GPIO is used as error status LED.

Referenced by main().

#define LED_DELAY   10

Delay in ms for LED blinking.

Referenced by main().

#define NB_GPIO_USED_PINS   5
#define POWER_SUPPLY_MODE_1_8V   false

Enable when operated in 1.8V VDDIN.

#define STATUS_LED   LED1_GPIO

LED1_GPIO is used as status LED.

Referenced by main().

static status_code_t ast_init ( )
static

Initialize Asynchronous Timer to trigger ADCIFB module at regular intervals.

Asynchronous Timer Initialization.

  • Start the 32KHz Oscillator
  • Initializes the AST module with periodic trigger events
Return values
STATUS_OKConfiguration OK
ERR_TIMEOUTError in configuring the AST module

References ast_clear_all_status_flags(), AST_CLOCK_SOURCE, ast_enable(), ast_enable_periodic0(), ast_init_counter(), AST_PRESCALER, ast_set_periodic0_value(), AST_TRIGGER_PRESCALER, BOARD_OSC32_PINSEL, ERR_TIMEOUT, scif_osc32_opt_t::mode, OSC32_STARTUP_8192, SCIF_OSC_MODE_2PIN_CRYSTAL_HICUR, scif_start_osc32(), STATUS_OK, SYSCLK_AST, sysclk_disable_pba_module(), sysclk_enable_hsb_module(), sysclk_enable_pba_module(), and SYSCLK_EVENT.

Referenced by main().

ISR ( ADCIFB_interrupt_handler  ,
AVR32_ADCIFB_IRQ_GROUP  ,
ADC_INTERRUPT_PRIORITY   
)
int main ( void  )

Main Application Routine.

  • Initialize the system clocks
  • Initialize the sleep manager
  • Initialize the power save measures
  • Initialize the ADCIFB module
  • Initialize the AST to trigger ADCIFB at regular intervals
  • Go to STATIC sleep mode and wake up on a touch status change

References adc_init(), adc_output, ast_clear_all_status_flags(), ast_init(), DBG_USART, delay_init, delay_ms, ERROR_LED, gpio_clr_gpio_pin(), gpio_set_gpio_pin(), gpio_tgl_gpio_pin(), init_dbg_rs232(), LED_DELAY, pm_asyn_wake_up_disable(), pm_asyn_wake_up_enable(), power_save_measures_init(), print_dbg(), print_dbg_hex(), sleepmgr_enter_sleep(), sleepmgr_init(), sleepmgr_lock_mode(), SLEEPMGR_STATIC, STATUS_LED, STATUS_OK, sysclk_disable_pba_module(), sysclk_enable_pba_module(), sysclk_enable_peripheral_clock(), sysclk_get_cpu_hz(), sysclk_get_pba_hz(), SYSCLK_GPIO, and sysclk_init().

static void power_save_measures_init ( )
static

Initializes the power saving measures to reduce power consumption.

Low Power Configuration Initializes the power saving measures to reduce power consumption.

  • Enable pullups on GPIO pins
  • Disable the clocks to unused modules
  • Disable internal voltage regulator when in 1.8V supply mode

References gpio_configure_group(), GPIO_DIR_INPUT, GPIO_PULL_UP, gpio_used_pins, sysclk_disable_cpu_module(), and SYSCLK_OCD.

Referenced by main().

uint32_t adc_output
static

Static variable to store the ADCIFB output value.

Referenced by ISR(), and main().

volatile avr32_adcifb_t* adcifb = ADC

Global variable to Store the ADCIFB module address.

Referenced by adc_init(), and ISR().

volatile unsigned int cycle_cnt
static
uint32_t gpio_used_pins[NB_GPIO_USED_PINS]
Initial value:
= {
AVR32_SCIF_XIN32_2_0_PIN,
AVR32_SCIF_XOUT32_2_0_PIN,
}
#define EXAMPLE_ADCIFB_PIN
ADCIFB Input pin.
Definition: conf_example.h:45
#define STATUS_LED
LED1_GPIO is used as status LED.
Definition: adcifb_sleepwalking_example.c:166
#define ERROR_LED
LED0_GPIO is used as error status LED.
Definition: adcifb_sleepwalking_example.c:168

Array to hold the used GPIO pins.

Referenced by power_save_measures_init().