Microchip® Advanced Software Framework

nf.h File Reference
#include "conf_nf.h"
#include "board.h"
#include "gpio.h"
#include "ecchrs.h"
#include "nf.h"
#include "nf_512B.h"
#include "nf_2KB.h"

Data Structures

struct  St_nf_conf
 
struct  St_nf_id
 
struct  St_nf_link_id_block
 

Macros

#define _GLOBEXT_   extern
 
#define AVR32_EBI_NAND_FLASH_ADDRESS   AVR32_EBI_CS3_ADDRESS
 
#define G_CACHE_PROG   (NF_CACHE_PROGRAM)
 
#define G_CE_LOW   (NF_CE_LOW)
 
#define G_CLK_DFC_NFC   (CLK_DFC_NFC)
 
#define G_COPY_BACK_CONT   (NF_COPYBACK_CONT)
 
#define G_COPY_BACK_DISCONT   (NF_COPYBACK_DISCONT)
 
#define G_DEV_ID   (NF_DEV_ID)
 
#define G_DEV_MAKER   (NF_DEV_MAKER)
 
#define G_N_BLOCKS   (NF_N_BLOCKS)
 
#define G_N_ROW_CYCLES   (NF_N_ROW_CYCLES)
 
#define G_N_ZONES   (NF_N_ZONES)
 
#define G_OFST_BLK_STATUS   0
 
#define G_PROTECT_DEV   (NF_PROTECTED_DEVICES)
 
#define G_SHIFT_BLOCK_PAGE   (NF_SHIFT_BLOCK_PAGE)
 
#define G_SHIFT_PAGE_BYTE   (NF_SHIFT_PAGE_BYTE)
 
#define Is_nf_2k()   ( true )
 
#define Is_nf_512()   ( false )
 
#define Is_not_nf_2k()   ( false )
 
#define Is_not_nf_512()   ( true )
 
#define M_ID_HYNIX   0xAD
 
#define M_ID_INFINEON   0xC1
 
#define M_ID_MICRON   0x2C
 Resets the configuration state machine of the NFC. More...
 
#define M_ID_SAMSUNG   0xEC
 
#define M_ID_SANDISK   0x98
 
#define M_ID_ST   0x20
 
#define M_ID_TOSHIBA   0x98
 
#define M_ID_TOSHIBA96   0x96
 
#define NF_BAD_CONFIG   false
 
#define NF_BLOCK_ERASE_CMD   0x60
 Erase command. More...
 
#define NF_BLOCK_ERASE_CONFIRM_CMD   0xD0
 Confirm erase command. More...
 
#define NF_CACHE_PROGRAM_CMD   0x15
 Cache program (fast) command (2KB) More...
 
#define NF_COPY_BACK_CMD   0x35
 Copy-back command (2KB) More...
 
#define NF_DETECTION_ID   (DISABLE)
 
#define nf_force_CE()
 
#define NF_GENERIC_DRIVER   false
 
#define NF_MASK_STATUS_FAIL   (1<<0)
 Fail. More...
 
#define NF_MASK_STATUS_READY   (1<<6)
 Ready. More...
 
#define NF_MASK_STATUS_T_RDY_2KB   (1<<5)
 True Ready. More...
 
#define NF_MASK_STATUS_T_RDY_512B   (1<<6)
 True Ready. More...
 
#define NF_MAX_DEVICES   4
 
#define NF_N_GOOD_STATIC_BLOCK   32
 
#define Nf_open_page_read(page_addr, byte_addr)
 Opens a page for read. More...
 
#define Nf_open_page_write(page_addr, byte_addr)
 Opens a page for write. More...
 
#define NF_PAGE_PROGRAM_CMD   0x10
 Page Program command. More...
 
#define NF_RANDOM_DATA_INPUT_CMD   0x85
 Random data input command (2KB) More...
 
#define NF_RANDOM_READ_CMD_C1   0x05
 Random read Command (2KB) More...
 
#define NF_RANDOM_READ_CMD_C2   0xE0
 Confirm random read Command (2KB) More...
 
#define NF_READ_A_AREA_CMD   0x00
 Read Command of zone A (512B) More...
 
#define NF_READ_B_AREA_CMD   0x01
 Read Command of zone B (512B) More...
 
#define NF_READ_C_AREA_CMD   0x50
 Read Command of zone C (spare) (512B) More...
 
#define NF_READ_CMD   0x00
 Read Command (2KB) More...
 
#define NF_READ_CMD2   0x30
 Confirm read Command (2KB) More...
 
#define NF_READ_ID2_CMD   0x91
 Read ID 2 Command. More...
 
#define NF_READ_ID_CMD   0x90
 Read ID Command. More...
 
#define NF_READ_STATUS_CMD   0x70
 Read Status command. More...
 
#define NF_RESET_CMD   0xff
 Reset command. More...
 
#define NF_SEQUENTIAL_DATA_INPUT_CMD   0x80
 Sequential data input command. More...
 
#define NF_SHIFT_SECTOR_BYTE   9
 
#define NF_SPARE_POS   2048
 
#define nf_unforce_CE()
 
#define Nf_wait_cache_busy()
 Macro that tests the cache busy. More...
 
#define NFC_BLK_ID_DATA   0xFF
 
#define NFC_BLK_ID_FBB   0xB4
 
#define NFC_BLK_ID_QUARANTINE   0x8D
 
#define NFC_BLK_ID_RCV   0x72
 
#define NFC_BLK_ID_SUBLUT   0xE8
 
#define NFC_BLK_ID_SYSTEM   0x39
 
#define NFC_OFST_3_DATA_DST   0xFF
 
#define NFC_OFST_3_DATA_SRC   0x00
 
#define NFC_OFST_4_FBB_DRIVER_RELEASE   0x01
 
#define NFC_OFST_6_FBB_INVALID   0
 
#define NFC_OFST_6_FBB_VALID   0xFF
 
#define NFC_SPARE_DATA_INVALID   0
 
#define NFC_SPARE_DATA_VALID   0xFF
 
#define NFC_SPARE_OFST_1_BLK_ID   1
 
#define NFC_SPARE_OFST_2_BYTE_2   2
 
#define NFC_SPARE_OFST_3_BYTE_3   3
 
#define NFC_SPARE_OFST_4_BYTE_4   4
 
#define NFC_SPARE_OFST_6_LBA   6
 
#define NFC_SPARE_OFST_ECC1   13
 
#define NFC_SPARE_OFST_ECC2   8
 
#define NFC_SPARE_OFST_EXPORT   11
 
#define SIZE_BLOCK_PAGE   ((U8)1<<G_SHIFT_BLOCK_PAGE)
 
#define SIZE_PAGE_BYTE   ((U16)1<<G_SHIFT_PAGE_BYTE)
 
#define SIZE_PAGE_SECTOR   ((U8)1<<(G_SHIFT_PAGE_BYTE - S_SHIFT_SECTOR_BYTE))
 
#define SIZE_SECTOR_BYTE   ((U16)1<<S_SHIFT_SECTOR_BYTE)
 

Functions

bool nf_check_status (void)
 Check the status of the selected device. More...
 
U8 nf_check_type (U8 nb_dev)
 Tests the Nand Flash configuration. More...
 
void nf_copy_back_conf (U32 page_addr)
 
void nf_copy_back_init (U32 page_addr)
 Prepare a copy-back session. More...
 
U8 nf_detect (void)
 
void nf_erase_block (U32 page_addr, U8 force_erase)
 Erases a block. More...
 
U8 nf_get_freq (void)
 returns the frequency supported by the selected NF. More...
 
void nf_init (U32 hsb_f_hz)
 Initializes the Nand Flash Controller and low level driver. More...
 
void nf_mark_bad_block (U32 page_addr)
 Mark a block as 'invalid' by clearing it entirely. More...
 
void nf_open_page_read (U32 page_addr, U16 byte_addr)
 Opens a page for read. More...
 
void nf_open_page_write (U32 page_addr, U16 byte_addr)
 Opens a page for write. More...
 
void nf_print_block (U16 block_addr, U8 dev_id)
 
void nf_protect (void)
 Protect all the flashes. More...
 
static __always_inline U8 nf_rd_data (void)
 Read a data byte from the Nand Flash. More...
 
U32 nf_read_id (U8 read_id_cmd, U8 nf_num)
 Read the ID of the Nand-Flash. More...
 
void nf_read_spare_byte (U8 _MEM_TYPE_SLOW_ *p_byte, U8 n_byte, U32 page_addr)
 
void nf_reset_nands (U8 nb_dev)
 Reset all the NF devices. More...
 
static __always_inline void nf_select (U8 dev)
 Send a command cycle on the last selected Nand Flash. More...
 
static __always_inline void nf_send_nop (void)
 Ensure that both CLE and ALE are not asserted. More...
 
void nf_unprotect (void)
 unprotect all the flashes More...
 
void nf_wait_busy (void)
 Tests the true busy. More...
 
static __always_inline void nf_wr_addr (U8 addr)
 Send an address cycle on the last selected Nand Flash. More...
 
static __always_inline void nf_wr_cmd (U8 cmd)
 Send a command cycle on the last selected Nand Flash. More...
 
static __always_inline void nf_wr_data (U8 data)
 Write a data byte to the Nand Flash. More...