Microchip® Advanced Software Framework

 All Data Structures Files Functions Variables Typedefs Enumerations Enumerator Macros Groups Pages
CPU - SCIF - System Control Interface

Driver for the SCIF (System Control Interface).

The SCIF controls the oscillators, Generic Clocks, BODs, VREG, Temperature Sensor, and Backup Registers.

Data Structures

struct  scif_dfll_closedloop_conf_t
 DFLL closed-loop mode settings. More...
 
struct  scif_dfll_openloop_conf_t
 DFLL open-loop mode settings. More...
 
struct  scif_dfll_ssg_conf_t
 DFLL SSG settings. More...
 
struct  scif_gclk_opt_t
 Generic clock generation settings. More...
 
struct  scif_osc32_opt_t
 OSC32 startup options. More...
 
struct  scif_osc_opt_t
 OSC0/OSC1 startup options. More...
 

Macros

#define AVR32_SCIF_OSCCTRL0_OSCEN_DISABLE   0x00000000
 
#define AVR32_SCIF_OSCCTRL0_OSCEN_ENABLE   0x00000001
 
#define AVR32_SCIF_OSCCTRL32_OSC32EN_DISABLE   0x00000000
 
#define AVR32_SCIF_OSCCTRL32_OSC32EN_ENABLE   0x00000001
 
#define SCIF_DFLL_MAXFREQ_HZ   150000000UL
 
#define SCIF_DFLL_MAXFREQ_KHZ   150000
 The max DFLL output frequency. More...
 
#define SCIF_DFLL_MINFREQ_HZ   40000000UL
 
#define SCIF_DFLL_MINFREQ_KHZ   40000
 The min DFLL output frequency. More...
 
#define SCIF_EXT_CRYSTAL_MAX_FREQ_HZ   20000000UL
 
#define SCIF_EXT_CRYSTAL_MIN_FREQ_HZ   4000000UL
 Device-specific data. More...
 
#define SCIF_NOT_SUPPORTED   (-10000)
 Define "not supported" for the chosen implementation. More...
 
#define SCIF_OSC32_FREQ_HZ   32768
 The OSC32 frequency. More...
 
#define SCIF_POLL_TIMEOUT   100000
 The timeguard used for polling in ticks. More...
 
#define SCIF_RC120M_FREQ_HZ   120000000UL
 The RC120M frequency. More...
 
#define SCIF_RC120M_FREQ_KHZ   120000
 
#define SCIF_RC32K_FREQ_HZ   32768
 The RC32K slow clock frequency. More...
 
#define SCIF_RC32K_FREQ_KHZ   (SCIF_RC32K_FREQ_HZ/1000)
 
#define SCIF_SLOWCLOCK_FREQ_HZ   AVR32_SCIF_RCOSC_FREQUENCY
 The RCSYS slow clock frequency. More...
 
#define SCIF_SLOWCLOCK_FREQ_KHZ   (SCIF_SLOWCLOCK_FREQ_HZ/1000)
 
#define SCIF_UNLOCK(reg)   (AVR32_SCIF.unlock = (AVR32_SCIF_UNLOCK_KEY_VALUE << AVR32_SCIF_UNLOCK_KEY_OFFSET)|(reg))
 Unlock SCIF register macro. More...
 

Enumerations

enum  scif_gcctrl_oscsel_t {
  SCIF_GCCTRL_SLOWCLOCK = AVR32_SCIF_GCCTRL_OSCSEL_RCSYS,
  SCIF_GCCTRL_OSC32K = AVR32_SCIF_GCCTRL_OSCSEL_OSC32K,
  SCIF_GCCTRL_DFLL0 = AVR32_SCIF_GCCTRL_OSCSEL_DFLL0,
  SCIF_GCCTRL_OSC0 = AVR32_SCIF_GCCTRL_OSCSEL_OSC0,
  SCIF_GCCTRL_RC120M = AVR32_SCIF_GCCTRL_OSCSEL_RC120M,
  SCIF_GCCTRL_CPUCLOCK = AVR32_SCIF_GCCTRL_OSCSEL_CLK_CPU,
  SCIF_GCCTRL_HSBCLOCK = AVR32_SCIF_GCCTRL_OSCSEL_CLK_HSB,
  SCIF_GCCTRL_PBACLOCK = AVR32_SCIF_GCCTRL_OSCSEL_CLK_PBA,
  SCIF_GCCTRL_PBBCLOCK = AVR32_SCIF_GCCTRL_OSCSEL_CLK_PBB,
  SCIF_GCCTRL_RC32K = AVR32_SCIF_GCCTRL_OSCSEL_RC32K,
  SCIF_GCCTRL_CLK1K = AVR32_SCIF_GCCTRL_OSCSEL_CLK_1K,
  SCIF_GCCTRL_OSCSEL_INVALID
}
 The different clock source for the generic clocks. More...
 
enum  scif_osc_mode_t {
  SCIF_OSC_MODE_EXT_CLK = 0,
  SCIF_OSC_MODE_2PIN_CRYSTAL = 1,
  SCIF_OSC_MODE_NOT_SUPPORTED_1 = 2,
  SCIF_OSC_MODE_NOT_SUPPORTED_2 = 3,
  SCIF_OSC_MODE_2PIN_CRYSTAL_HICUR = 4,
  SCIF_OSC_MODE_NOT_SUPPORTED_3 = 5,
  SCIF_OSC_MODE_NOT_SUPPORTED_4 = 6,
  SCIF_OSC_MODE_NOT_SUPPORTED_5 = 7
}
 The different oscillator modes. More...
 
enum  scif_osc_t {
  SCIF_OSC0 = 0,
  SCIF_OSC1 = 1
}
 The different oscillators. More...
 

Interrupt Functions

static __always_inline void scif_enable_interrupts (unsigned long mask)
 Enable SCIF interrupts. More...
 
static __always_inline void scif_disable_interrupts (unsigned long mask)
 Disable SCIF interrupts. More...
 
static __always_inline
unsigned long 
scif_get_enabled_interrupts (void)
 Read the SCIF currently enabled interrupts. More...
 
static __always_inline
unsigned long 
scif_get_interrupts_status (void)
 Read the interrupt status of the SCIF. More...
 
static __always_inline void scif_clear_interrupts_status (unsigned long mask)
 Clear raised interrupts from the SCIF. More...
 

Power and Clocks Status Functions

static __always_inline
unsigned long 
scif_get_pclk_status (void)
 Read the Power and Clocks Status of the SCIF. More...
 

OSC0/OSC1 Functions

long int scif_start_osc (scif_osc_t osc, const scif_osc_opt_t *opt, bool wait_for_ready)
 Configure and start an OSC0/OSC1 oscillator. More...
 
bool scif_is_osc_ready (scif_osc_t osc)
 Is an oscillator stable and ready to be used as clock source? More...
 
long int scif_stop_osc (scif_osc_t osc)
 Stop an oscillator. More...
 
long int scif_configure_osc_crystalmode (scif_osc_t osc, unsigned int fcrystal)
 Configure an oscillator in crystal mode. More...
 
long int scif_configure_osc_extmode (scif_osc_t osc)
 Configure an external clock as input clock. More...
 
long int scif_enable_osc (scif_osc_t osc, unsigned int startup, bool wait_for_ready)
 Enable an oscillator with a given startup time. More...
 

OSC32 Functions

long int scif_start_osc32 (const scif_osc32_opt_t *opt, bool wait_for_ready)
 Configure and start the OSC32 oscillator. More...
 
static __always_inline bool scif_is_osc32_ready (void)
 Is OSC32 stable and ready to be used as clock source? More...
 
static __always_inline void scif_osc32_1kout_ena (void)
 Enable the 1kHz output of the OSC32 oscillator. More...
 
static __always_inline void scif_osc32_1kout_dis (void)
 Disable the 1kHz output of the OSC32 oscillator. More...
 
static __always_inline void scif_osc32_32kout_ena (void)
 Enable the 32kHz output of the OSC32 oscillator. More...
 
static __always_inline void scif_osc32_32kout_dis (void)
 Disable the 32kHz output of the OSC32 oscillator. More...
 
long int scif_stop_osc32 (void)
 Stop the OSC32 oscillator. More...
 

DFLL Control Functions

long int scif_dfll0_openloop_start (const scif_dfll_openloop_conf_t *pdfllconfig)
 Configure and start the DFLL0 in open loop mode. More...
 
long int scif_dfll0_openloop_start_auto (unsigned long TargetFreqkHz)
 Automatic configuration and start of the DFLL0 in open loop mode. More...
 
long int scif_dfll0_openloop_updatefreq (const scif_dfll_openloop_conf_t *pdfllconfig)
 Update the frequency of the DFLL0 in open loop mode. More...
 
long int scif_dfll0_openloop_updatefreq_auto (unsigned long TargetFreq)
 Automatic configuration to update the frequency of the DFLL0 in open loop mode. More...
 
long int scif_dfll0_openloop_stop (void)
 Stop the DFLL0 in open loop mode. More...
 
long int scif_dfll0_ssg_enable (scif_dfll_ssg_conf_t *pssg_conf)
 Configure and enable the SSG. More...
 
long int scif_dfll0_closedloop_start (const scif_dfll_closedloop_conf_t *pdfllconfig)
 Configure and start the DFLL0 in closed loop mode. More...
 
long int scif_dfll0_closedloop_configure_and_start (const scif_gclk_opt_t *gc_dfllif_ref_opt, unsigned long long target_freq_hz, bool enable_ssg)
 Depending on the target frequency, compute the DFLL configuration parameters and start the DFLL0 in closed loop mode. More...
 
#define scif_dfll0_ssg_gc_enable(pgc_conf)   scif_start_gclk(AVR32_SCIF_GCLK_DFLLIF_SSG, pgc_conf)
 Configure and enable the SSG reference generic clock. More...
 
#define scif_dfll0_closedloop_mainref_gc_enable(pgc_conf)   scif_start_gclk(AVR32_SCIF_GCLK_DFLLIF_REF, pgc_conf)
 Configure and enable the closed-loop mode main reference generic clock. More...
 
#define scif_dfll0_closedloop_dither_gc_enable(pgc_conf)   scif_dfll0_ssg_gc_enable(pgc_conf)
 Configure and enable the generic clock used by the closed-loop mode dithering stage and by the SSG. More...
 

120MHz RCosc Functions

void scif_start_rc120M (void)
 Start the 120MHz internal RCosc (RC120M) clock. More...
 
void scif_stop_rc120M (void)
 Stop the 120MHz internal RCosc (RC120M) clock. More...
 

32kHz internal RCosc (RC32K) Functions

void scif_start_rc32k (void)
 Start the 32kHz internal RCosc (RC32K) clock. More...
 
void scif_stop_rc32k (void)
 Stop the 32kHz internal RCosc (RC32K) clock. More...
 
void scif_disable_rc32out (void)
 Un-force the RC32 signal from being output on the dedicated pin (PA20) More...
 

Generic Clock Functions

long int scif_start_gclk (unsigned int gclk, const scif_gclk_opt_t *opt)
 Setup and start a generic clock. More...
 
long int scif_stop_gclk (unsigned int gclk)
 Stop a generic clock. More...
 
long int scif_gc_setup (unsigned int gclk, scif_gcctrl_oscsel_t clk_src, unsigned int diven, unsigned int divfactor)
 Setup a generic clock. More...
 
long int scif_gc_enable (unsigned int gclk)
 Enable a generic clock. More...
 

Miscellaneous Functions

long int scif_pclksr_statushigh_wait (unsigned long statusMask)
 Wait for a status high in the Power and Clocks status register. More...
 

#define AVR32_SCIF_OSCCTRL0_OSCEN_DISABLE   0x00000000
#define AVR32_SCIF_OSCCTRL0_OSCEN_ENABLE   0x00000001
#define AVR32_SCIF_OSCCTRL32_OSC32EN_DISABLE   0x00000000
#define AVR32_SCIF_OSCCTRL32_OSC32EN_ENABLE   0x00000001
#define scif_dfll0_closedloop_dither_gc_enable (   pgc_conf)    scif_dfll0_ssg_gc_enable(pgc_conf)

Configure and enable the generic clock used by the closed-loop mode dithering stage and by the SSG.

Parameters
pgc_confThe settings for the generic clock [INPUT]
Returns
Status.
Return values
0Dithering & SSG reference generic clock configured and started successfully.
<0Error.
#define scif_dfll0_closedloop_mainref_gc_enable (   pgc_conf)    scif_start_gclk(AVR32_SCIF_GCLK_DFLLIF_REF, pgc_conf)

Configure and enable the closed-loop mode main reference generic clock.

Parameters
pgc_confThe settings for the generic clock [INPUT]
Returns
Status.
Return values
0Main reference generic clock configured and started successfully.
<0Error.

Referenced by scif_dfll0_closedloop_configure_and_start().

#define scif_dfll0_ssg_gc_enable (   pgc_conf)    scif_start_gclk(AVR32_SCIF_GCLK_DFLLIF_SSG, pgc_conf)

Configure and enable the SSG reference generic clock.

Note
The frequency of the SSG reference clock should be higher than the CLK_DFLLIF_REF to ensure that the DFLLIF can lock.
Parameters
pgc_confThe settings for the generic clock [INPUT]
Returns
Status.
Return values
0SSG Generic clock configured and started successfully.
<0Error.
#define SCIF_DFLL_MAXFREQ_HZ   150000000UL
#define SCIF_DFLL_MAXFREQ_KHZ   150000

The max DFLL output frequency.

Referenced by scif_dfll0_openloop_start_auto().

#define SCIF_DFLL_MINFREQ_HZ   40000000UL
#define SCIF_DFLL_MINFREQ_KHZ   40000

The min DFLL output frequency.

Referenced by scif_dfll0_openloop_start_auto().

#define SCIF_EXT_CRYSTAL_MAX_FREQ_HZ   20000000UL

Referenced by scif_start_osc(), and scif_start_osc32().

#define SCIF_EXT_CRYSTAL_MIN_FREQ_HZ   4000000UL

Device-specific data.

< External crystal/clock min frequency (in Herz) External crystal/clock max frequency (in Herz)

Referenced by scif_start_osc(), and scif_start_osc32().

#define SCIF_NOT_SUPPORTED   (-10000)

Define "not supported" for the chosen implementation.

#define SCIF_OSC32_FREQ_HZ   32768

The OSC32 frequency.

#define SCIF_POLL_TIMEOUT   100000

The timeguard used for polling in ticks.

Referenced by scif_pclksr_statushigh_wait(), and scif_stop_gclk().

#define SCIF_RC120M_FREQ_HZ   120000000UL
#define SCIF_RC120M_FREQ_KHZ   120000
#define SCIF_RC32K_FREQ_HZ   32768

The RC32K slow clock frequency.

Referenced by scif_dfll0_closedloop_configure_and_start().

#define SCIF_RC32K_FREQ_KHZ   (SCIF_RC32K_FREQ_HZ/1000)
#define SCIF_SLOWCLOCK_FREQ_HZ   AVR32_SCIF_RCOSC_FREQUENCY

The RCSYS slow clock frequency.

Referenced by pcl_configure_clocks_rcsys(), and scif_dfll0_closedloop_configure_and_start().

#define SCIF_SLOWCLOCK_FREQ_KHZ   (SCIF_SLOWCLOCK_FREQ_HZ/1000)

The different clock source for the generic clocks.

Enumerator
SCIF_GCCTRL_SLOWCLOCK 
SCIF_GCCTRL_OSC32K 
SCIF_GCCTRL_DFLL0 
SCIF_GCCTRL_OSC0 
SCIF_GCCTRL_RC120M 
SCIF_GCCTRL_CPUCLOCK 
SCIF_GCCTRL_HSBCLOCK 
SCIF_GCCTRL_PBACLOCK 
SCIF_GCCTRL_PBBCLOCK 
SCIF_GCCTRL_RC32K 
SCIF_GCCTRL_CLK1K 
SCIF_GCCTRL_OSCSEL_INVALID 

The different oscillator modes.

Enumerator
SCIF_OSC_MODE_EXT_CLK 
SCIF_OSC_MODE_2PIN_CRYSTAL 
SCIF_OSC_MODE_NOT_SUPPORTED_1 
SCIF_OSC_MODE_NOT_SUPPORTED_2 
SCIF_OSC_MODE_2PIN_CRYSTAL_HICUR 
SCIF_OSC_MODE_NOT_SUPPORTED_3 
SCIF_OSC_MODE_NOT_SUPPORTED_4 
SCIF_OSC_MODE_NOT_SUPPORTED_5 
enum scif_osc_t

The different oscillators.

Enumerator
SCIF_OSC0 
SCIF_OSC1 

static __always_inline void scif_clear_interrupts_status ( unsigned long  mask)
static

Clear raised interrupts from the SCIF.

Parameters
maskThe interrupts to clear.
long int scif_configure_osc_crystalmode ( scif_osc_t  osc,
unsigned int  fcrystal 
)

Configure an oscillator in crystal mode.

Parameters
oscThe oscillator to configure [INPUT]
fcrystalCrystal frequency (Hz) [INPUT]
Returns
Status.
Return values
0Oscillator successfully configured.
<0Error configuring the oscillator.

References AVR32_ENTER_CRITICAL_REGION, AVR32_LEAVE_CRITICAL_REGION, u_avr32_scif_oscctrl0_t::oscctrl0, u_avr32_scif_oscctrl0_t::OSCCTRL0, PASS, SCIF_OSC_MODE_2PIN_CRYSTAL, and SCIF_UNLOCK.

Referenced by pcl_configure_clocks_osc0(), and pcl_switch_to_osc().

long int scif_configure_osc_extmode ( scif_osc_t  osc)

Configure an external clock as input clock.

Parameters
oscThe external clock to configure [INPUT]
Returns
Status.
Return values
0External clock successfully configured.
<0Error configuring the external clock.

References AVR32_ENTER_CRITICAL_REGION, AVR32_LEAVE_CRITICAL_REGION, u_avr32_scif_oscctrl0_t::oscctrl0, u_avr32_scif_oscctrl0_t::OSCCTRL0, PASS, SCIF_OSC_MODE_EXT_CLK, and SCIF_UNLOCK.

long int scif_dfll0_closedloop_configure_and_start ( const scif_gclk_opt_t gc_dfllif_ref_opt,
unsigned long long  target_freq_hz,
bool  enable_ssg 
)

Depending on the target frequency, compute the DFLL configuration parameters and start the DFLL0 in closed loop mode.

Note
Configures and enables the generic clock CLK_DFLLIF_REF to serve as the main reference.
This function only supports the following source clocks for the CLK_DFLLIF_REF generic clock: SCIF_GCCTRL_SLOWCLOCK (aka RCSYS), SCIF_GCCTRL_OSC32K, SCIF_GCCTRL_RC32K, SCIF_GCCTRL_OSC0, SCIF_GCCTRL_RC120M, SCIF_GCCTRL_CLK1K.
Parameters
gc_dfllif_ref_optThe settings for the CLK_DFLLIF_REF generic clock [INPUT]
target_freq_hzThe target frequency (in Hz) [INPUT]
enable_ssgEnable/disable the SSG feature [INPUT]
Returns
Status.
Return values
0DFLL0 configured and started successfully.
<0Error.

References scif_gclk_opt_t::clock_source, scif_dfll_closedloop_conf_t::coarse, scif_dfll_closedloop_conf_t::coarsemaxstep, scif_gclk_opt_t::diven, scif_gclk_opt_t::divider, scif_gclk_opt_t::extosc_f, scif_dfll_closedloop_conf_t::finemaxstep, scif_dfll_closedloop_conf_t::fmul, scif_dfll_closedloop_conf_t::imul, PASS, scif_dfll0_closedloop_mainref_gc_enable, scif_dfll0_closedloop_start(), SCIF_DFLL_MAXFREQ_HZ, SCIF_DFLL_MINFREQ_HZ, SCIF_GCCTRL_CLK1K, SCIF_GCCTRL_OSC0, SCIF_GCCTRL_OSC32K, SCIF_GCCTRL_RC120M, SCIF_GCCTRL_RC32K, SCIF_GCCTRL_SLOWCLOCK, SCIF_RC120M_FREQ_HZ, SCIF_RC32K_FREQ_HZ, and SCIF_SLOWCLOCK_FREQ_HZ.

Referenced by pcl_configure_clocks_dfll0().

long int scif_dfll0_closedloop_start ( const scif_dfll_closedloop_conf_t pdfllconfig)

Configure and start the DFLL0 in closed loop mode.

Note
The main reference generic clock must have previously been started.
Parameters
pdfllconfigThe DFLL parameters in closed loop mode [INPUT]
Returns
Status.
Return values
0DFLL0 configured and started successfully.
<0Error.

References AVR32_ENTER_CRITICAL_REGION, AVR32_LEAVE_CRITICAL_REGION, scif_dfll_closedloop_conf_t::coarse, scif_dfll_closedloop_conf_t::coarsemaxstep, u_avr32_scif_dfll0conf_t::dfll0conf, u_avr32_scif_dfll0conf_t::DFLL0CONF, ENABLE, scif_dfll_closedloop_conf_t::finemaxstep, scif_dfll_closedloop_conf_t::fmul, scif_dfll_closedloop_conf_t::imul, PASS, SCIF_DFLL0_MODE_CLOSEDLOOP, scif_pclksr_statushigh_wait(), and SCIF_UNLOCK.

Referenced by scif_dfll0_closedloop_configure_and_start().

long int scif_dfll0_openloop_start ( const scif_dfll_openloop_conf_t pdfllconfig)

Configure and start the DFLL0 in open loop mode.

Parameters
pdfllconfigThe DFLL parameters in open loop mode [INPUT]
Returns
Status.
Return values
0DFLL0 configured and started successfully.
<0Error.

References AVR32_ENTER_CRITICAL_REGION, AVR32_LEAVE_CRITICAL_REGION, scif_dfll_openloop_conf_t::coarse, u_avr32_scif_dfll0conf_t::dfll0conf, u_avr32_scif_dfll0conf_t::DFLL0CONF, ENABLE, scif_dfll_openloop_conf_t::fine, PASS, SCIF_DFLL0_MODE_OPENLOOP, scif_pclksr_statushigh_wait(), and SCIF_UNLOCK.

Referenced by scif_dfll0_openloop_start_auto().

long int scif_dfll0_openloop_start_auto ( unsigned long  TargetFreqkHz)

Automatic configuration and start of the DFLL0 in open loop mode.

Parameters
TargetFreqkHzThe DFLL target frequency (in kHz) [INPUT]
Returns
Status.
Return values
0DFLL0 configured and started successfully.
<0Error.

References scif_dfll_openloop_conf_t::coarse, scif_dfll_openloop_conf_t::fine, scif_dfll0_openloop_start(), SCIF_DFLL_COARSE_MAX, SCIF_DFLL_FINE_HALF, SCIF_DFLL_FINE_MAX, SCIF_DFLL_MAXFREQ_KHZ, and SCIF_DFLL_MINFREQ_KHZ.

long int scif_dfll0_openloop_stop ( void  )

Stop the DFLL0 in open loop mode.

Returns
Status.
Return values
0DFLL0 successfully stopped.
<0Error.

References AVR32_ENTER_CRITICAL_REGION, AVR32_LEAVE_CRITICAL_REGION, u_avr32_scif_dfll0conf_t::dfll0conf, u_avr32_scif_dfll0conf_t::DFLL0CONF, PASS, scif_pclksr_statushigh_wait(), and SCIF_UNLOCK.

long int scif_dfll0_openloop_updatefreq ( const scif_dfll_openloop_conf_t pdfllconfig)

Update the frequency of the DFLL0 in open loop mode.

Parameters
pdfllconfigThe DFLL parameters in open loop mode [INPUT]
Returns
Status.
Return values
0DFLL0 frequency updated successfully.
<0Error.

References AVR32_ENTER_CRITICAL_REGION, AVR32_LEAVE_CRITICAL_REGION, scif_dfll_openloop_conf_t::coarse, u_avr32_scif_dfll0conf_t::dfll0conf, u_avr32_scif_dfll0conf_t::DFLL0CONF, scif_dfll_openloop_conf_t::fine, PASS, scif_pclksr_statushigh_wait(), and SCIF_UNLOCK.

long int scif_dfll0_openloop_updatefreq_auto ( unsigned long  TargetFreq)

Automatic configuration to update the frequency of the DFLL0 in open loop mode.

Parameters
TargetFreqThe DFLL target frequency (in kHz) [INPUT]
Returns
Status.
Return values
0DFLL0 frequency updated successfully.
<0Error.
long int scif_dfll0_ssg_enable ( scif_dfll_ssg_conf_t pssg_conf)

Configure and enable the SSG.

Note
The SSG reference generic clock must have previously been enabled.
Parameters
pssg_confThe settings for the SCIF.DFLL0SSG register [INPUT]
Returns
Status.
Return values
0SSG Generic clock configured and started successfully.
<0Error.

References scif_dfll_ssg_conf_t::amplitude, AVR32_ENTER_CRITICAL_REGION, AVR32_LEAVE_CRITICAL_REGION, u_avr32_scif_dfll0ssg_t::dfll0ssg, u_avr32_scif_dfll0ssg_t::DFLL0SSG, ENABLE, PASS, SCIF_UNLOCK, scif_dfll_ssg_conf_t::step_size, and scif_dfll_ssg_conf_t::use_random.

static __always_inline void scif_disable_interrupts ( unsigned long  mask)
static

Disable SCIF interrupts.

Parameters
maskthe interrupts to disable.
void scif_disable_rc32out ( void  )

Un-force the RC32 signal from being output on the dedicated pin (PA20)

References AVR32_ENTER_CRITICAL_REGION, and AVR32_LEAVE_CRITICAL_REGION.

Referenced by scif_start_osc32().

static __always_inline void scif_enable_interrupts ( unsigned long  mask)
static

Enable SCIF interrupts.

Parameters
maskthe interrupts to enable.
long int scif_enable_osc ( scif_osc_t  osc,
unsigned int  startup,
bool  wait_for_ready 
)

Enable an oscillator with a given startup time.

Parameters
oscThe oscillator to configure [INPUT]
startupOscillator startup time (one of AVR32_SCIF_OSCCTRLx_STARTUP_x_RCOSC) [INPUT]
wait_for_readyWait for the oscillator to be stable before return [INPUT]
Returns
Status.
Return values
0Oscillator successfully started
<0Error starting the oscillator.

References AVR32_ENTER_CRITICAL_REGION, AVR32_LEAVE_CRITICAL_REGION, ENABLE, u_avr32_scif_oscctrl0_t::oscctrl0, u_avr32_scif_oscctrl0_t::OSCCTRL0, PASS, scif_pclksr_statushigh_wait(), and SCIF_UNLOCK.

Referenced by pcl_configure_clocks_osc0(), and pcl_switch_to_osc().

long int scif_gc_enable ( unsigned int  gclk)

Enable a generic clock.

Parameters
gclkgeneric clock number (0 for gc0...)
Returns
Status.
Return values
0Success.
<0An error occurred.

References PASS.

Referenced by pcl_configure_usb_clock().

long int scif_gc_setup ( unsigned int  gclk,
scif_gcctrl_oscsel_t  clk_src,
unsigned int  diven,
unsigned int  divfactor 
)

Setup a generic clock.

Parameters
gclkgeneric clock number (0 for gc0...)
clk_srcThe input clock source to use for the generic clock
divenGeneric clock divisor enable
divfactorGeneric clock divisor
Note
If the generic clock is already enabled, this function will disable it, apply the configuration then restart the generic clock.
Returns
Status.
Return values
0Success.
<0An error occurred.

References PASS, SCIF_GCCTRL_OSCSEL_INVALID, and scif_stop_gclk().

Referenced by pcl_configure_usb_clock().

static __always_inline unsigned long scif_get_enabled_interrupts ( void  )
static

Read the SCIF currently enabled interrupts.

Returns
The enabled interrupts.
static __always_inline unsigned long scif_get_interrupts_status ( void  )
static

Read the interrupt status of the SCIF.

Returns
The interrupts which have been triggered.
static __always_inline unsigned long scif_get_pclk_status ( void  )
static

Read the Power and Clocks Status of the SCIF.

Returns
The content of the PCLKSR register
static __always_inline bool scif_is_osc32_ready ( void  )
static

Is OSC32 stable and ready to be used as clock source?

Returns
Status.
Return values
trueoscillator stable and ready
falseoscillator not enabled or not ready.
bool scif_is_osc_ready ( scif_osc_t  osc)

Is an oscillator stable and ready to be used as clock source?

Parameters
oscThe oscillator [INPUT]
Returns
Status.
Return values
trueoscillator stable and ready
falseoscillator not enabled or not ready.
static __always_inline void scif_osc32_1kout_dis ( void  )
static

Disable the 1kHz output of the OSC32 oscillator.

static __always_inline void scif_osc32_1kout_ena ( void  )
static

Enable the 1kHz output of the OSC32 oscillator.

static __always_inline void scif_osc32_32kout_dis ( void  )
static

Disable the 32kHz output of the OSC32 oscillator.

static __always_inline void scif_osc32_32kout_ena ( void  )
static

Enable the 32kHz output of the OSC32 oscillator.

long int scif_pclksr_statushigh_wait ( unsigned long  statusMask)

Wait for a status high in the Power and Clocks status register.

Parameters
statusMaskMask field of the status to poll [INPUT]
Returns
Status.
Return values
0Status is high.
<0SCIF_POLL_TIMEOUT Timeout expired before the status was high.

Wait for a status high in the Power and Clocks status register.

Misc

Wait for a status high in the Power and Clocks status register.

Parameters
statusMaskMask field of the status to poll [INPUT]
Returns
Status.
Return values
0Status is high.
<0SCIF_POLL_TIMEOUT Timeout expired before the status was high.

References PASS, and SCIF_POLL_TIMEOUT.

Referenced by scif_dfll0_closedloop_start(), scif_dfll0_openloop_start(), scif_dfll0_openloop_stop(), scif_dfll0_openloop_updatefreq(), scif_enable_osc(), scif_start_osc(), and scif_start_osc32().

long int scif_start_gclk ( unsigned int  gclk,
const scif_gclk_opt_t opt 
)

Setup and start a generic clock.

Parameters
gclkThe generic clock number to setup and start (cf. datasheet)
optThe settings for the generic clock.
Returns
Status.
Return values
0Success.
<0An error occurred.

Setup and start a generic clock.

References scif_gclk_opt_t::clock_source, scif_gclk_opt_t::diven, scif_gclk_opt_t::divider, PASS, and SCIF_GCCTRL_OSCSEL_INVALID.

long int scif_start_osc ( scif_osc_t  osc,
const scif_osc_opt_t opt,
bool  wait_for_ready 
)

Configure and start an OSC0/OSC1 oscillator.

Parameters
oscThe oscillator to start [INPUT]
optThe configuration of the oscillator [INPUT]
wait_for_readyWait for the oscillator to be stable before return [INPUT]
Note
To avoid an infinite loop, this function checks the osc0 ready flag SCIF_POLL_TIMEOUT times.
Returns
Status.
Return values
0Oscillator start successful.
<0Error starting the oscillator.

Configure and start an OSC0/OSC1 oscillator.

Power and Clocks Status Functions OSC0/OSC1 Functions

References AVR32_ENTER_CRITICAL_REGION, AVR32_LEAVE_CRITICAL_REGION, ENABLE, scif_osc_opt_t::freq_hz, scif_osc_opt_t::gain, scif_osc_opt_t::mode, u_avr32_scif_oscctrl0_t::oscctrl0, u_avr32_scif_oscctrl0_t::OSCCTRL0, PASS, SCIF_EXT_CRYSTAL_MAX_FREQ_HZ, SCIF_EXT_CRYSTAL_MIN_FREQ_HZ, SCIF_OSC_MODE_2PIN_CRYSTAL, SCIF_OSC_MODE_EXT_CLK, scif_pclksr_statushigh_wait(), SCIF_UNLOCK, and scif_osc_opt_t::startup.

long int scif_start_osc32 ( const scif_osc32_opt_t opt,
bool  wait_for_ready 
)

Configure and start the OSC32 oscillator.

Parameters
optThe configuration of the oscillator [INPUT]
wait_for_readyWait for the oscillator to be stable before return [INPUT]
Note
To avoid an infinite loop, this function checks the osc32 ready flag SCIF_POLL_TIMEOUT times.
Returns
Status.
Return values
0Oscillator start successful.
<0Error starting the oscillator.

Configure and start the OSC32 oscillator.

References AVR32_ENTER_CRITICAL_REGION, AVR32_LEAVE_CRITICAL_REGION, scif_osc32_opt_t::en1k, scif_osc32_opt_t::en32k, ENABLE, scif_osc32_opt_t::mode, u_avr32_scif_oscctrl32_t::oscctrl32, u_avr32_scif_oscctrl32_t::OSCCTRL32, PASS, scif_osc32_opt_t::pinsel, scif_disable_rc32out(), SCIF_EXT_CRYSTAL_MAX_FREQ_HZ, SCIF_EXT_CRYSTAL_MIN_FREQ_HZ, SCIF_OSC_MODE_2PIN_CRYSTAL, SCIF_OSC_MODE_2PIN_CRYSTAL_HICUR, SCIF_OSC_MODE_EXT_CLK, scif_pclksr_statushigh_wait(), SCIF_UNLOCK, and scif_osc32_opt_t::startup.

Referenced by main().

void scif_start_rc120M ( void  )

Start the 120MHz internal RCosc (RC120M) clock.

Start the 120MHz internal RCosc (RC120M) clock.

References AVR32_ENTER_CRITICAL_REGION, AVR32_LEAVE_CRITICAL_REGION, and SCIF_UNLOCK.

Referenced by pcl_configure_clocks_rc120m().

void scif_start_rc32k ( void  )

Start the 32kHz internal RCosc (RC32K) clock.

Start the 32kHz internal RCosc (RC32K) clock.

References AVR32_ENTER_CRITICAL_REGION, AVR32_LEAVE_CRITICAL_REGION, and SCIF_UNLOCK.

long int scif_stop_gclk ( unsigned int  gclk)

Stop a generic clock.

Parameters
gclkThe generic clock number to stop.
Note
To avoid an infinite loop, this function checks the Clock enable flag SCIF_POLL_TIMEOUT times.
Returns
Status.
Return values
0Success.
<0Unable to stop generic clock.

References PASS, and SCIF_POLL_TIMEOUT.

Referenced by scif_gc_setup().

long int scif_stop_osc ( scif_osc_t  osc)

Stop an oscillator.

Parameters
oscThe oscillator to stop
Returns
Status.
Return values
0Oscillator successfully stopped.
<0An error occurred when stopping the oscillator.

References AVR32_ENTER_CRITICAL_REGION, AVR32_LEAVE_CRITICAL_REGION, PASS, and SCIF_UNLOCK.

long int scif_stop_osc32 ( void  )

Stop the OSC32 oscillator.

Returns
Status.
Return values
0Oscillator successfully stopped.
<0An error occurred when stopping the oscillator.

References PASS, and SCIF_UNLOCK.

void scif_stop_rc120M ( void  )

Stop the 120MHz internal RCosc (RC120M) clock.

References AVR32_ENTER_CRITICAL_REGION, AVR32_LEAVE_CRITICAL_REGION, and SCIF_UNLOCK.

void scif_stop_rc32k ( void  )

Stop the 32kHz internal RCosc (RC32K) clock.

References AVR32_ENTER_CRITICAL_REGION, AVR32_LEAVE_CRITICAL_REGION, and SCIF_UNLOCK.