Macros | |
#define | ADDRESSED 3 |
#define | ATTACHED 0 |
#define | CONFIGURED 4 |
#define | DEFAULT 2 |
#define | Is_device_enumerated() (usb_configuration_nb != 0) |
Returns true when device connected and correctly enumerated with a host. More... | |
#define | POWERED 1 |
#define | SUSPENDED 5 |
#define | USB_CONFIG_ATTRIBUTES_RESERVED 0x80 |
#define | USB_CONFIG_BUSPOWERED (USB_CONFIG_ATTRIBUTES_RESERVED | 0x00) |
#define | USB_CONFIG_REMOTEWAKEUP (USB_CONFIG_ATTRIBUTES_RESERVED | 0x20) |
#define | USB_CONFIG_SELFPOWERED (USB_CONFIG_ATTRIBUTES_RESERVED | 0x40) |
Functions | |
void | usb_process_request (void) |
This function reads the SETUP request sent to the default control endpoint and calls the appropriate function. More... | |
Variables | |
volatile U8 | usb_configuration_nb |
#define ADDRESSED 3 |
#define ATTACHED 0 |
#define CONFIGURED 4 |
#define DEFAULT 2 |
#define Is_device_enumerated | ( | ) | (usb_configuration_nb != 0) |
Returns true when device connected and correctly enumerated with a host.
The device high-level application should test this before performing any applicative request.
Referenced by device_template_task().
#define POWERED 1 |
#define SUSPENDED 5 |
#define USB_CONFIG_ATTRIBUTES_RESERVED 0x80 |
#define USB_CONFIG_BUSPOWERED (USB_CONFIG_ATTRIBUTES_RESERVED | 0x00) |
#define USB_CONFIG_REMOTEWAKEUP (USB_CONFIG_ATTRIBUTES_RESERVED | 0x20) |
#define USB_CONFIG_SELFPOWERED (USB_CONFIG_ATTRIBUTES_RESERVED | 0x40) |
void usb_process_request | ( | void | ) |
This function reads the SETUP request sent to the default control endpoint and calls the appropriate function.
When exiting of the usb_read_request function, the device is ready to manage the next request.
If the received request is not supported or a non-standard USB request, the function will call the custom decoding function in usb_specific_request module.
< unsupported request => call to user read request
References bmRequestType, CLEAR_FEATURE, EP_CONTROL, GET_CONFIGURATION, GET_DESCRIPTOR, GET_INTERFACE, GET_STATUS, SET_ADDRESS, SET_CONFIGURATION, SET_DESCRIPTOR, SET_FEATURE, SET_INTERFACE, SYNCH_FRAME, Usb_ack_setup_received_free, usb_clear_feature(), Usb_enable_stall_handshake, usb_get_configuration(), usb_get_descriptor(), usb_get_interface(), usb_get_status(), Usb_read_endpoint_data, Usb_reset_endpoint_fifo_access, usb_set_address(), usb_set_configuration(), usb_set_feature(), usb_set_interface(), and usb_user_read_request().
Referenced by usb_device_task().
volatile U8 usb_configuration_nb |