Class-Specific AS Interface Descriptor.
#include <usb_descriptors.h>
Data Fields | |
uint8_t | bDelay |
uint8_t | bDescriptorSubType |
uint8_t | bDescriptorType |
uint8_t | bLenght |
uint8_t | bTerminalLink |
uint16_t | wFormatTag |
uint8_t S_usb_as_interface_descriptor::bDelay |
uint8_t S_usb_as_interface_descriptor::bDescriptorSubType |
uint8_t S_usb_as_interface_descriptor::bDescriptorType |
uint8_t S_usb_as_interface_descriptor::bLenght |
uint8_t S_usb_as_interface_descriptor::bTerminalLink |
uint16_t S_usb_as_interface_descriptor::wFormatTag |