Microchip® Advanced Software Framework

S_usb_feature_unit_descriptor_micro Struct Reference

Class-Specific Feature Unit Descriptor.

#include <usb_descriptors.h>

Data Fields

uint8_t bControSize
 
uint8_t bDescriptorSubType
 
uint8_t bDescriptorType
 
uint8_t bLenght
 
uint8_t bmaControlCh1
 
uint8_t bmaControlMaster
 
uint8_t bSourceID
 
uint8_t bUnitID
 

uint8_t S_usb_feature_unit_descriptor_micro::bControSize
uint8_t S_usb_feature_unit_descriptor_micro::bDescriptorSubType
uint8_t S_usb_feature_unit_descriptor_micro::bDescriptorType
uint8_t S_usb_feature_unit_descriptor_micro::bLenght
uint8_t S_usb_feature_unit_descriptor_micro::bmaControlCh1
uint8_t S_usb_feature_unit_descriptor_micro::bmaControlMaster
uint8_t S_usb_feature_unit_descriptor_micro::bSourceID
uint8_t S_usb_feature_unit_descriptor_micro::bUnitID