Define for each 'feature unit' the max numbers of bmaControls One of them is used by the microphone!
#include <device_audio_task.h>
Data Fields | |
uint16_t | byte_count |
volatile uint8_t | g_n_bits_per_sample |
volatile uint8_t | g_n_channels |
volatile uint32_t | g_sample_freq |
uint8_t | interf_audio_stream |
bool | sample_rate_set |
uint16_t device_audio_task_data_t::byte_count |
volatile uint8_t device_audio_task_data_t::g_n_bits_per_sample |
volatile uint8_t device_audio_task_data_t::g_n_channels |
volatile uint32_t device_audio_task_data_t::g_sample_freq |
uint8_t device_audio_task_data_t::interf_audio_stream |
bool device_audio_task_data_t::sample_rate_set |