Microchip® Advanced Software Framework

scsi_decoder.c File Reference
#include "conf_usb.h"
#include "scsi_decoder.h"
#include "usb_drv.h"
#include "ctrl_access.h"

Functions

static void sbc_header_mode_sense (bool b_sense_10, uint8_t u8_data_length)
 Writes the header of the MODE SENSE (6) and (10) commands. More...
 
bool sbc_inquiry (void)
 Manages the INQUIRY command. More...
 
void sbc_lun_status_is_busy_or_change (void)
 Sends the status "busy or changed". More...
 
void sbc_lun_status_is_cdb_field (void)
 Sends the status "FAIL because CDB field is invalid". More...
 
void sbc_lun_status_is_fail (void)
 Sends the status "FAILED". More...
 
void sbc_lun_status_is_good (void)
 Sends the status "GOOD". More...
 
void sbc_lun_status_is_not_present (void)
 Sends the status "LUN not present". More...
 
void sbc_lun_status_is_protected (void)
 Sends the status "FAILED because of write protection". More...
 
bool sbc_mode_sense (bool b_sense_10)
 Manages the MODE SENSE (6) and (10) commands. More...
 
bool sbc_prevent_allow_medium_removal (void)
 Manages the PREVENT ALLOW MEDIUM REMOVAL command. More...
 
bool sbc_read_10 (void)
 Manages the READ (10) command. More...
 
bool sbc_read_capacity (void)
 Manages the READ CAPACITY (10) command. More...
 
bool sbc_request_sense (void)
 Manages the REQUEST SENSE command. More...
 
bool sbc_test_unit_ready (void)
 Manages the TEST UNIT READY command. More...
 
bool sbc_write_10 (void)
 Manages the WRITE (10) command. More...
 
bool scsi_decode_command (void)
 Decodes and launches the execution of SCSI commands. More...
 
static void send_informational_exceptions_page (void)
 Writes the Informational Exceptions Control mode page. More...
 
static void send_read_write_error_recovery_page (uint8_t length)
 Writes the Error Recovery mode page. More...
 

Variables

uint8_t g_scsi_command [16]
 SCSI command buffer. More...
 
uint32_t g_scsi_data_remaining
 Remaining data transfer length. More...
 
uint8_t g_scsi_ep_ms_in
 USB mass-storage IN endpoint. More...
 
uint8_t g_scsi_ep_ms_out
 USB mass-storage OUT endpoint. More...
 
s_scsi_sense g_scsi_sense
 Sense data. More...
 
uint8_t g_scsi_status
 SCSI status. More...
 
uint8_t ms_endpoint
 
static const
sbc_st_std_inquiry_data 
sbc_std_inquiry_data
 INQUIRY data. More...
 
uint8_t usb_LUN
 

static void sbc_header_mode_sense ( bool  b_sense_10,
uint8_t  u8_data_length 
)
static

Writes the header of the MODE SENSE (6) and (10) commands.

Parameters
b_sense_10Boolean indicating whether the (10) version of the command is requested:
  • true to specify a MODE SENSE (10) command;
  • false to specify a MODE SENSE (6) command.
u8_data_lengthData length in bytes.

References g_scsi_ep_ms_in, mem_wr_protect(), SBC_BLOCK_DESCRIPTOR_LENGTH, SBC_DEV_SPEC_PARAM_WR_ENABLE, SBC_DEV_SPEC_PARAM_WR_PROTECT, SBC_MEDIUM_TYPE, usb_LUN, Usb_reset_endpoint_fifo_access, and Usb_write_endpoint_data.

Referenced by sbc_mode_sense().

bool sbc_inquiry ( void  )

Manages the INQUIRY command.

The INQUIRY command requests that information regarding the logical unit and SCSI target device be sent to the application client.

See sbc_st_std_inquiry_data.

Returns
Boolean indicating success.

References EP_MS_IN, g_scsi_command, g_scsi_ep_ms_in, Is_usb_endpoint_enabled, Is_usb_in_ready, min, sbc_lun_status_is_cdb_field(), sbc_lun_status_is_good(), Sbc_valid_write_usb, Usb_nb_busy_bank, Usb_reset_endpoint_fifo_access, and usb_write_ep_txpacket().

Referenced by scsi_decode_command().

void sbc_lun_status_is_busy_or_change ( void  )
void sbc_lun_status_is_cdb_field ( void  )

Sends the status "FAIL because CDB field is invalid".

References SBC_ASC_INVALID_FIELD_IN_CDB, Sbc_build_sense, Sbc_send_failed, and SBC_SENSE_KEY_ILLEGAL_REQUEST.

Referenced by sbc_inquiry(), sbc_mode_sense(), sbc_read_10(), and sbc_write_10().

void sbc_lun_status_is_fail ( void  )
void sbc_lun_status_is_not_present ( void  )
void sbc_lun_status_is_protected ( void  )

Sends the status "FAILED because of write protection".

References SBC_ASC_WRITE_PROTECTED, Sbc_build_sense, Sbc_send_failed, and SBC_SENSE_KEY_DATA_PROTECT.

Referenced by sbc_write_10().

bool sbc_mode_sense ( bool  b_sense_10)

Manages the MODE SENSE (6) and (10) commands.

The MODE SENSE (6/10) commands provide a means for a device server to report parameters to an application client. They are complementary commands to the MODE SELECT (6/10) commands. Device servers that implement the MODE SENSE (6/10) commands shall also implement the MODE SELECT (6/10) commands.

Parameters
b_sense_10Boolean indicating whether the (10) version of the command is requested:
  • true to specify a MODE SENSE (10) command;
  • false to specify a MODE SENSE (6) command.
Returns
Boolean indicating success.

References g_scsi_command, sbc_header_mode_sense(), sbc_lun_status_is_cdb_field(), sbc_lun_status_is_good(), SBC_MODE_DATA_LENGTH_CODE_ALL, SBC_MODE_DATA_LENGTH_INFORMATIONAL_EXCEPTIONS, SBC_MODE_DATA_LENGTH_READ_WRITE_ERROR_RECOVERY, SBC_MSK_PAGE_CODE, SBC_PAGE_CODE_ALL, SBC_PAGE_CODE_INFORMATIONAL_EXCEPTIONS, SBC_PAGE_CODE_READ_WRITE_ERROR_RECOVERY, Sbc_valid_write_usb, send_informational_exceptions_page(), and send_read_write_error_recovery_page().

Referenced by scsi_decode_command().

bool sbc_prevent_allow_medium_removal ( void  )

Manages the PREVENT ALLOW MEDIUM REMOVAL command.

The PREVENT ALLOW MEDIUM REMOVAL command requests that the logical unit enable or disable the removal of the medium. The logical unit shall not allow medium removal if any initiator port currently has medium removal prevented.

Returns
Boolean indicating success.

References sbc_lun_status_is_good().

Referenced by scsi_decode_command().

bool sbc_read_10 ( void  )

Manages the READ (10) command.

The READ (10) command requests that the device server read the specified logical block(s) and transfer them to the data-in buffer. Each logical block read includes user data and, if the medium is formatted with protection information enabled, protection information. Each logical block transferred includes user data and may include protection information, based on the RDPROTECT field and the medium format. The most recent data value written in the addressed logical block shall be returned.

Returns
Boolean indicating success.

References CTRL_BUSY, CTRL_FAIL, CTRL_GOOD, CTRL_NO_PRESENT, EP_MS_OUT, g_scsi_command, g_scsi_data_remaining, LSB, memory_2_usb(), ms_endpoint, MSB, MSB0W, MSB1W, MSB2W, MSB3W, sbc_lun_status_is_busy_or_change(), sbc_lun_status_is_cdb_field(), sbc_lun_status_is_fail(), sbc_lun_status_is_good(), sbc_lun_status_is_not_present(), and usb_LUN.

Referenced by scsi_decode_command().

bool sbc_read_capacity ( void  )

Manages the READ CAPACITY (10) command.

The READ CAPACITY (10) command requests that the device server transfer 8 bytes of parameter data describing the capacity and medium format of the direct-access block device to the data-in buffer. This command may be processed as if it has a HEAD OF QUEUE task attribute. If the logical unit supports protection information, the application client should use the READ CAPACITY (16) command instead of the READ CAPACITY (10) command.

Returns
Boolean indicating success.

References CTRL_BUSY, CTRL_FAIL, CTRL_GOOD, CTRL_NO_PRESENT, g_scsi_ep_ms_in, mem_read_capacity(), Sbc_format_mcu_to_scsi_data, sbc_format_mcu_to_scsi_data, sbc_lun_status_is_busy_or_change(), sbc_lun_status_is_fail(), sbc_lun_status_is_good(), sbc_lun_status_is_not_present(), SBC_READ_CAPACITY_LENGTH, Sbc_valid_write_usb, usb_LUN, Usb_reset_endpoint_fifo_access, and Usb_write_endpoint_data.

Referenced by scsi_decode_command().

bool sbc_test_unit_ready ( void  )

Manages the TEST UNIT READY command.

The TEST UNIT READY command provides a means to check if the logical unit is ready. This is not a request for a self-test. If the logical unit is able to accept an appropriate medium-access command without returning CHECK CONDITION status, this command shall return a GOOD status. If the logical unit is unable to become operational or is in a state such that an application client action (e.g., START UNIT command) is required to make the logical unit ready, the command shall be terminated with CHECK CONDITION status, with the sense key set to NOT READY.

Returns
Boolean indicating success.

References CTRL_BUSY, CTRL_FAIL, CTRL_GOOD, CTRL_NO_PRESENT, mem_test_unit_ready(), sbc_lun_status_is_busy_or_change(), sbc_lun_status_is_fail(), sbc_lun_status_is_good(), sbc_lun_status_is_not_present(), and usb_LUN.

Referenced by scsi_decode_command().

bool sbc_write_10 ( void  )

Manages the WRITE (10) command.

The WRITE (10) command requests that the device server transfer the specified logical block(s) from the data-out buffer and write them. Each logical block transferred includes user data and may include protection information, based on the WRPROTECT field and the medium format. Each logical block written includes user data and, if the medium is formatted with protection information enabled, protection information.

Returns
Boolean indicating success.

References CTRL_BUSY, CTRL_FAIL, CTRL_GOOD, CTRL_NO_PRESENT, EP_MS_IN, g_scsi_command, g_scsi_data_remaining, LSB, mem_wr_protect(), ms_endpoint, MSB, MSB0W, MSB1W, MSB2W, MSB3W, sbc_lun_status_is_busy_or_change(), sbc_lun_status_is_cdb_field(), sbc_lun_status_is_fail(), sbc_lun_status_is_good(), sbc_lun_status_is_not_present(), sbc_lun_status_is_protected(), usb_2_memory(), and usb_LUN.

Referenced by scsi_decode_command().

bool scsi_decode_command ( void  )

Decodes and launches the execution of SCSI commands.

Returns
Boolean indicating success.

References g_scsi_command, SBC_ASC_INVALID_COMMAND_OPERATION_CODE, Sbc_build_sense, SBC_CMD_ACCESS_CONTROL_IN, SBC_CMD_ACCESS_CONTROL_OUT, SBC_CMD_EXTENDED_COPY, SBC_CMD_FORMAT_UNIT, SBC_CMD_INQUIRY, SBC_CMD_LOG_SELECT, SBC_CMD_LOG_SENSE, SBC_CMD_MODE_SELECT_10, SBC_CMD_MODE_SELECT_6, SBC_CMD_MODE_SENSE_10, SBC_CMD_MODE_SENSE_6, SBC_CMD_PERSISTENT_RESERVE_IN, SBC_CMD_PERSISTENT_RESERVE_OUT, SBC_CMD_PREFETCH_10, SBC_CMD_PREFETCH_16, SBC_CMD_PREVENT_ALLOW_MEDIUM_REMOVAL, SBC_CMD_READ_10, SBC_CMD_READ_12, SBC_CMD_READ_16, SBC_CMD_READ_6, SBC_CMD_READ_ATTRIBUTE, SBC_CMD_READ_BUFFER, SBC_CMD_READ_CAPACITY_10, SBC_CMD_READ_DEFECT_DATA_10, SBC_CMD_READ_DEFECT_DATA_12, SBC_CMD_READ_LONG_10, SBC_CMD_REASSIGN_BLOCKS, SBC_CMD_RECEIVE_COPY_RESULTS, SBC_CMD_RECEIVE_DIAGNOSTIC_RESULTS, SBC_CMD_REPORT_LUNS, SBC_CMD_REQUEST_SENSE, SBC_CMD_SEND_DIAGNOSTIC, SBC_CMD_START_STOP_UNIT, SBC_CMD_SYNCHRONIZE_CACHE_10, SBC_CMD_SYNCHRONIZE_CACHE_16, SBC_CMD_TEST_UNIT_READY, SBC_CMD_VERIFY_10, SBC_CMD_VERIFY_12, SBC_CMD_VERIFY_16, SBC_CMD_WRITE_10, SBC_CMD_WRITE_12, SBC_CMD_WRITE_16, SBC_CMD_WRITE_6, SBC_CMD_WRITE_AND_VERIFY_10, SBC_CMD_WRITE_AND_VERIFY_12, SBC_CMD_WRITE_AND_VERIFY_16, SBC_CMD_WRITE_ATTRIBUTE, SBC_CMD_WRITE_BUFFER, SBC_CMD_WRITE_LONG_10, SBC_CMD_WRITE_SAME_10, SBC_CMD_WRITE_SAME_16, SBC_CMD_XDREAD_10, SBC_CMD_XDWRITE_10, SBC_CMD_XDWRITEREAD_10, SBC_CMD_XPWRITE_10, sbc_inquiry(), sbc_lun_status_is_good(), sbc_mode_sense(), sbc_prevent_allow_medium_removal(), sbc_read_10(), sbc_read_capacity(), sbc_request_sense(), Sbc_send_failed, SBC_SENSE_KEY_ILLEGAL_REQUEST, sbc_test_unit_ready(), sbc_write_10(), Scsi_start_read_action, Scsi_start_write_action, Scsi_stop_read_action, and Scsi_stop_write_action.

Referenced by usb_mass_storage_cbw().

static void send_informational_exceptions_page ( void  )
static
static void send_read_write_error_recovery_page ( uint8_t  length)
static

uint8_t g_scsi_command[16]
uint32_t g_scsi_data_remaining

Remaining data transfer length.

Referenced by sbc_read_10(), sbc_write_10(), usb_mass_storage_cbw(), and usb_mass_storage_csw().

s_scsi_sense g_scsi_sense

Sense data.

uint8_t g_scsi_status

SCSI status.

Referenced by usb_mass_storage_csw().

uint8_t ms_endpoint
const sbc_st_std_inquiry_data sbc_std_inquiry_data
static

INQUIRY data.