#include "conf_usb.h"
#include "compiler.h"
#include "usb_drv.h"
#include "usb_host_enum.h"
#include "usb_host_task.h"
#include "usb_task.h"
Macros | |
#define | REG_CLASS_CNT (sizeof(registered_class) / sizeof(registered_class[0])) |
#define | REG_VID_PID_CNT (sizeof(registered_VID_PID) / sizeof(registered_VID_PID[0])) |
Functions | |
bool | host_check_class (void) |
This function checks if the device class is supported. More... | |
bool | host_check_VID_PID (void) |
This function checks if the VID and the PID are supported (if the VID & PID belong to the VID_PID table). More... | |
U32 | host_get_timeout (void) |
Status_t | host_transfer_control (void *data_pointer) |
This function is the generic control pipe management function. More... | |
Variables | |
volatile U8 | bmattributes |
bmAttributes byte of connected device More... | |
volatile U16 | device_PID |
PID of connected device. More... | |
volatile U16 | device_VID |
VID of connected device. More... | |
volatile S_interface | interface_supported [MAX_INTERFACE_SUPPORTED] |
Supported interfaces. More... | |
volatile U8 | maxpower |
maxpower byte of connected device (unit is 2 mA) More... | |
volatile U8 | nb_interface_supported = 0 |
Number of interfaces the host is able to support in the connected device. More... | |
static const U8 | registered_class [] = CLASS_SUBCLASS_PROTOCOL |
Table of registered classes (see conf_usb.h for table contents) More... | |
static const U16 | registered_VID_PID [] = VID_PID_TABLE |
Table of registered devices (see conf_usb.h for table contents) More... | |
#define REG_CLASS_CNT (sizeof(registered_class) / sizeof(registered_class[0])) |
Referenced by host_check_class().
#define REG_VID_PID_CNT (sizeof(registered_VID_PID) / sizeof(registered_VID_PID[0])) |
Referenced by host_check_VID_PID().
U32 host_get_timeout | ( | void | ) |
|
static |
Table of registered classes (see conf_usb.h for table contents)
Referenced by host_check_class().
|
static |
Table of registered devices (see conf_usb.h for table contents)
Referenced by host_check_VID_PID().