This is an example application for the mXT143E Xplained, designed to demonstrate the use of maXTouch devices, via a simple paint application.
This example has been tested with the mXT143E Xplained on the following boards:
This example can track the movement and pressure of fingers on the display, drawing the selected color from a pallet at the point of contact with a size corresponding to the size of the touch contact. Multiple fingers can be used to draw multiple lines simultaneously.
Relevant module dependencies for this application are:
This software was written for the GNU GCC and IAR for AVR. Other compilers may or may not work.
For further information, visit Microchip.